Path Planning

Path planning utilizes ROS2 service calls to the services running on AI Accelerator.

Setup

ark_path_planning_init()

Initializes the ROS2 service client to the path planner running on AI Accelerator

Planning and executing a path

The following is the two main methods to plan a path and execute it.

ark_move_path_plan_js(targetName, targetJ, speed_factor, popUpOnFailure) => bool

Perform a collision free move to a desired set of joint angles at the specified speed factor. Arguments

  • targetName (string): The name of the target. Can be a waypoint name. It’s used to cache the path planning result to speed up subsequent calls to the same target.

  • targetJ (array of 6 numbers): The desired joint angles.

  • speed_factor (number): The speed factor (from 0 to 1) at which to execute the path.

  • popUpOnFailure (bool): The flag to indicate whether we want the popup dialog to display if path planning fails.

ark_move_path_plan(targetName, targetP, speed_factor, popUpOnFailure) => bool

Perform a collision free move to a desired tool position at the specified speed factor Arguments

  • targetName (string): The name of the target. Can be a waypoint name. It’s used to cache the path planning result to speed up subsequent calls to the same target.

  • targetP (pose): The desired tool pose.

  • speed_factor (number): The speed factor (from 0 to 1) at which to execute the path.

  • popUpOnFailure (bool): The flag to indicate whether we want the popup dialog to display if path planning fails.

ROS2 Services

In addition to the URScript commands above, users can interact with the path planner via the ROS2 services provided in the following table.

Service Name

Type

Description

set_joint_limits

ur_cumotion_msgs/srv/SetJointLimits

Set the joint limits to be used by the path planner

attach_object

ur_cumotion_msgs/srv/AttachObject

Include/exclude part geometry during path planning

check_joint_states

ur_cumotion_msgs/srv/CheckJointStates

Check whether the given robot joint states are valid, i.e. collision-free and within joint limits. Note that multiple joint states can be checked at the same time

clear_cache

std_srvs/srv/Trigger

Clear the path planning cache

The parameters for each of the services’ request and response are given below.

SetJointLimits

Request

Parameter

Type

Description

joint_names

string[]

The names of the joints for which the limits will be set

lower_limits

float64[]

The lower limits to be set

upper_limits

float64[]

The upper limits to be set

Valid entries for joint_names are "shoulder_pan_joint", "shoulder_lift_joint", "elbow_joint",  "wrist_1_joint", "wrist_2_joint", and "wrist_3_joint", which represent the Base, Shoulder, Elblow, Wrist 1, Wrist 2, and Wrist 3 joints, respectively. Although the underlying ROS2 service supports setting joint limits individually, due to limitations of struct parsing, it’s recommended that users set lower and upper limits of all 6 joints at once, in which case joint_names can be omitted or empty. An example will be later provided. Response

Parameter

Type

Description

success

bool

True if set_joint_limits call is successful or false otherwise

error_message

string

The error message if unsuccessful

AttachObject

Request

Parameter

Type

Description

attach_object

bool

Whether to attach or detach the object

object_name

string

The object to be attached. If detached, this can be empty

Response

Parameter

Type

Description

—

—

—

success

bool

True if attach_object call is successful or false otherwise

CheckJointStates

Request

Parameter

Type

Description

joint_states

sensor_msgs/JointState[]

The joint states to be checked for validity

Response

Parameter

Type

Description

—

—

—

error_codes

StateValidityErrorCodes[]

The error validities with error codes for all the joint states

StateValidityErrorCodes

int32 val

int32 VALID=1

int32 INVALID_STATE_JOINT_LIMITS=-1
int32 INVALID_STATE_WORLD_COLLISION=-2
int32 INVALID_STATE_SELF_COLLISION=-3
int32 INVALID_STATE_UNKNOWN_ISSUE=-4

There’s no parameter for the std_srvs/srv/Trigger type.

Example Usages

Users can use the built-in ros_service_client_factory URScript command to create a service client by appending ARK_ROS2Namespace + "/ur_cumotion/" to the service name with the provided service type. See examples below.

joint_limit_client = ros_service_client_factory(ARK_ROS2Namespace + "/ur_cumotion/set_joint_limits", "ur_cumotion_msgs/srv/SetJointLimits")
attach_object_client = ros_service_client_factory(ARK_ROS2Namespace + "/ur_cumotion/attach_object", "ur_cumotion_msgs/srv/AttachObject")
check_joint_states_client = ros_service_client_factory(ARK_ROS2Namespace + "/ur_cumotion/check_joint_states", "std_srvs/srv/CheckJointStates")
clear_cache_client = ros_service_client_factory(ARK_ROS2Namespace + "/ur_cumotion/clear_cache", "std_srvs/srv/Trigger")

Afterwards, users can call the service by calling the call method of the service client. The argument in the call method is a struct that populate all the parameters required by the service type.

To clear the path planning cache, call

clear_cache_client.call(struct())

To set joint limits of all six joints to be - and + 360 degrees, we can call

joint_limit_client.call(struct(joint_names=[], lower_limits=[-3.14159, -3.14159, -3.14159, -3.14159, -3.14159, -3.14159], upper_limits=[3.14159, 3.14159, 3.14159, 3.14159, 3.14159, 3.14159]))

To attach a part named part_1, i.e. include the collision spheres of part_1 in path planning calculations, call

attach_object_client.call(struct(attach_object=True, object_name="part_1"))

Note that part_1 must be defined in the collision models. See example documentation for details.

To detach, i.e. remove the collision spheres of the part, call

attach_object_client.call(struct(attach_object=False, object_name=""))

To check whether the joint configuration [1.5, -3.0603, -1.8406, 0.3079, 1.5734, 1.4186] is valid, we can call

q=[1.5, -3.0603, -1.8406, 0.3079, 1.5734, 1.4186]
header = struct(seq=0, stamp=struct(sec=0, nanosec=0), frame_id="")
joint_state = struct(header=header, name=[], position=q, velocity=[], effort=[])
resp = check_joint_states_client.call(struct(joint_states=[joint_state]))
textmsg("error_code = " + to_str(resp.error_codes[0].val))