This document contains information about URInterface message types.
Documentation regarding ROS2 common message types, can be found at ROS2 Common interfaces.
std_msgs/Header header
uint8 CURRENT=0
uint8 VOLTAGE=1
uint8 domain # can be VOLTAGE or CURRENT
float32 value
std_msgs/Header header
bool data
std_msgs/Header header
uint64 cycle_counter
std_msgs/Header header
float32 current
std_msgs/Header header
bool[] state
std_msgs/Header header
float64[] data
std_msgs/Header header
float32 data
std_msgs/Header header
float64 data
uint8 JOINT_MODE_RESET=235
uint8 JOINT_MODE_SHUTTING_DOWN=236
uint8 JOINT_MODE_PART_D_CALIBRATION=237
uint8 JOINT_MODE_BACKDRIVE=238
uint8 JOINT_MODE_POWER_OFF=239
uint8 JOINT_MODE_READY_FOR_POWER_OFF=240
uint8 JOINT_MODE_NOT_RESPONDING=245
uint8 JOINT_MODE_MOTOR_INITIALISATION=246
uint8 JOINT_MODE_BOOTING=247
uint8 JOINT_MODE_PART_D_CALIBRATION_ERROR=248
uint8 JOINT_MODE_BOOTLOADER=249
uint8 JOINT_MODE_CALIBRATION=250
uint8 JOINT_MODE_VIOLATION=251
uint8 JOINT_MODE_FAULT=252
uint8 JOINT_MODE_RUNNING=253
uint8 JOINT_MODE_IDLE=255
std_msgs/Header header
uint8[6] joint_modes
uint8 tool_mode
std_msgs/Header header
float32[6] joint_temperatures
std_msgs/Header header
float64[6] voltages
int8 DISCONNECTED=0
int8 CONFIRM_SAFETY=1
int8 BOOTING=2
int8 POWER_OFF=3
int8 POWER_ON=4
int8 IDLE=5
int8 BACKDRIVE=6
int8 RUNNING=7
int8 UPDATING_FIRMWARE=8
std_msgs/Header header
int8 value
int8 PROGRAM_STATE_UNDEFINED=-1
int8 PROGRAM_STATE_STOPPING=0
int8 PROGRAM_STATE_STOPPED=1
int8 PROGRAM_STATE_RUNNING=2
int8 PROGRAM_STATE_PAUSING=3
int8 PROGRAM_STATE_PAUSED=4
int8 PROGRAM_STATE_RESUMING=5
int8 PROGRAM_STATE_RETRACTING=6
std_msgs/Header header
int8 value
int8 NORMAL=1
int8 REDUCED=2
int8 PROTECTIVE_STOP=3
int8 RECOVERY=4
int8 SAFEGUARD_STOP=5
int8 SYSTEM_EMERGENCY_STOP=6
int8 ROBOT_EMERGENCY_STOP=7
int8 VIOLATION=8
int8 FAULT=9
int8 VALIDATE_JOINT_ID=10
int8 UNDEFINED_SAFETY_MODE=11
int8 AUTOMATIC_MODE_SAFEGUARD_STOP=12
int8 SYSTEM_THREE_POSITION_ENABLING_STOP=13
std_msgs/Header header
int8 safety_state
# Note: 'fun' is short for function of the pin to be selected
bool OUTPUT_CURRENT = 0
bool OUTPUT_VOLTAGE = 1
# The value for pin [0-1]
# Value for 'FUN_CURRENT' must be from [0.002; 0.020] A ;
# Value for 'FUN_VOLTAGE' must be from [0; 10] V ;
# request fields
int8 pin
bool output_type
float64 value
bool success
# The value for pin [0-7]
# valid values for 'state' when setting digital IO or flags
bool STATE_OFF = 0
bool STATE_ON = 1
# request fields
int8 pin
bool state
bool success
# Set the speed slider on the teach pendant to the specified value.
#
# Value must be from [0; 1.0];
float32 value
bool success
std_msgs/Header header
float64 speed_scale
std_msgs/Header header
geometry_msgs/Pose pose
geometry_msgs/Twist speed
std_msgs/Header header
uint8 TOOL_OUPUT=0
uint8 TOOL_POWER=1
uint8 TOOL_SAFE=2
uint8 output_mode
uint8 OUTPUT_MODE_DISABLED=0
uint8 OUTPUT_MODE_SINKING=1
uint8 OUTPUT_MODE_SOURCING=2
uint8 OUTPUT_MODE_PUSH_PULL=3
uint8[2] output_pin_mode
std_msgs/Header header
float64 voltage
float64 current
std_msgs/Header header
std_msgs/String[] names
# Note: 'fun' is short for function of the pin to be selected
bool OUTPUT_CURRENT = 0
bool OUTPUT_VOLTAGE = 1
# The value for pin [0-1]
# Value for 'FUN_CURRENT' must be from [0.002; 0.020] A ;
# Value for 'FUN_VOLTAGE' must be from [0; 10] V ;
# request fields
int8 pin
bool output_type
float64 value
---
bool success
# The value for pin [0-7]
# valid values for 'state' when setting digital IO or flags
bool STATE_OFF = 0
bool STATE_ON = 1
# request fields
int8 pin
bool state
---
bool success
# Set the speed slider on the teach pendant to the specified value.
#
# Value must be from [0; 1.0];
float32 value
---
bool success
This document contains information about URInterface message types.
Documentation regarding ROS2 common message types, can be found at ROS2 Common interfaces.
std_msgs/Header header
uint8 CURRENT=0
uint8 VOLTAGE=1
uint8 domain # can be VOLTAGE or CURRENT
float32 value
std_msgs/Header header
bool data
std_msgs/Header header
uint64 cycle_counter
std_msgs/Header header
float32 current
std_msgs/Header header
bool[] state
std_msgs/Header header
float64[] data
std_msgs/Header header
float32 data
std_msgs/Header header
float64 data
uint8 JOINT_MODE_RESET=235
uint8 JOINT_MODE_SHUTTING_DOWN=236
uint8 JOINT_MODE_PART_D_CALIBRATION=237
uint8 JOINT_MODE_BACKDRIVE=238
uint8 JOINT_MODE_POWER_OFF=239
uint8 JOINT_MODE_READY_FOR_POWER_OFF=240
uint8 JOINT_MODE_NOT_RESPONDING=245
uint8 JOINT_MODE_MOTOR_INITIALISATION=246
uint8 JOINT_MODE_BOOTING=247
uint8 JOINT_MODE_PART_D_CALIBRATION_ERROR=248
uint8 JOINT_MODE_BOOTLOADER=249
uint8 JOINT_MODE_CALIBRATION=250
uint8 JOINT_MODE_VIOLATION=251
uint8 JOINT_MODE_FAULT=252
uint8 JOINT_MODE_RUNNING=253
uint8 JOINT_MODE_IDLE=255
std_msgs/Header header
uint8[6] joint_modes
uint8 tool_mode
std_msgs/Header header
float32[6] joint_temperatures
std_msgs/Header header
float64[6] voltages
int8 DISCONNECTED=0
int8 CONFIRM_SAFETY=1
int8 BOOTING=2
int8 POWER_OFF=3
int8 POWER_ON=4
int8 IDLE=5
int8 BACKDRIVE=6
int8 RUNNING=7
int8 UPDATING_FIRMWARE=8
std_msgs/Header header
int8 value
int8 PROGRAM_STATE_UNDEFINED=-1
int8 PROGRAM_STATE_STOPPING=0
int8 PROGRAM_STATE_STOPPED=1
int8 PROGRAM_STATE_RUNNING=2
int8 PROGRAM_STATE_PAUSING=3
int8 PROGRAM_STATE_PAUSED=4
int8 PROGRAM_STATE_RESUMING=5
int8 PROGRAM_STATE_RETRACTING=6
std_msgs/Header header
int8 value
int8 NORMAL=1
int8 REDUCED=2
int8 PROTECTIVE_STOP=3
int8 RECOVERY=4
int8 SAFEGUARD_STOP=5
int8 SYSTEM_EMERGENCY_STOP=6
int8 ROBOT_EMERGENCY_STOP=7
int8 VIOLATION=8
int8 FAULT=9
int8 VALIDATE_JOINT_ID=10
int8 UNDEFINED_SAFETY_MODE=11
int8 AUTOMATIC_MODE_SAFEGUARD_STOP=12
int8 SYSTEM_THREE_POSITION_ENABLING_STOP=13
std_msgs/Header header
int8 safety_state
# Note: 'fun' is short for function of the pin to be selected
bool OUTPUT_CURRENT = 0
bool OUTPUT_VOLTAGE = 1
# The value for pin [0-1]
# Value for 'FUN_CURRENT' must be from [0.002; 0.020] A ;
# Value for 'FUN_VOLTAGE' must be from [0; 10] V ;
# request fields
int8 pin
bool output_type
float64 value
bool success
# The value for pin [0-7]
# valid values for 'state' when setting digital IO or flags
bool STATE_OFF = 0
bool STATE_ON = 1
# request fields
int8 pin
bool state
bool success
# Set the speed slider on the teach pendant to the specified value.
#
# Value must be from [0; 1.0];
float32 value
bool success
std_msgs/Header header
float64 speed_scale
std_msgs/Header header
geometry_msgs/Pose pose
geometry_msgs/Twist speed
std_msgs/Header header
uint8 TOOL_OUPUT=0
uint8 TOOL_POWER=1
uint8 TOOL_SAFE=2
uint8 output_mode
uint8 OUTPUT_MODE_DISABLED=0
uint8 OUTPUT_MODE_SINKING=1
uint8 OUTPUT_MODE_SOURCING=2
uint8 OUTPUT_MODE_PUSH_PULL=3
uint8[2] output_pin_mode
std_msgs/Header header
float64 voltage
float64 current
std_msgs/Header header
std_msgs/String[] names
# Note: 'fun' is short for function of the pin to be selected
bool OUTPUT_CURRENT = 0
bool OUTPUT_VOLTAGE = 1
# The value for pin [0-1]
# Value for 'FUN_CURRENT' must be from [0.002; 0.020] A ;
# Value for 'FUN_VOLTAGE' must be from [0; 10] V ;
# request fields
int8 pin
bool output_type
float64 value
---
bool success
# The value for pin [0-7]
# valid values for 'state' when setting digital IO or flags
bool STATE_OFF = 0
bool STATE_ON = 1
# request fields
int8 pin
bool state
---
bool success
# Set the speed slider on the teach pendant to the specified value.
#
# Value must be from [0; 1.0];
float32 value
---
bool success