Returns the data stored on the specified Application Node
the name of the Application Node to fetch
Returns a list of the Application Nodes that contribute data to the currently loaded Application
Returns true if a grid from application is valid. If the variable name is not a grid or a grid defined somewhere else then it always returns true.
The name of the variable being validated
true if the grid is valid or is not a grid but a different variable type
returns a reply promise to the specified message
The type of message being sent
Optionaldata: anyThe message data
returns an observable that will emit any messages replied to the specified message
The type of message being sent
Optionaldata: anyThe message data
returns a reply promise for the requested message
The type of message being sent
Optionaldata: anyThe message data
returns an observable that will emit any messages replied to the requested message
The type of message being sent
Optionaldata: anyThe message data
Provides access to data stored in the application