Universal Robots TypeScript API - v10.12.0
Preparing search index...
contribution-api
JointPositions
Interface JointPositions
JointPositions defines a position of the robot, specified by the angle of the joints.
interface
JointPositions
{
base
:
number
;
elbow
:
number
;
shoulder
:
number
;
wrist1
:
number
;
wrist2
:
number
;
wrist3
:
number
;
}
Index
Properties
base
elbow
shoulder
wrist1
wrist2
wrist3
Properties
base
base
:
number
elbow
elbow
:
number
shoulder
shoulder
:
number
wrist1
wrist1
:
number
wrist2
wrist2
:
number
wrist3
wrist3
:
number
Settings
Member Visibility
External
Inherited
Protected
Theme
OS
Light
Dark
On This Page
Properties
base
elbow
shoulder
wrist1
wrist2
wrist3
Universal Robots TypeScript API - v10.12.0
Loading...
JointPositions defines a position of the robot, specified by the angle of the joints.