OptionalframeFrame to be shown as selected frame
OptionalframeWhether it should be possible to select another frame on the 'Move' screen
OptionaljointJoint positions to be shown as the preview robot
Whether the current screen is used to select and define a waypoint
The label for the waypoint
OptionalpositionPosition to be shown as the preview robot
OptionaltcpActive TCP to be set on move-screen initiation
OptionaltcpWhether it should be possible to select another TCP on the 'Move' screen
MoveScreenOptions
Object describing the options for an opened 'Move' screen