OptionalenabledOptionalparametersOptionalpermissionsOptionalrecordingThe frequency at which the recording should be taken, in Hertz (Hz). This parameter is optional and can be set to customize the recording interval. Must be between 1 and 500 Hz. Defaults to 100 Hz if not specified or out of range.
OptionalrecordingAn array of RTDE (Real-Time Data Exchange) signal names to be recorded during the smart skill execution. This parameter is optional and can be used to specify which signals to capture. Defaults to ['timestamp', 'target_q', 'actual_TCP_pose', 'target_TCP_pose', 'robot_status_bits', 'tcp_offset']. Note: 'target_q' will always be recorded.
Optionalversion
Describes an instance of a smart skill, with its own set of configuration parameters