Setup URSim with Docker
URSim is the offline simulator by Universal Robots. Packed into a remote or virtual machine it acts almost identically to a real robot connected over the network. While it is possible to get URSim running locally on a Linux system or inside a VirtualBox virtual machine, we will focus on getting things setup using Docker. Using Docker for your simulated robot allows you to very quickly spin up a robot testing instance with very little computational overload.
This guide will assume that you have Docker already installed and setup such that you can startup Docker containers using your current user.
The following example will start up a simulator on a UR5e. See the Docker image documentation for more details and configuration options.
Start a URSim docker container
To startup a simulated robot run the following command. This will start a Docker container named
ursim and startup a simulated UR5e robot. It exposes ports 5900 and 6080 for the browser-based
polyscope access. Note that this will expose the simulated robot to your local area network if you
don’t have any further level of security such as a firewall active. To prevent this, you can either
skip the port forwarding instructions (skip the two -p port:port statements) in which case
you’ll have to use the container’s IP address to access the polyscope gui rather than localhost or
you can restrict the port forwarding to a certain network interface (such as the looppack interface)
see Docker’s upstream documentation on port exposure for further information.
docker run --rm -it -p 5900:5900 -p 6080:6080 --name ursim universalrobots/ursim_e-series
External Control
To use the external control functionality, we will need the external_control URCap installed on
the robot and a program containing its ExternalControl program node. Both can be prepared on the
host machine either by creating an own Dockerfile containing those or by mounting two folders
containing installed URCaps and programs. See the Docker image documentation.
In this example, we will bind-mount a folder for the programs and URCaps. First, let’s create a local folder where we can store things inside:
mkdir -p ${HOME}/.ursim/programs
mkdir -p ${HOME}/.ursim/urcaps
Then, we can “install” the URCap by placing its .jar file inside the urcaps folder
URCAP_VERSION=1.0.5 # latest version as if writing this
curl -L -o ${HOME}/.ursim/urcaps/externalcontrol-${URCAP_VERSION}.jar \
https://github.com/UniversalRobots/Universal_Robots_ExternalControl_URCap/releases/download/v${URCAP_VERSION}/externalcontrol-${URCAP_VERSION}.jar
With this, start your URSim containers with the following command:
docker run --rm -it -p 5900:5900 -p 6080:6080 -v ${HOME}/.ursim/urcaps:/urcaps -v ${HOME}/.ursim/programs:/ursim/programs --name ursim universalrobots/ursim_e-series
With this, you should be able to setup the external_control URCap and create a program as
described in URCap setup guide.
Network setup
As described above, you can always start the URSim container using the default network setup. It will most probably always get the same IP address assigned every time, as long as you don’t have any other docker containers running. However, to make things a bit more explicit, we can setup our own docker network where we can assign a static IP address to our URSim container.
docker network create --subnet=192.168.56.0/24 ursim_net
docker run --rm -it -p 5900:5900 -p 6080:6080 --net ursim_net --ip 192.168.56.101 universalrobots/ursim_e-series
The above commands first create a network for docker and then create a container with the URSim image attaching to this network.
We can skip the port exposure, as we use a fixed IP address for the simulated robot. Therefore, the VNC web server will be available at http://192.168.56.101:6080/vnc.html.
Script startup
All of the above is put together in a script in the ur_client_library package.
rosrun ur_client_library start_ursim.sh
This will start a URSim docker container running on 192.168.56.101 with the external_control
URCap preinstalled. Created programs and installation changes will be stored persistently inside
${HOME}/.ursim/programs.
With this, you can run
roslaunch ur_robot_driver ur5e_bringup.launch robot_ip:=192.168.56.101
ros2 run ur_client_library start_ursim.sh
This will start a URSim docker container running on 192.168.56.101 with the external_control
URCap preinstalled. Created programs and installation changes will be stored persistently inside
${HOME}/.ursim/programs.
With this, you can run
ros2 launch ur_robot_driver ur_control.launch.py ur_type:=ur5e robot_ip:=192.168.56.101
If you have installed the client library from another source than ROS / ROS 2 or have
compiled it yourself, run the start_ursim.sh script directly from the package’s
scripts folder.