Overview
This driver collaborates closely with other ROS packages:
ur_calibrationPackage containing the calibration extraction program that will extract parameters for correctly parametrizing the URDF with calibration data from the specific robot.
ur_controllersControllers specifically made for UR manipulators.
ur_dashboard_msgsMessage packages used for the dashboard communication.
ur_moveit_configMoveIt! configuration for a plain robot. This is good as a starting point, but for a real application you would rather create your own MoveIt! configuration package containing your actual robot environment.
ur_description(separate repository)URDF description for UR manipulators
Feature list and roadmap
Feature |
ROS2 Driver |
|---|---|
joint-position-based control |
yes |
scaled joint-position-based control |
|
joint-velocity-based control |
yes1 |
Cartesian position-based control |
no |
Cartesian twist-based control |
no |
Trajectory forwarding for execution on robot |
|
reporting of tcp wrench |
yes |
pausing of programs |
yes |
continue trajectories after EM-Stop resume |
yes |
continue trajectories after protective stop |
yes |
panel interaction in between possible |
yes |
get and set IO states |
|
use tool communication forwarder on e-series |
yes (Setting up the tool communication on an e-Series / UR Series robot) |
use the driver without a teach pendant necessary |
yes |
support of CB1 and CB2 robots |
no |
trajectory extrapolation on robot on missing packages |
yes |
use ROS as drop-in for TP-programs |
yes |
headless mode |
yes (Headless mode) |
extract calibration from robot |
yes (ur_calibration) |
send custom script commands to robot |
|
Reconnect on a disconnected robot |
yes |
Freedrive Mode |
|
Tool Contact mode |
|
Force Mode |
1 Velocity-based joint control is implemented in the driver, the velocity-based joint trajectory controller would need tweaking of the gain parameters for each model.