Example driver
In the examples
subfolder you will find a minimal example of a running driver. It starts an
instance of the UrDriver
class and prints the RTDE values read from the controller. To run it make
sure to
have an instance of a robot controller / URSim running at the configured IP address (or adapt the address to your needs)
run it from the package’s main folder (the one where this README.md file is stored), as for simplicity reasons it doesn’t use any sophisticated method to locate the required files.