Usage

This chapter explains how to use the ur_robot_driver

Quick start

Driver startup

  • To start it with hardware, use:

    $ ros2 launch ur_robot_driver ur_control.launch.py ur_type:=<UR_TYPE> robot_ip:=<IP_OF_THE_ROBOT> launch_rviz:=true
    

    After starting the launch file start the external_control URCap program from the pendant, as described here.

  • To run it with URSim check details about it in this section.

  • To use mocked hardware (capability of ros2_control), use use_mock_hardware argument, like:

    $ ros2 launch ur_robot_driver ur_control.launch.py ur_type:=ur5e robot_ip:=yyy.yyy.yyy.yyy use_mock_hardware:=true
    

Sending commands to controllers

Once the driver is started, you can use it like any other ROS robot arm driver by sending trajectories to the /scaled_joint_trajectory_controller/follow_joint_trajectory action. If you’re new to that, please have a look at the section “Move the robot”.

Robot frames

While most tf frames come from the URDF and are published from the robot_state_publisher, there are a couple of things to know:

  • The base frame is the robot’s base as the robot controller sees it.

  • The tool0 is the tool frame as calculated using forward kinematics. If there is no additional tool configured on the Teach pendant (TP) and the URDF uses the specific robot’s calibration the lookup from base -> tool0 should be the same as the tcp pose shown on the TP when the feature “Base” is selected.

Troubleshooting

This section will cover some previously raised issues.

I started everything, but I cannot control the robot

The driver is started, but trajectory execution doesn’t work. Instead, the driver logs

Can't accept new action goals. Controller is not running.

The External Control program node from the URCap is not running on the robot. Make sure to create a program containing this node on the robot and start it using the “Play” button play_button. Inside the ROS terminal you should see the output Robot connected to reverse interface. Ready to receive control commands.

Note

When interacting with the teach pendant, or sending other primary programs to the robot, the program will be stopped. On the ROS terminal you will see an output Connection to reverse interface dropped.. Please see the section Continuation after interruptions for details on how to continue.

In general, make sure you’re starting up the robot as explained here.

When starting the program on the teach pendant, I get an error “The connection to the remote PC could not be established”

Make sure, the IP address setup is correct, as described in the setup guide.

Note

This error can also show up, when the ROS driver is not running.

When starting the driver, it crashes with “Variable ‘speed_slider_mask’ is currently controlled by another RTDE client”

Probably, there is a fieldbus enabled on the robot. Currently, this driver cannot be used together with an enabled fieldbus. Disable any fieldbus to workaround this error. ROS 1 driver issue #204 contains a guide how to do this.

I sent raw script code to the robot but it is not executed

On the e-Series the robot has to be in remote control mode to accept script code from an external source. This has to be switched from the Teach-Pendant.

Using the dashboard doesn’t work

On the e-Series the robot has to be in remote control mode to accept certain calls on the dashboard server. See Available dashboard commands for details.

When I start the driver, I get a symbol lookup error

This error can show for example like this:

[ros2_control_node-1] /opt/ros/rolling/lib/controller_manager/ros2_control_node: symbol lookup error: /opt/ros/rolling/lib/libpal_statistics_msgs__rosidl_typesupport_fastrtps_cpp.so: undefined symbol: _ZN8eprosima7fastcdr3Cdr9serializeEj
[ERROR] [ros2_control_node-1]: process has died [pid 251, exit code 127, cmd '/opt/ros/rolling/lib/controller_manager/ros2_control_node --ros-args --params-file /opt/ros/rolling/share/ur_robot_driver/config/ur5e_update_rate.yaml --params-file /tmp/launch_params_cdtxg1uh'].

When an upstream package introduces an ABI break, you may see this error. This can happen in two situations:

  • You have installed ROS a longer time ago and you have installed the driver package recently.

  • You have compiled the driver from source and you have updated your system, so the upstream libraries are there in a newer (ABI incompatible) version.

When this happens, it is best to update your complete system using

$ sudo apt update && sudo apt dist-upgrade

and then recompile your workspace if you have built things from source.