ur_controllers

This package contains controllers and hardware interface for ros2_controllers that are special to the UR robot family. Currently this contains:

  • A speed_scaling_state_broadcaster that publishes the current execution speed as reported by the robot to a topic interface. Values are floating points between 0 and 1.

  • A scaled_joint_trajectory_controller that is similar to the joint_trajectory_controller, but it uses the speed scaling reported to align progress of the trajectory between the robot and controller.

  • A io_and_status_controller that allows setting I/O ports, controlling some UR-specific functionality and publishes status information about the robot.

  • A tool_contact_controller that exposes an action to enable the tool contact function on the robot.

  • A twist_controller that streams Cartesian TCP velocities to the robot.

About this package

This package contains controllers not being available in the default ros2_controllers set. They are created to support more features offered by the UR robot family. Some of these controllers are example implementations for certain features and are intended to be generalized and merged into the default ros2_controllers controller set at some future point.

Controller description

This packages offers a couple of specific controllers that will be explained in the following sections.

ur_controllers/SpeedScalingStateBroadcaster

This controller publishes the current actual execution speed as reported by the robot. Values are floating points between 0 and 1.

In the ur_robot_driver this is calculated by multiplying the two RTDE data fields speed_scaling (which should be equal to the value shown by the speed slider position on the teach pendant) and target_speed_fraction (Which is the fraction to which execution gets slowed down by the controller).

ur_controlers/ScaledJointTrajectoryController

These controllers work similar to the well-known joint_trajectory_controller.

However, they are extended to handle the robot’s execution speed specifically. Because the default joint_trajectory_controller would interpolate the trajectory with the configured time constraints (ie: always assume maximum velocity and acceleration supported by the robot), this could lead to significant path deviation due to multiple reasons:

  • The speed slider on the robot might not be at 100%, so motion commands sent from ROS would effectively get scaled down resulting in a slower execution.

  • The robot could scale down motions based on configured safety limits resulting in a slower motion than expected and therefore not reaching the desired target in a control cycle.

  • Motions might not be executed at all, e.g. because the robot is E-stopped or in a protective stop

  • Motion commands sent to the robot might not be interpreted, e.g. because there is no external_control program node running on the robot controller.

  • The program interpreting motion commands could be paused.

The following plot illustrates the problem:

Trajectory execution with default trajectory controller

The graph shows a trajectory with one joint being moved to a target point and back to its starting point. As the joint’s speed is limited to a very low setting on the teach pendant, speed scaling (black line) activates and limits the joint speed (green line). As a result, the target trajectory (light blue) doesn’t get executed by the robot, but instead the pink trajectory is executed. The vertical distance between the light blue line and the pink line is the path error in each control cycle. We can see that the path deviation gets above 300 degrees at some point and the target point at -6 radians never gets reached.

All of the cases mentioned above are addressed by the scaled trajectory versions. Trajectory execution can be transparently scaled down using the speed slider on the teach pendant without leading to additional path deviations. Pausing the program or hitting the E-stop effectively leads to speed_scaling being 0 meaning the trajectory will not be continued until the program is continued. This way, trajectory executions can be explicitly paused and continued.

With the scaled version of the trajectory controller the example motion shown in the previous diagram becomes:

Trajectory execution with scaled_joint_trajectory_controller

The deviation between trajectory interpolation on the ROS side and actual robot execution stays minimal and the robot reaches the intermediate setpoint instead of returning “too early” as in the example above.

Under the hood this is implemented by proceeding the trajectory not by a full time step but only by the fraction determined by the current speed scaling. If speed scaling is currently at 50% then interpolation of the current control cycle will start half a time step after the beginning of the previous control cycle.

ur_controllers/GPIOController

This controller allows setting I/O ports, controlling some UR-specific functionality and publishes status information about the robot.

Published topics

  • ~/io_states [ur_msgs/msg/IOStates]: Status of all I/O ports (except T1 and T2)

  • ~/robot_mode [ur_dashboard_msgs/msg/RobotMode]: The current robot mode (e.g. POWER_OFF, IDLE, RUNNING)

  • ~/robot_program_running [std_msgs/msg/Bool]: Publishes whether the External Control program is running or not. If this is false no commands can be sent to the robot.

  • ~/safety_mode [ur_dashboard_msgs/msg/SafetyMode]: The robot’s current safety mode (e.g. PROTECTIVE_STOP, ROBOT_EMERGENCY_STOP, NORMAL)

  • ~/tool_data [ur_msgs/msg/ToolDataMsg]: Information about the robot’s tool configuration

  • ~/tool_data_t1 [ur_msgs/msg/ToolDataT1Msg]: Smart Panel (T1) inputs and outputs on a V2 tool flange. A message is published only while the robot reports Tool Flange V2 or later.

  • ~/tool_data_t2 [ur_msgs/msg/ToolDataT2Msg]: Measured voltage and current of connector T2. A message is published only while the robot reports Tool Flange V2 or later.

Smart Panel (T1)

~/tool_data_t1 publishes the Smart Panel signals on a V2 tool flange:

  • Left button, T1_DI0 (smart_panel_digital_in_states[0])

  • Center button, T1_DI1 (smart_panel_digital_in_states[1])

  • Right button, T1_DI2 (smart_panel_digital_in_states[2])

  • T1_CI0 and T1_CI1 (configurable_digital_in_states). This pair is a configurable safety-rated 2PE and can be used as the Freedrive pair.

  • Smart Panel detect, T1_CONNECTED (smart_panel_connected)

  • Smart Panel LED, T1_DO0 (digital_out_states[0]). digital_out_states is T1_DO0–T1_DO3.

Advertised services

  • ~/hand_back_control [std_srvs/srv/Trigger]: Calling this service will make the robot program exit the External Control program node and continue with the rest of the program.

  • ~/resend_robot_program [std_srvs/srv/Trigger]: When Headless mode is used, this service can be used to restart the External Control program on the robot.

  • ~/set_io [ur_msgs/srv/SetIO]: Set an output pin on the robot.

  • ~/set_analog_output [ur_msgs/srv/SetAnalogOutput]: Set an analog output on the robot. This also allows specifying the domain.

  • ~/set_payload [ur_msgs/srv/SetPayload]: Change the robot’s payload on-the-fly.

  • ~/set_speed_slider [ur_msgs/srv/SetSpeedSliderFraction]: Set the value of the speed slider.

  • ~/zero_ftsensor [std_srvs/srv/Trigger]: Zeroes the reported wrench of the force torque sensor.

ur_controllers/PassthroughTrajectoryController

This controller uses a control_msgs/FollowJointTrajectory action but instead of interpolating the trajectory on the ROS pc it forwards the complete trajectory to the robot controller for interpolation and execution. This way, the realtime requirements for the control PC can be massively decreased, since the robot always “knows” what to do next. That means that you should be able to run a stable driver connection also without a real-time patched kernel.

Interpolation depends on the robot controller’s implementation, but in conjunction with the ur_robot_driver it defaults to mimicking ros2_control’s spline interpolation. So, any trajectory planned e.g. with MoveIt! will be executed following the trajectory exactly.

A trajectory sent to the controller’s action server will be forwarded to the robot controller and executed there. Once all setpoints are transferred to the robot, the controller goes into a waiting state where it waits for the trajectory to be finished. While waiting, the controller tracks the time spent on the trajectory to ensure the robot isn’t stuck during execution.

This controller also supports speed scaling such that and scaling down of the trajectory done by the robot, for example due to safety settings on the robot or simply because a slower execution is configured on the teach pendant. This will be considered, during execution monitoring, so the controller basically tracks the scaled time instead of the real time.

Note

When using this controller with the URSim simulator execution times can be slightly larger than the expected time depending on the simulation host’s resources. This effect will not be present when using a real UR arm.

Note

This controller can currently only be used with URSim or a real UR robot. Neither mock hardware nor gazebo support this type of trajectory interfaces at the time being.

Tolerances

Currently, the trajectory passthrough controller only supports goal tolerances and goal time tolerances passed in the action directly. Please make sure that the tolerances are completely filled with all joint names.

A goal time tolerance of 0.0 means that no goal time tolerance is set and the action will not fail when execution takes too long.

A goal tolerance of 0.0 disables the corresponding tolerance check. For example, a position tolerance of 0.0 means that the final joint position is not checked. The same applies to velocity and acceleration tolerances.

Action interface / usage

To use this controller, publish a goal to the ~/follow_joint_trajectory action interface similar to the joint_trajectory_controller.

Currently, the controller doesn’t support replacing a running trajectory action. While a trajectory is being executed, goals will be rejected until the action has finished. If you want to replace it, first cancel the running action and then send a new one.

Parameters

The trajectory passthrough controller uses the following parameters:

Parameter name

Type

Default value

Description

joints (required)

string_array

<empty>

Joint names to listen to

state_interfaces (required)

string_array

<empty>

State interfaces provided by the hardware for all joints. Subset of ["position", "velocity", "acceleration"]

speed_scaling_interface_name

string

speed_scaling/speed_scaling_factor

Fully qualified name of the speed scaling interface name.

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

Interfaces

In order to use this, the hardware has to export a command interface for passthrough operations for each joint. It always has to export position, velocity and acceleration interfaces in order to be able to project the full JointTrajectory definition. This is why there are separate fields used, as for passthrough mode accelerations might be relevant also for robots that don’t support commanding accelerations directly to their joints.

<gpio name="${tf_prefix}trajectory_passthrough">
  <command_interface name="setpoint_positions_0"/>
  <command_interface name="setpoint_positions_1"/>
  <command_interface name="setpoint_positions_2"/>
  <command_interface name="setpoint_positions_3"/>
  <command_interface name="setpoint_positions_4"/>
  <command_interface name="setpoint_positions_5"/>
  <command_interface name="setpoint_velocities_0"/>
  <command_interface name="setpoint_velocities_1"/>
  <command_interface name="setpoint_velocities_2"/>
  <command_interface name="setpoint_velocities_3"/>
  <command_interface name="setpoint_velocities_4"/>
  <command_interface name="setpoint_velocities_5"/>
  <command_interface name="setpoint_accelerations_0"/>
  <command_interface name="setpoint_accelerations_1"/>
  <command_interface name="setpoint_accelerations_2"/>
  <command_interface name="setpoint_accelerations_3"/>
  <command_interface name="setpoint_accelerations_4"/>
  <command_interface name="setpoint_accelerations_5"/>
  <command_interface name="transfer_state"/>
  <command_interface name="time_from_start"/>
  <command_interface name="abort"/>
</gpio>

Note

The hardware component has to take care that the passthrough command interfaces cannot be activated in parallel to the streaming command interfaces.

Implementation details / dataflow

  • A trajectory passed to the controller will be sent to the hardware component one by one.

  • The controller will send one setpoint and then wait for the hardware to acknowledge that it can take a new setpoint.

  • This happens until all setpoints have been transferred to the hardware. Then, the controller goes into a waiting state where it monitors execution time and waits for the hardware to finish execution.

  • If execution takes longer than anticipated, a warning will be printed.

  • If execution finished taking longer than expected (plus the goal time tolerance), the action will fail.

  • When the hardware reports that execution has been aborted (The passthrough_trajectory_abort command interface), the action will be aborted.

  • When the action is preempted, execution on the hardware is preempted.

ur_controllers/TwistController

This controller streams Cartesian TCP velocities to the robot. It accepts velocity commands on a topic and forwards them to the hardware interface, which executes them using the URScript function speedl(...).

Unlike the forward_velocity_controller, which commands joint-space velocities via speedj, this controller commands tool-space velocities in the robot’s base frame.

Warning

With the twist controller, the user is responsible for sending commands that are safe and achievable. The robot will try to follow commands as fast as possible without trajectory planning.

Note

The robot will scale down the execution speed if its safety limits or speed slider require it. Unlike trajectory-based controllers, the twist controller does not automatically account for this scaling. Monitor the speed_scaling_state_broadcaster to detect when the robot is scaling down and adapt your commands accordingly.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

Topic interface / usage

The controller provides the ~/twist topic of type geometry_msgs/msg/TwistStamped for streaming velocity commands. To use this topic, the controller has to be in active state.

The header.frame_id must be the robot’s base frame (base or ${tf_prefix}base when using a prefixed robot). Commands in other frames are currently ignored.

Linear velocities are given in m/s and angular velocities in rad/s. Both are expressed in the robot’s base frame.

When the controller is activated or deactivated, all velocity commands are reset to zero. While active, the last received command is held until a new message arrives.

To activate the controller, first deactivate any other motion controller that claims the same hardware interfaces:

ros2 control switch_controllers --deactivate joint_trajectory_controller \
  --activate twist_controller

Example command to move the TCP slowly along the base x axis:

ros2 topic pub --rate 50 /twist_controller/twist geometry_msgs/msg/TwistStamped \
  "{header: {frame_id: 'base'}, twist: {linear: {x: 0.05}}}"

Note

For continuous motion, publish commands at a steady rate. When you stop publishing, the robot will continue executing the last received velocity until you send a zero twist or deactivate the controller.

Controller compatibility

The twist controller is mutually exclusive with all other motion controllers (joint_trajectory_controller, passthrough_trajectory_controller, forward_position_controller, forward_velocity_controller, forward_effort_controller, freedrive_mode_controller). It can be combined with the tool_contact_controller and the force_mode_controller*.

Note

When combining force_mode and twist remember that force_mode will “claim” axes that aren’t available for twist commands anymore.

Interfaces

In order to use this controller, the hardware has to export command interfaces for Cartesian velocities:

<gpio name="${tf_prefix}twist">
  <command_interface name="linear_velocity_x"/>
  <command_interface name="linear_velocity_y"/>
  <command_interface name="linear_velocity_z"/>
  <command_interface name="angular_velocity_x"/>
  <command_interface name="angular_velocity_y"/>
  <command_interface name="angular_velocity_z"/>
</gpio>

Note

The hardware component ensures that the twist command interfaces cannot be activated in parallel to other streaming or trajectory command interfaces.

ur_controllers/ForceModeController

This controller activates the robot’s Force Mode. This allows direct force control running on the robot control box. This controller basically interfaces the URScript function force_mode(...).

Force mode can be combined with (and only with) the passthrough trajectory controller in order to execute motions under a given force constraints.

Note

This is not an admittance controller, as given force constraints in a certain Cartesian dimension will overwrite the motion commands in that dimension. E.g. when specifying a certain force in the base frame’s z direction, any motion resulting from the move command in the base frame’s z axis will not be executed.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

check_io_successful_retries

int

10

Amount of retries for checking if setting force_mode was successful

Service interface / usage

The controller provides two services: One for activating force_mode and one for leaving it. To use those services, the controller has to be in active state.

  • ~/stop_force_mode [std_srvs/srv/Trigger]: Stop force mode

  • ~/start_force_mode [ur_msgs/srv/SetForceMode]: Start force mode

In ur_msgs/srv/SetForceMode the fields have the following meanings:

task_frame

All information (selection vector, wrench, limits, etc) will be considered to be relative to that pose. The pose’s frame_id can be anything that is transformable to the robot’s base frame.

selection_vector_<x,y,z,rx,ry,rz>

1 means that the robot will be compliant in the corresponding axis of the task frame.

wrench

The forces/torques the robot will apply to its environment. The robot adjusts its position along/about compliant axis in order to achieve the specified force/torque. Values have no effect for non- compliant axes. Actual wrench applied may be lower than requested due to joint safety limits.

type

An integer [1;3] specifying how the robot interprets the force frame

1

The force frame is transformed in a way such that its y-axis is aligned with a vector pointing from the robot tcp towards the origin of the force frame.

2

The force frame is not transformed.

3

The force frame is transformed in a way such that its x-axis is the projection of the robot tcp velocity vector onto the x-y plane of the force frame.

speed_limits

Maximum allowed tcp speed (relative to the task frame). This is only relevant for axes marked as compliant in the selection_vector.

deviation_limits

For non-compliant axes, these values are the maximum allowed deviation along/about an axis between the actual tcp position and the one set by the program.

damping_factor

Force mode damping factor. Sets the damping parameter in force mode. In range [0;1], default value is 0.025 A value of 1 is full damping, so the robot will decelerate quickly if no force is present. A value of 0 is no damping, here the robot will maintain the speed.

gain_scaling

Force mode gain scaling factor. Scales the gain in force mode. scaling parameter is in range [0;2], default is 0.5. A value larger than 1 can make force mode unstable, e.g. in case of collisions or pushing against hard surfaces.

ur_controllers/FrictionModelController

This controller allows setting per-joint viscous and Coulomb friction scale factors for direct torque control. The friction model scales control how much internal friction compensation the robot applies during direct torque control mode.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

check_io_successful_retries

int

10

Amount of retries for checking if setting friction scales was successful

Service interface / usage

The controller provides a service for setting friction scale factors. To use this service, the controller has to be in active state.

  • ~/set_friction_model_parameters [ur_msgs/srv/SetFrictionModelParameters]: Set per-joint viscous and Coulomb friction scale factors for direct torque control. Each array must contain exactly one value for each joint in range [0-1] where 0 means no compensation and 1 means full compensation.

ur_controllers/FreedriveModeController

This controller activates the robot’s Freedrive Mode, allowing to manually move the robot’ joints. This controller can’t be combined with any other motion controller.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

inactive_timeout

int

1

Time interval (in seconds) of message inactivity after which freedrive is deactivated

Usage

The controller provides the ~/enable_freedrive_mode topic of type [std_msgs/msg/Bool] for handling activation and deactivation:

  • to start and keep freedrive active, you’ll have to frequently publish a True msg on the indicated topic. If no further messages are received by the controller within the inactive_timeout seconds, freedrive mode will be deactivated. Hence, it is recommended to publish a True message at least every inactive_timeout/2 seconds.

    ros2 topic pub --rate 2 /freedrive_mode_controller/enable_freedrive_mode std_msgs/msg/Bool "{data: true}"
    
  • to deactivate freedrive mode is enough to publish a False msg on the indicated topic or to deactivate the controller or to stop publishing True on the enable topic and wait for the controller timeout.

ur_controllers/ToolContactController

This controller can enable tool contact on the robot. When tool contact is enabled, and the robot senses whether the tool has made contact with something. When that happens, it will stop all motion, and retract to where it first sensed the contact.

This controller can be used with any of the motion controllers.

The controller is not a direct representation of the URScript function tool_contact(direction), as it does not allow for choosing the direction. The direction of tool contact will always be the current TCP direction of movement.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

action_monitor_rate

double

20.0

The rate at which the action should be monitored in Hz.

Action interface / usage

The controller provides one action for enabling tool contact. For the controller to accept action goals it needs to be in active state.

  • ~/detect_tool_contact [ur_msgs/action/ToolContact]

    The action definition of ur_msgs/action/ToolContact has no fields, as a call to the action implicitly means that tool contact should be enabled. The result of the action is available through the status of the action itself. If the action succeeds it means that tool contact was detected, otherwise tool contact will remain active until it is either cancelled by the user, or aborted by the hardware. The action provides no feedback.

    The action can be called from the command line using the following command, when the controller is active:

    ros2 action send_goal /tool_contact_controller/detect_tool_contact ur_msgs/action/ToolContact
    

ur_controllers/URConfigurationController

This controller provides access to UR-specific robot configuration data. Currently, it provides a service to query the robot’s software version.

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

Service interface / usage

  • ~/get_software_version [ur_msgs/srv/GetRobotSoftwareVersion]: Get the robot’s software version. The response contains the major, minor and patch version of the robot’s software, as well as the build number if available. For example, for a robot running PolyScope 5.12.1 the response would be major version 5, minor version 12 and patch version 1.

ur_controllers/GravityUpdateController

This controller updates the gravity vector used by the robot controller. The robot uses this vector for gravity compensation during motion and torque control. By default, the robot assumes a gravity vector pointing straight down in its base frame (typically [0, 0, -9.82] m/s² in a standard floor-mounted setup).

Use this controller when the robot is mounted in a non-standard orientation, for example on a wall or ceiling, or when the base frame does not align with the physical gravity direction. The controller forwards the requested gravity vector to the robot through the URScript set_gravity() function.

The service accepts the gravity direction in any frame that can be transformed to the robot’s base frame. The controller rotates the vector into the base frame and forwards it to the hardware interface.

Note

The service expects the direction of gravity, pointing towards the Earth’s center. The controller negates this vector internally before sending it to the robot, as the underlying UR client library expects an anti-gravity vector (pointing away from the Earth’s center).

Parameters

Parameter name

Type

Default value

Description

tf_prefix

string

<empty>

Urdf prefix of the corresponding arm

check_io_successfull_retries

int

10

Amount of retries for checking if setting gravity was successful

Service interface / usage

The controller provides a service for setting the gravity vector. To use this service, the controller has to be in active state.

  • ~/set_gravity [ur_msgs/srv/SetGravity]: Set the gravity direction experienced by the robot.

The request contains a geometry_msgs/Vector3Stamped named gravity. The vector specifies the direction of gravity (towards the Earth’s center) and header.frame_id specifies the frame in which the vector is expressed. Any frame that can be transformed to the robot’s base frame can be used.

Example for a standard floor-mounted robot (gravity pointing down in the base frame):

ros2 service call /gravity_update_controller/set_gravity ur_msgs/srv/SetGravity \
  "{gravity: {header: {frame_id: 'base'}, vector: {x: 0.0, y: 0.0, z: -9.82}}}"

Example for a ceiling-mounted robot (gravity pointing up in the base frame):

ros2 service call /gravity_update_controller/set_gravity ur_msgs/srv/SetGravity \
  "{gravity: {header: {frame_id: 'base'}, vector: {x: 0.0, y: 0.0, z: 9.82}}}"

Note

When using the mocked hardware interface, the service may report failure even though the command was accepted, because the mock does not emulate the asynchronous success feedback from the robot.