ur_client_library
This documentation should help you to get started with the UR Client Library. The UR Client Library is a C++ library that allows you to control a UR robot from a remote computer. The library is open-source and can be found on GitHub.
Contents:
- Build / installation
- Setup a robot
- PolyScope version compatibility
- Library architecture
- Usage examples
- Dashboard client example
- Force Mode example
- Freedrive Mode example
- Instruction Executor example
- Primary Pipeline example
- Primary Pipeline Calibration example
- RTDE Client example
- RTDE register round-trip example
- External FTS example
- Script command interface
- Script Sender example
- Send script example
- Spline Interpolation example
- Tool Contact example
- Torque control example
- Trajectory Joint Interface example
- Trajectory streaming example
- Example driver
- Setup for real-time scheduling
- Migration notes
- C++ API Reference