Controllers
This help page describes the different controllers available for the ur_robot_driver. This
should help users finding the right controller for their specific use case.
Where are controllers defined?
Controllers are defined in the config/ur_controllers.yaml file.
How do controllers get loaded and started?
As this driver uses ros2_control all controllers are managed by the controller_manager. During startup, a default set of running controllers is loaded and started, another set is loaded in stopped mode. Stopped controllers won’t be usable right away, but they need to be started individually.
Controllers that are actually writing to some command interfaces (e.g. joint positions) will claim those interfaces. Only one controller claiming a certain interface can be active at one point.
Controllers can be switched either through the controller_manager’s service calls, through the
rqt_controller_manager gui or through the ros2 control verb from the package ros-${ROS_DISTRO}-ros2controlcli package.
For example, to switch from the default scaled_joint_trajectory_controller to the
forward_position_controller you can call
$ ros2 control switch_controllers --deactivate scaled_joint_trajectory_controller \
--activate forward_position_controller
[INFO 2024-09-23 20:32:04.373] [_ros2cli_1207798]: waiting for service /controller_manager/switch_controller to become available...
Successfully switched controllers
Read-only broadcasters
These broadcasters are read-only. They read states from the robot and publish them on a ROS topic. As they are read-only, they don’t claim any resources and can be combined freely. By default, they are all started and running. Those controllers do not require the robot to have the external_control script running.
joint_state_broadcaster
Type: joint_state_broadcaster/JointStateBroadcaster
Publishes all joints’ positions, velocities, and efforts as sensor_msgs/JointState on the
joint_states topic.
Note
The effort field contains motor currents, not physical joint torques by default. On newer
robot software versions (>= 5.23.0 / 10.11.0), the driver can report the actual joint torques as
efforts. To achieve that, set the hardware parameter use_currents_as_efforts to false.
See UR Hardware interface parameters for details.
speed_scaling_state_broadcaster
Type: ur_controllers/SpeedScalingStateBroadcaster
This broadcaster publishes the current actual execution speed as reported by the robot. Values are floating points between 0 and 1.
force_torque_sensor_broadcaster
Type: force_torque_sensor_broadcaster/ForceTorqueSensorBroadcaster
Publishes the robot’s wrench as reported from the controller.
Commanding controllers
The commanding controllers control the robot’s motions. Those controllers can’t be combined arbitrarily, as they will claim hardware resources. Only one controller can claim one hardware resource at a time.
scaled_joint_trajectory_controller (Default motion controller)
Type: ur_controllers/ScaledJointTrajectoryController
Scaled version of the joint_trajectory_controller. It uses the robot’s speed scaling information and thereby the safety compliance features, like pause on safeguard stop. In addition, it also makes it possible to adjust execution speed using the speed slider on the teach pendant or set the program in pause and restart it again. See it’s linked documentation for details.
io_and_status_controller
Type: ur_controllers/GPIOController
Allows setting I/O ports, controlling some UR-specific functionality and publishes status information about the robot.
forward_effort_controller
Type: effort_controllers/JointGroupEffortController
Allows setting target joint efforts (torques) directly. The user is therefore responsible for sending commands that are achievable. This controller is useful when implementing compliance or force control strategies.
forward_velocity_controller
Type: velocity_controllers/JointGroupVelocityController
Allows setting target joint velocities directly. The user is therefore responsible for sending commands that are achievable. This controller is particularly useful when doing servoing such as moveit_servo.
forward_position_controller
Type: position_controllers/JointGroupPositionController
Allows setting target joint positions directly. The robot tries to reach the target position as fast as possible. The user is responsible for sending commands that are achievable. This controller is particularly useful when doing servoing such as moveit_servo.
force_mode_controller
Type: ur_controllers/ForceModeController
Allows utilizing the robot’s builtin Force Mode.
freedrive_mode_controller
Type: ur_controllers/FreedriveModeController
Allows utilizing the robot’s Freedrive mode, making it possible to manually move the robot’s joints.