Script command interface
The Script Command Interface allows sending predefined commands to the robot while there is URScript running that is connected to it.
An example to utilize the script command interface can be found in the freedrive_example.cpp.
In order to use the ScriptCommandInterface, there has to be a script code running on the robot
that connects to the ScriptCommandInterface. This happens as part of the big
external_control.urscript. In order to reuse that with this example, we will create a full
UrDriver and leverage the ScriptCommandInterface through this.
At first, we create a ExampleRobotWrapper object in order to initialize communication with the
robot.
124 g_my_robot =
125 std::make_unique<ExampleRobotWrapper>(robot_ip, OUTPUT_RECIPE, INPUT_RECIPE, g_HEADLESS, "external_control.urp");
126
127 // Check if the robot version supports the friction scales command (requires 5.25.1 / 10.12.1)
128 auto version = g_my_robot->getUrDriver()->getVersion();
129 g_support_set_friction_scales = (version.major == 5 && version >= urcl::VersionInformation::fromString("5.25.1")) ||
130 (version.major >= 10 && version >= urcl::VersionInformation::fromString("10.12.1"));
131 if (!g_support_set_friction_scales)
132 {
133 URCL_LOG_INFO("Setting friction scales is not supported on this robot (version %s). "
134 "Requires at least 5.25.1 / 10.12.1. Skipping friction scale commands.",
135 version.toString().c_str());
136 }
137
138 if (!g_my_robot->isHealthy())
139 {
140 URCL_LOG_ERROR("Something in the robot initialization went wrong. Exiting. Please check the output above.");
141 return 1;
142 }
143
144 // We will send script commands from a separate thread. That will stay active as long as
145 // g_running is true.
146 g_running = true;
147 std::thread script_command_send_thread(sendScriptCommands);
The script commands will be sent in a separate thread which will be explained later.
Since the connection to the script command interface runs as part of the bigger external_control
script, we’ll wrap the calls alongside a full ExampleRobotWrapper. Hence, we’ll have to send
keepalive signals regularly to keep the script running:
151 std::chrono::duration<double> time_done(0);
152 std::chrono::duration<double> timeout(second_to_run);
153 auto stopwatch_last = std::chrono::steady_clock::now();
154 auto stopwatch_now = stopwatch_last;
155 while ((time_done < timeout || second_to_run.count() == 0) && g_my_robot->isHealthy())
156 {
157 g_my_robot->getUrDriver()->writeKeepalive();
158
159 stopwatch_now = std::chrono::steady_clock::now();
160 time_done += stopwatch_now - stopwatch_last;
161 stopwatch_last = stopwatch_now;
162 std::this_thread::sleep_for(
163 std::chrono::milliseconds(static_cast<int>(1.0 / g_my_robot->getUrDriver()->getControlFrequency())));
164 }
165
166 URCL_LOG_INFO("Timeout reached.");
167 g_my_robot->getUrDriver()->stopControl();
Sending script commands
Once the script is running on the robot, a connection to the driver’s script command interface
should be established. The UrDriver forwards most calls of the ScriptCommandInterface and
we will use that interface in this example. To send a script command, we can e.g. use
g_my_robot->getUrDriver()->zeroFTSensor().
In the example, we have wrapped the calls into a lambda function that will wait a specific timeout, print a log output what command will be sent and then call the respective command:
68 run_cmd("Setting tool voltage to 24V",
69 []() { g_my_robot->getUrDriver()->setToolVoltage(urcl::ToolVoltage::_24V); });
70 run_cmd("Enabling tool contact mode", []() { g_my_robot->getUrDriver()->startToolContact(); });
71
72 if (g_support_set_friction_scales)
73 {
74 // setFrictionScales is only supported from PolyScope 5.25.1 / PolyScope X 10.12.1 and upwards.
75 run_cmd("Turn off friction_compensation by setting the friction scales to zeroes",
76 []() { g_my_robot->getUrDriver()->setFrictionScales({ 0, 0, 0, 0, 0, 0 }, { 0, 0, 0, 0, 0, 0 }); });
77 }
78 run_cmd("Setting tool voltage to 0V", []() { g_my_robot->getUrDriver()->setToolVoltage(urcl::ToolVoltage::OFF); });
79 run_cmd("Zeroing the force torque sensor", []() { g_my_robot->getUrDriver()->zeroFTSensor(); });
80 run_cmd("Disabling tool contact mode", []() { g_my_robot->getUrDriver()->endToolContact(); });
81 run_cmd("Setting TCP offset to [0.0, 0.0, 0.10, 0.0, 0.0, 0.0]",
82 []() { g_my_robot->getUrDriver()->setTcpOffset({ 0.0, 0.0, 0.10, 0.0, 0.0, 0.0 }); });
83 run_cmd("Setting payload to 2.0kg with custom inertia and 0.5s transition time", []() {
84 g_my_robot->getUrDriver()->setTargetPayload(2.0, { 0.0, 0.0, 0.1 }, { 0.003, 0.003, 0.003, 0.0, 0.0, 0.0 }, 0.5);
85 });
86
87 if (g_support_set_friction_scales)
88 {
89 // setFrictionScales is only supported from PolyScope 5.25.1 / PolyScope X 10.12.1 and upwards.
90 run_cmd("Turn on friction_compensation by setting the friction scales to non-zero values", []() {
91 g_my_robot->getUrDriver()->setFrictionScales({ 0.9, 0.9, 0.8, 0.9, 0.9, 0.9 },
92 { 0.8, 0.8, 0.7, 0.8, 0.8, 0.8 });
93 });
94 }
95 }
The lambda itself looks like this:
52 auto run_cmd = [](const std::string& log_output, std::function<void()> func) {
53 const std::chrono::seconds timeout(3);
54 if (g_running)
55 {
56 // We wait a fixed time so that not each command is run directly behind each other.
57 // This is done for example purposes only, so users can follow the effect on the teach
58 // pendant.
59 std::this_thread::sleep_for(timeout);
60 URCL_LOG_INFO(log_output.c_str());
61 func();
62 }
63 };
For a list of all available script commands, please refer to the ScriptCommandInterface class
here.