Script Sender example

The following example creates a ScriptSender listening on port 12345 and sends the script textmsg("Hello, World!") when requested. A fully compilable example can be found in script_sender.cpp

Listing 51 examples/script_sender.cpp
33constexpr uint32_t PORT = 12345;
34
35int main(int argc, char* argv[])
36{
37  // Parse how may seconds to run
38  int second_to_run = -1;
39  if (argc > 2)
40  {
41    second_to_run = std::stoi(argv[2]);
42  }
43  urcl::control::ScriptSender sender(PORT, "textmsg(\"Hello, World!\")");
44
45  std::stringstream ss;
46  ss << "Waiting for incoming requests on port " << PORT;
47  if (second_to_run > 0)
48  {
49    ss << " for " << second_to_run << " seconds";
50  }
51  else
52  {
53    ss << " indefinitely";
54  }
55
56  std::cout << ss.str() << std::endl;
57
58  const auto start_time = std::chrono::system_clock::now();
59  while (second_to_run < 0 || std::chrono::system_clock::now() - start_time < std::chrono::seconds(second_to_run))
60  {
61    std::this_thread::sleep_for(std::chrono::milliseconds(500));
62  }
63  std::cout << "Timeout reached" << std::endl;
64
65  return 0;
66}