Trajectory streaming example
This example demonstrates open-ended trajectory streaming: a producer sends points to the
controller without declaring a total point count up front, then signals end-of-stream when it is
finished. Contrast this with the Trajectory Joint Interface example, which uses the finite
trajectory path where the point count is fixed in the initial TRAJECTORY_START message.
The streaming communication contract – the STREAM_START / STREAM_END handshake, the meaning
of the end-of-stream point count, the producer’s obligation not to starve the controller, and the
trajectory result codes – is described in Streaming trajectories. This page walks through the
example code and refers back to that section for the authoritative contract.
Setup
As with the other examples, we create a UrDriver (here through ExampleRobotWrapper) and
register a callback that fires when a trajectory finishes:
137 const bool headless_mode = true;
138 g_my_robot = std::make_unique<urcl::ExampleRobotWrapper>(robot_ip, OUTPUT_RECIPE, INPUT_RECIPE, headless_mode,
139 "external_control.urp");
140 if (!g_my_robot->isHealthy())
141 {
142 URCL_LOG_ERROR("Robot initialization failed. See preceding output for details.");
143 return 1;
144 }
145
146 g_my_robot->getUrDriver()->registerTrajectoryDoneCallback(&trajDoneCallback);
Trajectory execution is asynchronous, so completion is reported through a callback. The result distinguishes a successful run from a cancellation or a failure:
71void trajDoneCallback(const urcl::control::TrajectoryResult& result)
72{
73 g_trajectory_result = result;
74 g_trajectory_done = true;
75 URCL_LOG_INFO("Trajectory done with result %s", urcl::control::trajectoryResultToString(result).c_str());
76}
While a trajectory runs, the control PC must keep telling the robot program that the connection is
still alive. We do this by sending TRAJECTORY_NOOP messages while we wait; without them the robot
program stops waiting for input and the external_control program exits:
78// Pump TRAJECTORY_NOOP on the reverse socket while waiting for the
79// trajectory-done callback. Without this the URScript dispatcher's
80// reverse_socket read times out, which terminates the external_control
81// program entirely.
82void waitForTrajectoryDoneWithKeepalives()
83{
84 while (!g_trajectory_done)
85 {
86 std::this_thread::sleep_for(std::chrono::milliseconds(100));
87 g_my_robot->getUrDriver()->writeTrajectoryControlMessage(urcl::control::TrajectoryControlMessage::TRAJECTORY_NOOP);
88 }
89}
Generating a motion
To have something to stream, we sample a quintic-Hermite blend between two joint configurations. The blend has zero velocity and acceleration at both endpoints, which – as the streaming contract recommends – gives the final point the controlled-stop property needed to bring the robot cleanly to rest:
91// Sample a quintic-Hermite interpolation between q_start and q_end with zero
92// boundary velocity and acceleration, evaluated at fractional time s in [0, 1]
93// for a segment of total duration t_total:
94//
95// q(s) = q_start + (q_end - q_start) * (10s^3 - 15s^4 + 6s^5)
96// qd(t) = (q_end - q_start) * (30s^2 - 60s^3 + 30s^4) / t_total
97// qdd(t) = (q_end - q_start) * (60s - 180s^2 + 120s^3) / t_total^2
98struct SampledPoint
99{
100 urcl::vector6d_t q;
101 urcl::vector6d_t qd;
102 urcl::vector6d_t qdd;
103};
104
105SampledPoint sampleQuinticHermite(const urcl::vector6d_t& q_start, const urcl::vector6d_t& q_end, const double s,
106 const double t_total)
107{
108 const double s2 = s * s;
109 const double s3 = s2 * s;
110 const double s4 = s3 * s;
111 const double s5 = s4 * s;
112 const double pos_blend = 10.0 * s3 - 15.0 * s4 + 6.0 * s5;
113 const double vel_blend = (30.0 * s2 - 60.0 * s3 + 30.0 * s4) / t_total;
114 const double acc_blend = (60.0 * s - 180.0 * s2 + 120.0 * s3) / (t_total * t_total);
115
116 SampledPoint out{};
117 for (size_t i = 0; i < q_start.size(); ++i)
118 {
119 const double delta = q_end[i] - q_start[i];
120 out.q[i] = q_start[i] + delta * pos_blend;
121 out.qd[i] = delta * vel_blend;
122 out.qdd[i] = delta * acc_blend;
123 }
124 return out;
125}
Pre-positioning
Before streaming, we park the robot at a known start pose using an ordinary finite trajectory. This
doubles as a demonstration of the TRAJECTORY_START path for comparison:
149 // Park the robot at a known starting pose before the streaming demo. This
150 // also exercises the finite TRAJECTORY_START path for comparison.
151
152 const urcl::vector6d_t pose_a = { -1.57, -1.57, 0.0, -1.57, 0.0, 0.0 };
153 const urcl::vector6d_t pose_b = { -1.57, -1.20, 0.5, -1.57, 0.0, 0.0 };
154 const urcl::vector6d_t zero = { 0.0, 0.0, 0.0, 0.0, 0.0, 0.0 };
155
156 URCL_LOG_INFO("Pre-positioning to pose A via finite trajectory");
157 g_trajectory_done = false;
158 g_my_robot->getUrDriver()->writeTrajectoryControlMessage(urcl::control::TrajectoryControlMessage::TRAJECTORY_START,
159 1);
160 g_my_robot->getUrDriver()->writeTrajectorySplinePoint(pose_a, zero, zero, 3.0f);
161 waitForTrajectoryDoneWithKeepalives();
162 if (g_trajectory_result != urcl::control::TrajectoryResult::TRAJECTORY_RESULT_SUCCESS)
163 {
164 URCL_LOG_ERROR("Pre-positioning failed");
165 return 1;
166 }
Streaming the trajectory
We precompute all of the points up front. The final point inherits the qd = 0, qdd = 0
boundary condition of the quintic blend, so it is a compliant controlled-stop terminal:
169 // Stream a quintic-Hermite motion from pose A to pose B. All points are
170 // precomputed and written back-to-back; the robot works through them at its
171 // own pace. See doc/examples/trajectory_streaming.rst for details.
172
173 const int k_num_points = 200;
174 const double k_motion_duration_s = 2.0;
175 const double dt = k_motion_duration_s / k_num_points;
176
177 std::vector<SampledPoint> points;
178 points.reserve(k_num_points);
179 for (int i = 1; i <= k_num_points; ++i)
180 {
181 const double s = static_cast<double>(i) / k_num_points;
182 points.push_back(sampleQuinticHermite(pose_a, pose_b, s, k_motion_duration_s));
183 }
184 // The final quintic-Hermite point has qd=0, qdd=0: the controlled-stop
185 // terminal the streaming contract requires.
The stream itself is the STREAM_START -> points -> STREAM_END handshake. We open the stream,
write every point back-to-back, then close it, passing the total number of points written so the
controller knows how many are still outstanding before it reports completion:
187 URCL_LOG_INFO("Streaming %d points over %.2f s nominal motion duration", k_num_points, k_motion_duration_s);
188 g_trajectory_done = false;
189 g_trajectory_result = urcl::control::TrajectoryResult::TRAJECTORY_RESULT_UNKNOWN;
190
191 const auto stream_start_wall = std::chrono::steady_clock::now();
192 g_my_robot->getUrDriver()->writeTrajectoryControlMessage(
193 urcl::control::TrajectoryControlMessage::TRAJECTORY_STREAM_START);
194 for (const auto& p : points)
195 {
196 if (!g_my_robot->getUrDriver()->writeTrajectorySplinePoint(p.q, p.qd, p.qdd, static_cast<float>(dt)))
197 {
198 URCL_LOG_ERROR("writeTrajectorySplinePoint failed mid-stream");
199 return 1;
200 }
201 }
202 const auto stream_end_send_wall = std::chrono::steady_clock::now();
203 g_my_robot->getUrDriver()->writeTrajectoryControlMessage(
204 urcl::control::TrajectoryControlMessage::TRAJECTORY_STREAM_END, k_num_points);
205
206 waitForTrajectoryDoneWithKeepalives();
207 const auto callback_wall = std::chrono::steady_clock::now();
208
209 const auto send_duration =
210 std::chrono::duration_cast<std::chrono::milliseconds>(stream_end_send_wall - stream_start_wall);
211 const auto end_to_callback =
212 std::chrono::duration_cast<std::chrono::milliseconds>(callback_wall - stream_end_send_wall);
213 URCL_LOG_INFO("All %d points written in %lld ms wall-clock", k_num_points,
214 static_cast<long long>(send_duration.count()));
215 // Time from STREAM_END to the done callback. Here it is dominated by the
216 // consumer draining the batched backlog, not by STREAM_END processing; a
217 // steady-state producer would see roughly one controller step plus the
218 // stopj at trajectory thread exit. See doc/examples/trajectory_streaming.rst.
219 URCL_LOG_INFO("Time from sending STREAM_END to trajectory-done callback: %lld ms",
220 static_cast<long long>(end_to_callback.count()));
221 URCL_LOG_INFO("Final result: %s", urcl::control::trajectoryResultToString(g_trajectory_result).c_str());
222
223 if (g_trajectory_result != urcl::control::TrajectoryResult::TRAJECTORY_RESULT_SUCCESS)
224 {
225 URCL_LOG_ERROR("Streaming trajectory did not complete successfully");
226 return 1;
227 }
Because this example delivers the whole motion up front, it can never starve the controller: all the
work is in hand before execution finishes, so the robot simply plays through it. The example also
measures the time from sending STREAM_END to the trajectory-done callback. That time is large
here, but not because ending a stream is costly: the producer sends every point and then
STREAM_END within milliseconds, long before the robot has finished moving, so the callback cannot
fire until the robot has worked through the entire backlog. A producer that instead fed points in step
with the robot’s motion would send STREAM_END just as the robot reached the final point, and the
callback would follow almost immediately.
For the general case, where points are produced on the fly and pacing does matter, see the producer obligations in Streaming trajectories.