PolyScope version compatibility
Version-breaking changes
The table below shows breaking changes in the library compared to PolyScope versions. Compatibility is listed for CB3 robots (versions 3.x.y) and e-Series robots (versions 5.x.y) respectively. For PolyScope X (versions 10.x.y) all currently available versions are supported.
It might be possible to use the library in a more recent version than the compatible versions listed below, but that might either require some manual modifications or not using a subset of features. For that reason the breaking changes are also listed inside the table. Please note that choosing a higher library version than recommended happens on your own risk and will not be supported.
If your PolyScope version is less than the minimum required version for the latest library version, we suggest to upgrade your robot’s software. Please refer to the robot’s user manual how to update your robot.
If you don’t want to update your robot you can either use the release version as listed in the table below or checkout the latest tag before the breaking changes were introduced.
PolyScope version |
Max. release |
Latest tag |
Breaking changes |
|---|---|---|---|
< 3.12.3 / 5.5.1 |
1.1.0 |
||
< 3.14.3 / 5.9.4 |
1.3.1 |
Note
PolyScope X doesn’t support all features supported by this library for PolyScope 5. Currently, the following components are known not to be supported:
Dashboard client – PolyScope X does not have a Dashboard server, but in version 10.11.0 introduced the Robot API, that fulfills some of the same purposes. The robot API has not yet reached feature parity with the Dashboard server.
Implemented features, and their version requirements:
Introduced in PolyScope version
Functionality group
examples
10.11.0
Robot state control
power on, power off, brake release, etc
10.11.0
Load and play programs
load program, play, pause, etc
10.12.0
Robot Program interactions
Upload/update program, download program, list programs, etc
10.12.0
Get robot modes
Robot mode, safety mode, operational mode, remote control
10.14.0
Popup interactions
open, close, close safety popup
10.14.0
Get robot information
Polyscope version, robot model, serial number
10.14.0
System control
Shut down robot
10.14.0
Logging
Add entry to system log
10.14.0
Flight reports
Generating and downloading flight reports
Using external control on PolyScope X requires another URCapX for making external control work. This is currently in the process of being created. See Universal Robots External Control URCapX
Features requiring a specific PolyScope version
Features in this section have been added in a backwards-compatible way. It is still possible to use this library with an older compatible version, but trying to use one of the features below might lead to a runtime exception.
Torque control (From version 2.4.0)
The direct torque control mode is only available on PolyScope 5.23.0 / 10.10.0 and later. This
includes the TORQUE control mode in the ReverseInterface as well as the
setFrictionCompensation() function in the ScriptCommandInterface.