Dashboard client
Advertised Services
add_to_log (ur_dashboard_msgs/AddToLog)
Service to add a message to the robot’s log. On PolyScope X this requires version >= 10.14.0.
brake_release (std_srvs/Trigger)
Service to release the brakes. If the robot is currently powered off, it will get powered on the fly.
clear_operational_mode (std_srvs/Trigger)
If this service is called the operational mode can again be changed from PolyScope, and the user password is enabled.
close_popup (std_srvs/Trigger)
Close a (non-safety) popup on the teach pendant. On PolyScope X this requires version >= 10.14.0.
close_safety_popup (std_srvs/Trigger)
Close a safety popup on the teach pendant. On PolyScope X this requires version >= 10.14.0.
connect (std_srvs/Trigger)
Service to connect or reconnect to the dashboard server. Required after startup when autoconnect is false.
download_program (ur_dashboard_msgs/DownloadProgram)
PolyScope X only: Download a program with the given name from the robot and save it as
*.urpx file locally. This service is only available on a PolyScope X robot with version >=
10.12.0.
get_loaded_program (ur_dashboard_msgs/GetLoadedProgram)
Get the name of the currently loaded program.
get_programs (ur_dashboard_msgs/GetPrograms)
PolyScope X only: Get a list of all programs on the robot. This service is only available on a PolyScope X robot with version >= 10.12.0.
get_robot_mode (ur_dashboard_msgs/GetRobotMode)
Service to query the current robot mode
get_safety_mode (ur_dashboard_msgs/GetSafetyMode)
Service to query the current safety mode
is_in_remote_control (ur_dashboard_msgs/IsInRemoteControl)
Service to query whether the robot is in remote control
load_installation (ur_dashboard_msgs/Load)
Load a robot installation from a file
load_program (ur_dashboard_msgs/Load)
Load a robot program from a file on the robot. On PolyScope 5, this can be either file in the
robot’s programs folder or an absolute path to a file. The filename has to include the .urp
ending. On PolyScope X, this has to be the program’s name as shown in the Programs overview on the
robot, without a .urpx suffix.
pause (std_srvs/Trigger)
Pause a running program.
play (std_srvs/Trigger)
Start execution of a previously loaded program
popup (ur_dashboard_msgs/Popup)
Service to show a popup on the UR Teach pendant. On PolyScope X (>= 10.14.0) an optional title
can be provided; on PolyScope 5 / CB3 the title is ignored.
power_off (std_srvs/Trigger)
Power off the robot motors
power_on (std_srvs/Trigger)
Power on the robot motors. To fully start the robot, call ‘brake_release’ afterwards.
program_running (ur_dashboard_msgs/IsProgramRunning)
Query whether there is currently a program running
program_saved (ur_dashboard_msgs/IsProgramSaved)
Query whether the current program is saved
program_state (ur_dashboard_msgs/GetProgramState)
Service to query the current program state
quit (ur_dashboard_msgs/GetLoadedProgram)
Disconnect from the dashboard service.
raw_request (ur_dashboard_msgs/RawRequest)
General purpose service to send arbitrary messages to the dashboard server
restart_safety (std_srvs/Trigger)
Used when robot gets a safety fault or violation to restart the safety. After safety has been rebooted the robot will be in Power Off. NOTE: You should always ensure it is okay to restart the system. It is highly recommended to check the error log before using this command (either via PolyScope or e.g. ssh connection).
resume (std_srvs/Trigger)
PolyScope X only: Resume a paused program on a PolyScope X robot. This service is only available on a PolyScope X robot with version >= 10.11.0.
shutdown (std_srvs/Trigger)
Shutdown the robot controller. On PolyScope X this requires version >= 10.14.0.
stop (std_srvs/Trigger)
Stop program execution on the robot
unlock_protective_stop (std_srvs/Trigger)
Dismiss a protective stop to continue robot movements. NOTE: It is the responsibility of the user to ensure the cause of the protective stop is resolved before calling this service.
update_program (ur_dashboard_msgs/UpdateProgram)
PolyScope X only: Update a program on the robot. If the program does not exist or the program is currently loaded, this service call will fail. This service is only available on a PolyScope X robot with version >= 10.12.0.
upload_program (ur_dashboard_msgs/UploadProgram)
PolyScope X only: Upload a program to the robot. If a program with the same name already exists, this service call will fail. This service is only available on a PolyScope X robot with version >= 10.12.0.
get_polyscope_version (ur_dashboard_msgs/GetPolyScopeVersion)
CB3 | PolyScope 5 | PolyScope X >= 10.14.0 Get PolyScope version of the robot
get_serial_number (ur_dashboard_msgs/GetSerialNumber)
CB3 | PolyScope 5 | PolyScope X >= 10.14.0 Get serial number of robot
get_user_role (ur_dashboard_msgs/GetUserRole)
CB3 only Get current user role
set_user_role (ur_dashboard_msgs/SetUserRole)
CB3 only Set user role on the robot
get_operational_mode (ur_dashboard_msgs/GetOperationalMode)
PolyScope 5 | PolyScope X 10.12.0 onwards Get current operational mode of the robot
set_operational_mode (ur_dashboard_msgs/SetOperationalMode)
PolyScope 5 only Set operational mode of the robot. When this has been called, the teach pendant can not be used to change the operational mode until clear_operational_mode has been called.
get_robot_model (ur_dashboard_msgs/GetRobotModel)
CB3 | PolyScope 5 | PolyScope X >= 10.14.0 Get the robot model, in the format URx. It should be noted this call does not differentiate between e-series and CB3, so UR5 and UR5e will both report as UR5
get_safety_status (ur_dashboard_msgs/GetSafetyStatus)
PolyScope 5 only Get current safety status of the robot system, this is more detailed than get_safety_mode and should be preferred when possible
generate_flight_report (ur_dashboard_msgs/GenerateFlightReport)
CB3 | PolyScope 5 | PolyScope X >= 10.14.0 Generate flight report of the chosen type, defaults to SYSTEM. On PolyScope 5 / CB3 it is required to wait at least 30 seconds between triggering software or controller reports. On PolyScope X the report_type argument is ignored.
generate_support_file (ur_dashboard_msgs/GenerateSupportFile)
CB3 | PolyScope 5 Generate a support file a the specified location. Location is relative to the programs folder, if saving to a subfolder it must exist prior to the service call. Defaults to saving to the programs folder. On PolyScope X use download_support_file instead.
download_support_file (ur_dashboard_msgs/DownloadSupportFile)
PolyScope X only (>= 10.14.0): Download the robot’s support files as a zip archive to target_path on the machine running the dashboard client.
Parameters
autoconnect (default: true)
If true (default), the dashboard client connects to the robot during startup and retries until
the connection succeeds or ROS is shut down. If false, the node starts without contacting the
robot and only exposes the ~/connect service until a connection succeeds; call ~/connect
once the robot is available to register the remaining dashboard services.
receive_timeout (default: 20.0)
Timeout (in seconds, double) after which a call to the dashboard server will be considered failure if no answer has been received. This defaults to 20 seconds, as some operations (like loading larger programs) can take a while.
robot_ip (Required)
The IP address under which the robot is reachable.