Universal Robots ROS 2 Driver Documentation Logo
  • ur_client_library
  • ur_description
  • ur_robot_driver
    • Overview
    • Installation
    • Usage
    • Operation modes
    • Setting up the tool communication on an e-Series / UR Series robot
    • UR Hardware interface
    • UR Hardware interface parameters
    • Dashboard client
    • Robot state helper
    • Controller stopper
    • Trajectory until node
    • Migration notes
  • ur_calibration
  • ur_controllers
  • ur_moveit_config
  • ur_simulation_gz
  • ur_rtde_ros2_publisher
  • Tutorial examples
  • Migration Notes
  • Build status
  • ROS 2 integration paths
Universal Robots ROS 2 Driver Documentation
  • ur_robot_driver
  • Edit on GitHub

ur_robot_driver

Contents:

  • Overview
    • Feature list and roadmap
  • Installation
    • Installation of the ur_robot_driver
    • Setting up a UR robot for ur_robot_driver
  • Usage
    • Startup the driver
    • Move the robot
    • Controllers
    • Simulation
    • Sending URScript code to the robot
    • Quick start
    • Robot frames
    • Troubleshooting
  • Operation modes
    • Robot’s control modes
    • Driver’s operation modes
  • Setting up the tool communication on an e-Series / UR Series robot
    • Robot setup
    • Setup the ROS side
  • UR Hardware interface
    • Supported control modes
    • Interacting with the hardware interface
  • UR Hardware interface parameters
    • headless_mode
    • input_recipe_filename (Required)
    • kinematics/hash (Required)
    • non_blocking_read (default: “true”)
    • output_recipe_filename (Required)
    • reverse_port (Required)
    • robot_ip (Required)
    • script_filename (Required)
    • script_sender_port (Required)
    • servoj_gain (Required)
    • servoj_lookahead_time (Required)
    • tool_baud_rate (Required)
    • tool_parity (Required)
    • tool_rx_idle_chars (Required)
    • tool_stop_bits (Required)
    • tool_tx_idle_chars (Required)
    • tool_voltage (Required)
    • use_tool_communication (Required)
  • Dashboard client
    • Advertised Services
    • Parameters
  • Robot state helper
  • Controller stopper
    • Parameters
  • Trajectory until node
    • Action interface / usage
    • Implementation details
  • Migration notes
    • Iron -> Jazzy
    • Kilted -> Lyrical
    • Lyrical -> Maoka
Previous Next

© Copyright 2024, Universal Robots A/S.

Built with Sphinx using a theme provided by Read the Docs.
ROS 2 Rolling
Versions
Jazzy
Kilted
Rolling