Migration notes
Iron -> Jazzy
keep_alive_count -> robot_receive_timeout
Doing real-time control with a robot requires the control pc to conform to certain timing
constraints. For this keep_alive_count was used to estimate the tolerance that was given to the
ROS controller in terms of multiples of 20 ms. Now the timeout is directly configured using the
robot_receive_timeout parameter of the hardware interface.
ros2_control xacro tag moved to driver package
The description package no longer adds the ros2_control tag to the robot’s URDF. This is done
in the driver now. Therefore, there is a urdf folder containing the macro for generating a
ros2_control tag and a ready-to-use xacro file for a UR robot with a ros2_control tag.
If you want to create your own controlled robot, you should mimic that structure, as done e.g. in the custom_workcell_tutorial.
robot_description is now distributed by the robot_state_publisher
The robot_description isn’t propagated to all interested parties as a parameter. Instead, only
the robot_state_publisher is provided with the parameter, republishing it on the
robot_description topic.
Therefore, there is a new launchfile ur_rsp.launch.py which takes care about loading the
description and starting the robot_state_publisher. If you create a description that needs
other parameters than the packaged one, you can write your own rsp launch file and pass that as
description_launchfile argument to ur_control.launch.py.
Enforce absolute paths in launchfiles
All launchfiles now expect an absolute path for files that should be used to alter the launch
process (e.g. description file, controllers file). Before it was expecting e.g. a
description_package and a description_file argument with a relative path to the package.
The default files have not been changed, so unless you specified your custom package / file combinations, you will need to update that to an absolute path.
Absolute paths can still be generated dynamically using a package + relative path structure inside
other launchfiles or by using ros2 pkg prefix on the command line. For example, you can do
$ ros2 launch ur_robot_driver ur_control.launch.py ur_type:=ur20 robot_ip:=192.168.56.101 \
kinematics_params_file:=$(ros2 pkg prefix my_robot_cell_control)/share/my_robot_cell_control/config/my_robot_calibration.yaml
Removal of ros2_control_node
The ros2_control_node has been removed from the driver in #939. Instead, the
ur_control.launch.py launchfile now uses the controller_manager’s ros2_control_node
directly. This change is only relevant if you wrote your own launchfile starting the
ur_robot_driver’s ros2_control_node. In that case, you should adapt your launchfile to use
the controller_manager’s ros2_control_node instead. Remember to also remove the
robot_description parameter as explained above.
ur_control_node = Node(
- package="ur_robot_driver",
- executable="ur_ros2_control_node",
+ package="controller_manager",
+ executable="ros2_control_node",
parameters=[
- robot_description,
update_rate_config_file,
ParameterFile(initial_joint_controllers, allow_substs=True),
],
Kilted -> Lyrical
Removal of scaled_joint_trajectory_controller
Since the scaled_joint_trajectory_controller has been removed in ROS Lyrical Luth, the default
controller is now the joint_trajectory_controller. The reason for this is the scaling capabilities now has been merged upstream to joint_trajectory_controller. Thus, making the scaled_joint_trajectory_controller redundant.
User applications will most likely have to change the target action server for execution motions
scaled_joint_trajectory_controller/follow_joint_trajectory -> joint_trajectory_controller/follow_joint_trajectory
In custom controller specification files it is enough to change the controller type and the speed scaling state interface parameter. Go from
controller_manager:
ros__parameters:
my_traj_controller:
type: ur_controllers/ScaledJointTrajectoryController
my_traj_controller:
ros__parameters:
speed_scaling_interface_name: $(var tf_prefix)speed_scaling/speed_scaling_factor
to
controller_manager:
ros__parameters:
my_traj_controller:
type: joint_trajectory_controller/JointTrajectoryController
my_traj_controller:
ros__parameters:
speed_scaling:
state_interface: $(var tf_prefix)speed_scaling/speed_scaling_factor
Automatic robot model verification at startup
In Lyrical, the robot model is automatically verified at startup. The robot model will be queried from the connected robot and compared to the robot model specified in the URDF. If the models do not match, configuring the hardware will fail and an error will be logged.
This feature is enabled by default, but can be disabled by setting the verify_robot_model
parameter to false in the hardware configuration file. For example, the following command will
launch the driver without verifying the robot model:
ros2 launch ur_robot_driver ur_control.launch.py \
robot_ip:=192.168.56.101 \
ur_type:=ur18 \
verify_robot_model:=false
Note
This feature is also available in previous ROS distributions, but is disabled by default. It is recommended to enable this feature to ensure that the correct robot model is being used.
Lyrical -> Maoka
Blocking read enabled by default in launch files
From ROS Makoa onwards, the ur_robot_driver launch files have blocking read enabled by default.
If you want to disable this behavior, you can set the blocking_read parameter to false in your
launch file.
Note
Blocking read might not be the desired behavior in multi-robot (or multi hardware-interface)
setups, in which case you should create your own launch files anyway. This is why in the URDF
the default value of the blocking_read parameter is still false.
See Blocking read for more details on that feature.
Interface change of set_payload service
The SetPayload service in ur_msgs has changed to use geometry_msgs.msg.Inertia as the
payload field. Thus, service calls to /io_and_status_controller/set_payload have to be updated
from
ros2 service call /io_and_status_controller/set_payload ur_msgs/srv/SetPayload \
"{payload: {mass: 1.0, center_of_gravity: {x: 0.0, y: 0.0, z: 0.04}}}"
to
ros2 service call /io_and_status_controller/set_payload ur_msgs/srv/SetPayload \
"{payload: {m: 1.0, com: {x: 0.0, y: 0.0, z: 0.04}}}"
Payload inertia is now also supported, as well as a transition time:
ros2 service call /io_and_status_controller/set_payload ur_msgs/srv/SetPayload "
payload:
m: 1.0
com:
x: 0.0
y: 0.0
z: 0.04
ixx: 0.05
ixy: 0.02
ixz: 0.02
iyy: 0.05
iyz: 0.02
izz: 0.1
transition_time:
sec: 1
nanosec: 0
"