Setting up the tool communication on an e-Series / UR Series robot

Note

Currently, there seems to be issues with having the tool communication setup from this guide and the “Robotiq Grippers” URCap running in parallel. If you are planning to use the “Robotiq Grippers” URCap then currently please refrain from installing the rs485 URCap.

See this issue for details and the current state.

From the e-Series on, Universal Robots provide an rs485 based interface at the tool flange that can be used to attach an rs485-based device to the robot’s tcp without the need to wire a separate cable along the robot.

This driver enables forwarding this tool communication interface to an external machine for example to start a device’s ROS driver on a remote PC.

This document will guide you through installing the URCap needed for this and setting up your ROS launch files to utilize the robot’s tool communication.

Robot setup

For PolyScope 5, please install the rs485-1.0.urcap found in the resources folder. Installing a URCap is explained in the setup guide for the external-control URCap.

For PolyScope X, you can download the latest tool-comm-forwarder URCapX from its release page. After installation, please make sure to activate tool forwarding in the URCap’s application screen.

After installing the URCap the robot will expose its tool communication device to the network.

Note

If you cannot connect to the network-exposed tool communication port, please make sure that the robot isn’t configured to block inbound connections. To check if this is the case, go to the Hamburger Menu -> Settings -> Security -> General, and ensure port 54321 is not disabled in the fields under Inbound Connections.

Both fields can be cleared to remove all restrictions and enable all ports.

Screenshot showing the inbound connections menu screen.

Setup the ROS side

In order to use the tool communication in ROS, simply pass the correct parameters to the bringup launch files:

$ ros2 launch ur_robot_driver ur_control.launch.py ur_type:=ur5e robot_ip:=yyy.yyy.yyy.yyy use_tool_communication:=true use_mock_hardware:=false launch_rviz:=false
  # remember that your user needs to have the rights to write that file handle to /tmp/ttyUR

Following parameters can be set ur.ros2_control.xacro:

  • tool_voltage

  • tool_parity

  • tool_baud_rate

  • tool_stop_bits

  • tool_rx_idle_chars

  • tool_tx_idle_chars

  • tool_device_name

  • tool_tcp_port

The tool_device_name is an arbitrary name for the device file at which the device will be accessible in the local file system. Most ROS drivers for rs485 devices accept an argument to specify the device file path. With the example above you could run the rs485_node from the package imaginary_drivers using the following command:

$ ros2 run imaginary_drivers rs485_node --ros-args -p device:=/tmp/ttyUR

You can basically choose any device name, but your user has to have the correct rights to actually create a new file handle inside this directory. Therefore, we didn’t use the /dev folder in the example, as users usually don’t have the access rights to create new files there.

For all the other tool parameters seen above, please refer to the Universal Robots user manual.

More information can be found at Universal_Robots_ToolComm_Forwarder_URCap. The convenience script for socat call is here for ROS2 driver and can be run by:

$ ros2 run ur_robot_driver tool_communication.py --ros-args -p robot_ip:=192.168.56.101 -p device_name:=/tmp/ttyUR