Force and Torque Control

This page provides an overview of the force and torque control capabilities available in this driver. In ROS 2, joint torque control is also referred to as effort control. The driver supports both direct joint-level torque control and the robot’s built-in Cartesian force-mode control.

For position and velocity based control, see Position and Velocity Control.

For utility controllers such as freedrive, tool contact detection, and I/O control, see Utility Controllers.

Joint Torque Control

Direct joint-level torque control lets you command torque values to each of the robot’s joints. This is useful for implementing custom compliance, force control strategies, or research applications that require direct torque-level access.

Custom controllers should best be implemented as ros2_control controllers by using the driver’s exposed effort interfaces. The forward_effort_controller explained below is more of an easy-to-use example of how to send direct torque commands to the robot, rather than a building block for an application.

forward_effort_controller

Type: forward_command_controller/ForwardCommandController with interface_name: effort

This controller streams target joint efforts (torques) directly to the robot using the URScript function direct_torque(...). The robot automatically compensates for gravity, so the provided target torques should not include gravity compensation. The user is responsible for sending commands that are safe and achievable.

Note

This controller requires PolyScope >= 5.25.1 (PolyScope 5) or >= 10.12.1 (PolyScope X).

To activate this controller, deactivate any active motion controller first:

$ ros2 control switch_controllers --deactivate joint_trajectory_controller \
  --activate forward_effort_controller

The controller accepts commands on its ~/commands topic as std_msgs/msg/Float64MultiArray with one value per joint.

Warning

This controller is mutually exclusive with position and velocity controllers. Only one motion controller can be active at a time.

Note

The effort field in sensor_msgs/JointState (published by the joint_state_broadcaster) contains motor currents, not physical joint torques.

Friction Compensation

When using direct torque control, the robot’s internal friction compensation can be tuned using the friction_model_controller.

This controller sets per-joint viscous and Coulomb friction scale factors that determine how much internal friction compensation the robot applies during torque control mode. Each scale factor is in the range [0, 1], where 0 means no compensation and 1 means full compensation.

The controller exposes the ~/set_friction_model_parameters service (ur_msgs/srv/SetFrictionModelParameters) to configure these values. It is started as active by default in the driver’s launch file.

Note

The friction model controller is only relevant for effort control. While it is technically compatible with all motion controllers, adjusting friction parameters only has an effect during direct torque control.

Gravity Compensation

When the robot is mounted in a non-standard orientation, the gravity vector used for internal gravity compensation must be updated using the gravity_update_controller.

The controller exposes the ~/set_gravity service (ur_msgs/srv/SetGravity) to set the gravity direction experienced by the robot. The vector in the request points towards the Earth’s center and can be expressed in any frame transformable to the robot’s base frame. It is started as active by default in the driver’s launch file.

Force Mode Controller

The force_mode_controller provides Cartesian-space force and torque control using the robot’s built-in force mode. This interfaces the URScript function force_mode(...).

Unlike direct joint torque control, force mode operates in Cartesian space: you specify forces and torques relative to a task frame, along with a selection vector that determines which axes are force-controlled (compliant) and which remain position-controlled.

  • In compliant axes, the robot adjusts its position to achieve the specified force or torque.

  • In non-compliant axes, motion commands from the active position controller are executed normally.

Force mode can be combined with all position control modes (joint_trajectory_controller, passthrough_trajectory_controller, forward_position_controller, etc.) to execute motions under force constraints.

The controller provides two services:

  • ~/start_force_mode [ur_msgs/srv/SetForceMode]

  • ~/stop_force_mode [std_srvs/srv/Trigger]

Tip

The robot’s force/torque sensor is a relative sensor, meaning it measures changes in force and torque rather than absolute values. For best performance, zero the sensor using the ~/zero_ftsensor service on the io_and_status_controller before activating force mode and before the tool makes contact with the environment.

See the force_mode_controller documentation for full details on parameters, the service interface, and the meaning of each field.

An example demonstrating force mode usage is available at ur_robot_driver/examples/force_mode.py.

Freedrive Mode Controller

Type: ur_controllers/FreedriveModeController

Allows manually moving the robot’s joints without any active control. This controller cannot be combined with any other motion controller.

Freedrive mode is activated by publishing True messages on the ~/enable_freedrive_mode topic (std_msgs/msg/Bool). Messages must be sent continuously to keep freedrive active – if no message is received within the inactive_timeout (default: 1 second), freedrive mode is automatically deactivated.

$ ros2 topic pub --rate 2 /freedrive_mode_controller/enable_freedrive_mode \
  std_msgs/msg/Bool "{data: true}"

To deactivate, either publish False, deactivate the controller, or simply stop publishing.

See the freedrive_mode_controller documentation for full details.

Force/Torque Sensing

The robot’s TCP force/torque sensor is an independent sensing capability. It is not required for joint torque control to function. However, it can be useful alongside torque control for monitoring contact forces or implementing sensor-based control strategies.

force_torque_sensor_broadcaster

Type: force_torque_sensor_broadcaster/ForceTorqueSensorBroadcaster

Publishes the TCP wrench (forces and torques) as reported by the robot’s built-in sensor on the ft_data topic. This broadcaster is read-only and runs alongside any other controller.

The sensor can be zeroed using the ~/zero_ftsensor service on the io_and_status_controller.

Controller Compatibility

The following table summarizes how torque-related controllers can be combined:

Controller

Can combine with

forward_effort_controller

Mutually exclusive with all other joint-level motion controllers (position, velocity, trajectory).

force_mode_controller

All position control modes (joint_trajectory_controller, passthrough_trajectory_controller, forward_position_controller, etc.)

friction_model_controller

All controllers (only affects torque control behavior).

gravity_update_controller

All controllers (updates robot-internal gravity compensation).

force_torque_sensor_broadcaster

All controllers (read-only broadcaster).

Examples

force_mode.py

The ur_robot_driver/examples/force_mode.py example demonstrates how to:

  1. Switch to the passthrough_trajectory_controller and force_mode_controller

  2. Move the robot to a starting pose

  3. Activate force mode with a specified wrench, task frame, and selection vector

  4. Deactivate force mode after a set duration