Installing the Simulator
In a terminal in your IDE navigate to the ursim-polyscope directory with
cd ursim-polyscopexRun
. ./install.sh
This will install the simulator, and produce a binary executable named run-simulator
Running the simulator
You can start the simulator while in the ursim-polyscopex directory by running
./run-simulator
The simulator will then start up, and you can check it out opening your browser and visiting
Runtime parameters
It is possible to specify a specific robot type when running the simulator, using the
--robotType parameter
./run-simulator --robotType UR10
In certain situations an IT department might decide to block usage of port 80. In this case you would be blocked from accessing the default PolyScope X application port. An example of the error message could be similar to the following:
Error response from daemon: Ports are not available: exposing port TCP 0.0.0.0:80 -> 0.0.0.0:0:
listen tcp 0.0.0.0:80: bind: An attempt was made to access a socket in a
way forbidden by its access permissions.
In this case you can use the --port parameter to specify a different one
./run-simulator --port 45000
This will make PolyScope X available at http://localhost:45000.
To see the full list of supported robot types, use the help parameter --help
./run-simulator --help
Installing the SDK
In a terminal in your IDE navigate to the ursim-polyscope directory with
cd sdk-polyscopexRun
. ./install.sh
This will install the SDK, and you will be ready to start developing URCaps.