Changelog
0.12.125 - 2024-07-04
Compatible with PolyScope X 10.5.
Changed
Breaking: For
RobotPositionServicein@universal-robots/contribution-api, thegetInverseKinematicsnow needs an input argument forqNear.Breaking: Interface
FrameNamein@universal-robots/contribution-apihas been changed to a type of string.The
KinematicPositioninterface in@universal-robots/contribution-apihas been deprecated.The
Positioninterface in@universal-robots/contribution-apihas been deprecated.Revamped introduction to the SDK documentation
Added
New
Waypointtype in@universal-robots/contribution-apiwhich should be used instead of the now deprecatedKinematicPositionandPositionThe new Getting Started page guiding the user through creating their first URCap
A new more thorough guide on Working with the Simulator. There is a known issue when using the
--resetoption without--clear-applicationwhen working with the simulator described in a note in the following linked section.
Removed
Fixed
Default visibility filters for reading the Typescript APIs
0.11.95 - 2024-04-23
Compatible with PolyScope X 10.4.
Changed
Universal Robots NPM packages for the SDK is available by download and not packaged with the SDK-zip file.
Breaking: Bump
Angularfrom16.1.1to17.1.2
Added
Add Smart Skill option to the urcap generator in the SDK
Option to run the UR30 in the simulator.
Add URCap upgrade guide from v0.10 to v0.11
Removed
Breaking:
install.batfrom the SDK, directing Windows users towards DevContainers andWSL2.Documentation bundled with the SDK, it is now only available online.
Fixed
DevContainer terminal exit on commands with non 0 return code.
URProgram Node sample referenced internal component and not sample component.
URCap Generator
newurcap.shhanging during execution.Configuring DevContainer takes a long time in VS Code.
0.10.103 - 2024-01-18
Added
Document: Networking - Macvlan
Add
macvlanSDK sample
Fixed
npm run delete-urcapwould not delete a URCap including a Device
0.10.94 - 2023-12-20
Compatible with PolyScope X 10.3.
URCap development is now done inside a devContainer
Slimmed down SDK filesize
Cleaned up naming in the SDK, removed
UR+and instead usingURCap
Changed
Breaking: Renamed following packages:
Rename
LanguageSettingstoRobotSettingsRename
ProgramPresenterComponenttoProgramPresenter
Breaking: Moved following packages from
@universal-robots/contribution-typingsto@universal-robots/contribution-apiApplicationPresenter,ProgramPresenter,SmartSkillsPresenter, andSourcePresenter
Breaking: Move
WebComponentDialogComponentto sub-package@universal-robots/contribution-apiknown as@universal-robots/contribution-api/angular.Breaking: Move functions
convertValueandvalueRawConverter, from@universal-robots/utilities-units, to@universal-robots/contribution-api.Breaking: Move interface
@universal-robots/contribution-apito@universal-robots/ros2-interfacesBreaking: Rename
ApplicationAPItoApplicationPresenterAPIBreaking: Rename
ProgramAPItoProgramBehaviorApiBreaking: Rename
SmartSkillsAPItoSmartSkillsBehaviorAPIBreaking: Rename service
TreeServicetoProgramNodeServiceURCap installation guide URCap installation
Added
Document: Container cheat sheet
Document: Communicate with controller
Document: Smart Skills
Generate
requiments.txtinside URCaps. This file describes what frontend API versions is used by the URCap.Smart Skills URCap API
Add
RobotPositionServiceAdd built-in PolyScope X program nodes as samples
Add
--resetflag toURSim
Removed
Breaking: remove package
@universal-robots/contribution-typings
Fixed
hotplug devicedid not reconnect after reboothotplug devicewhere assigned to the wrong URCaphotplug devicedid not reconnect after update
0.9.27 - 2023-09-25
Changed
Breaking: Bump
Nodefrom16.14.0to18.17.1Breaking: Bump
Angularfrom14.1.1to16.1.1Breaking: In
manifest.yamlvolumeMountsare nowmounts. Seedatastoragesamples and documentation.Devices have changed to include a type instead of a specific device (e.g.
device: "ttytool:/dev/ur-ttylink"becomestype: ttyTool)
Added
For
Application nodesallow descriptive text to card inApplications menu