Communicating with the robot controller
It is possible for a backend container contribution to communicate with the robots controller using different interfaces. To establish controller communication two parts are required:
In the Manifest.yaml describe what service the container should access.
From code implement the socket communication using the service name and correct interface port number.
Controller services
These are the available services that can be reached from a container contribution.
Service |
DNS name |
Description |
|---|---|---|
Controller Primary |
urcontrol-primary |
Primary interface on controller |
Controller Secondary |
urcontrol-secondary |
Secondary interface on controller |
Controller Real-time |
urcontrol-real-time |
Real-time interface on controller |
Controller RTDE |
urcontrol-rtde |
RTDE interface on controller |
Controller interpreter |
urcontrol-interpreter |
Interpreter interface on controller |
Controller primary read-only |
urcontrol-primary-read-only |
Read-only access |
Controller secondary read-only |
urcontrol-secondary-read-only |
Read-only access |
Controller real-time read-only |
urcontrol-real-time-read-only |
Read-only access |
Container services |
servicegateway |
Ingress access to containers |
Controller ports
These are the ports needed when creating a socket from code
Interface |
Port |
|---|---|
Primary |
30001 |
Secondary |
30002 |
Realtime (Deprecated) |
30003 |
RTDE |
30004 |
Primary read-only |
30011 |
Secondary read-only |
30012 |
Realtime read-only |
30013 |
Interpreter |
30020 |
Communicating with a service
The following is snippets from the calibration-info sample, that demonstrates how to set up a backend contribution for reading the controllers primary interface.
manifest.yaml
The following shows how the backend contribution of the calibration-info sample is configured to read from the controllers primary interface.
....
containers:
- id: calibration-info
image: calibration-info:latest
services:
- service: urcontrol-primary-read-only
...
The “services” section describe what services should be made available to the contribution (see “Controller services” table). “urcontrol-primary-read-only” will allow reading from the controller primary socket
Socket implementation
When implementing the socket communication the service name from the manifest must be used as host, the port can be found in the controller ports section above. In this case the host is “urcontrol-primary-read-only” and the port for the primary interface is 30001.
....
private static final String HOST = "urcontrol-primary-read-only";
private static final int PORT = 30011;
private final Socket socket;
private final DataInput input;
public ControllerConnection() throws IOException {
socket = new Socket(HOST, PORT);
input = new DataInputStream(new BufferedInputStream(socket.getInputStream()));
}
...
Further reading
See Overview Of Client Interfaces for an overall explanation of the robots client interfaces.