PolyScope X - SDK Documentation Logo

General

  • Welcome to the Documentation
  • Setup
  • PolyScope X SDK user guide
  • Getting Started
  • How to guides
    • URCap contribution manifest
    • Communicating with the robot controller
    • Working with the PolyScope X Simulator
    • Creating a container backend Contribution
    • Creating a Frontend Contribution
    • Creating a gripper contribution
    • Enabling live development of URCapX contributions
    • Redirecting backend REST and WebSocket communication during URCap development
    • ROS2 - Backend Contribution
    • ROS2 - Frontend Contribution
    • UI Design Library
    • URCap Contribution Generator
    • Working With Units
    • Data storage
    • Modifying pre-installed files in a container
    • Networking - Macvlan
    • Persisting Data
    • Serial communication via the Tool Connector
    • USB - Hot plug
    • Smart Skills Contributions
    • Sidebar Contributions
      • What is the Sidebar?
      • How to add a Sidebar Item to a Front-end Contribution?
        • 1. Add the Folders and Files
        • 2. Add the Behavior
        • 3. Add the sidebar item to the app.module.ts:
        • 4. Add the translations for your new sidebar item in the en.json:
        • 5. Add the webcomponent files
        • 6. Add the contents to gripper-sidebar-item.component.ts
        • 7. Add the presenter to the App
        • 8. Edit the contribution.json file to include the sidebar item:
    • Operator Screen Contributions
    • Docker cheat sheet
    • CPU architecture and container compatibility
  • Resources
  • Design Guidelines

Appendix

  • Changelog
  • License
PolyScope X - SDK Documentation
  • How to guides
  • Sidebar Contributions

Note: You are viewing documentation for version SDK-v0.17. The latest version is SDK-v0.22.

Sidebar Contributions

What is the Sidebar?

The sidebar is a quickly accessible part of the interface, useful for many different, often used functions. Some of the built-in functionalities you will find in the sidebar, include the ability to jog the robot, see information about global variables and navigate the program tree while setting up your program.

The API to contribute a sidebar item means that your URCap will be able to provide quick access to various functions of your software, be that opening and closing a gripper, quickly reconfiguring a pallet or providing guidance to programmers or operators.

Creating a sidebar item is very similar to the process of creating any other URCap contribution in Polyscope X, so if you have already created a program node, application node or smart skill, the following instructions should feel quite familiar.

How to add a Sidebar Item to a Front-end Contribution?

If you have a URCap that does not contain a sidebar item you can add one by following these steps:

1. Add the Folders and Files

Add a folder to your frontend where you store your sidebar item(s), and add the sidebar item behavior worker TS file to that folder. In our example we call our folder gripper-sidebar-item and likewise for the behavior worker (it is not required that the folder and the behavior worker are named the same):

└─ src
   ├─ app
   │  ├─ app.module.ts
   │  └─ components
   │     ├─ gripper-program-node
   │     │  ├─ gripper-program-node.behavior.worker.ts
   │     │  ├─ gripper-program-node.component.html
   │     │  ├─ gripper-program-node.component.ts
   │     │  └─ gripper-program-node.node.ts
   │     └─ gripper-sidebar-item
   │        └─ gripper-sidebar-item.behavior.worker.ts
   ├─ assets
   │  ├─ i18n
   │  └─ icons
   ├─ contribution.json
   ├─ index.html
   ├─ main.ts
   └─ styles.scss

2. Add the Behavior

Add the default behavior to the empty gripper-sidebar-item.behavior.worker.ts file:

import { registerSidebarBehavior, SidebarItemBehaviors } from '@universal-robots/contribution-api';

const behaviors: SidebarItemBehaviors = {
    // factory is required
    factory: () => {
        return { type: 'gripper-sidebar-item', version: '1.0.0' };
    },
};

registerSidebarBehavior(behaviors);

3. Add the sidebar item to the app.module.ts:

registerWorkersWithWebPack() {
    ...
    new Worker(new URL('./components/gripper-sidebar-item/gripper-sidebar-item.behavior.worker.ts' /* webpackChunkName: "gripper-sidebar-item.worker" */, import.meta.url), {
        name: 'gripper-sidebar-item',
        type: 'module',
    });
}

4. Add the translations for your new sidebar item in the en.json:

{
  "sidebar-items": {
    "gripper-sidebar-item": { //Note that this _MUST_ match the componentTagName found in contribution.json
      "title": "Gripper"
    }
  }
}

5. Add the webcomponent files

Add the *.html, *ts and optionally the *.scss styles file.

└─ gripper-sidebar-item
   ├─ gripper-sidebar-item.behavior.worker.ts
   ├─ gripper-sidebar-item.component.html
   ├─ gripper-sidebar-item.component.scss
   └─ gripper-sidebar-item.component.ts

6. Add the contents to gripper-sidebar-item.component.ts

import { ChangeDetectionStrategy, Component, Input } from '@angular/core';
import { SidebarItem, SidebarItemPresenter, SidebarPresenterAPI } from '@universal-robots/contribution-api';

@Component({
    templateUrl: './gripper.component.html',
    styleUrls: ['./gripper.component.scss'],
    changeDetection: ChangeDetectionStrategy.OnPush,
})
export class GripperComponentSidebarItem implements SidebarItemPresenter {
    @Input()
    instance: SidebarItem;

    @Input()
    presenterAPI: SidebarPresenterAPI;
}

7. Add the presenter to the App

In the app.module.ts add the creation of the web-component:

ngDoBootstrap() {

    ...

    customElements.define(
        'gripper-component-sidebar-item',
        createCustomElement(GripperComponentSidebarItem, { injector: this.injector })
    );
}

8. Edit the contribution.json file to include the sidebar item:

{
    "sidebar": [
        {
            "name": "gripper-sidebar-item",
            "iconURI": "assets/icons/gripper-icon.svg",
            "presenterURI": "main.js",
            "behaviorURI": "gripper-sidebar-item-behavior-worker.js",
            "translationPath": "assets/i18n/",
            "componentTagName": "gripper-sidebar-item",
            "size": "large"
        }
    ]
}

Rebuild and reinstall the URCap with the new sidebar item presenter and look for the Gripper icon in the sidebar!

Previous Next

© Copyright 2026, Universal Robots A/S.

Other Versions v: SDK-v0.17
Tags
SDK-v0.14
SDK-v0.15
SDK-v0.16
SDK-v0.17
SDK-v0.18
SDK-v0.19
SDK-v0.20
SDK-v0.21
SDK-v0.22 (latest)