My first URCap Guide

Before you start

Make sure you have followed the steps during Setup. This should set you up with the running DevContainer inside VS Code or IntelliJ.

Important

For the best experience it is recommended that you already have some knowledge about Angular, TypeScript, HTML, CSS, URScript and Robot programming, but even without these skills you should be able to follow this guide and have your first URCap running in the simulator.

Angular Docs
Typescript Docs
HTML Docs

Tip

It is possible to follow this guide using the No Install SDK on GitHub. The Resource page provides direction to the appropriate GitHub repository.

Goal of this Guide

This guide should help you to understand the basic concept of URCap development with the PolyScope X SDK. Within this project you will create a simple URCap that allows to turn on a digital output for a certain amount of time. From the program node the user will define: how long the digital output will turn True and which output should light up. Therefore, the program node will contain two controls for these inputs. The generated URScript Code should then perform the desired action. The URCap will be named “LightUp”.

Note

As we progress through this guide, we will be iterating over the code examples throughout the section. This iterative process is designed to enhance your understanding and application of the concepts. However, due to this iterative approach, the code snippets will differ from the full code provided at the end of the section.

The finished ProgramNode should look like this:

LightUp

Create New URCap Project

First you are going to create a new URCap Project.

All commands provided in this guide should be typed into the Terminal of your IDE.

Bring up your Terminal with CTRL + J or ⌘ + J

Create new URCap with:

./newurcap.sh

This will open a new Dialog in the Terminal to define your URCap Project. The first questions are mandatory and concern vendor and URCap details. It is required to choose a vendor name and a vendor ID. The ID and name should represent the company developing the URCap.

? Name of Vendor Sample Company
? Id of Vendor sample-company

Note

Be aware that the sample files at the bottom of the page expects sample-company. This means that if you choose another name then it needs to be appropriately changed in the ‘ngDoBootstrap()’ function in app.module.ts and createProgramNode in light-up-program.behavior.worker.ts

Similar to the vendor name and ID, the name and ID for the URCap needs to be defined. The ID is also defining the path of the URCap Project.

? Name of URCap Contribution Light Up
? Id of URCap Contribution light-up

Then it asks if a frontend should be generated.

? Do you want to include a Web frontend (Y/n) y

The next prompt will ask if a Docker Container (backend) should be included. For the LightUp URCap, no Docker Container is needed as it does not need any backend processes to work. Inside such a Docker Container it would be possible to run code in a different programming language than TypeScript (e.g. Python or C++). This is useful for certain applications where code already exists in these languages or where communication between devices is needed. More on this topic can be found under Creating a container backend Contribution.

? Include a Docker Container Contribution (backend) (Y/n) n

When asked if Angular or JavaScript should be used, choose the Option Angular.

? What type of URCap Web contribution should be created? (Use arrow up/down keys)
❯ Angular

For the Light Up URCap a Program Node is necessary, therefore choose to include one. A Program Node is the part of the URCap that can actually be inserted into the Program Tree of a Robot Program. As with the prompts before, we need to assign a name to the node. For this sample we can use the following scheme:

? Include Program Node (Y/n) Y

? Name of Program Node light-up-program

Then it will ask if an Application Node should be included. In our case we do not need an Application Node.

? Include Application Node (Y/n) n

Then next questions are if a SmartSkill, Sidebar and Operatorscreen should be included. In this example they are not needed.

? Include Smart Skill (Y/n) n
? Include Sidebar (Y/n) n
? Include Operator screen (Y/n) n

After finishing the dialog the URCap project will be created in a new folder with the name ‘light-up’.

Build your URCap

To build your blank project you need to navigate into your URCap project folder.

cd light-up/

Inside the folder you will need to install all required dependencies. This step only needs to be done once or as soon as the project dependencies change. To do so use this command:

npm install

Warning

Should this command take longer than a couple of minutes and you are working on Windows, make sure that you have followed the steps from WSL-Setup

To build your URCap you need to execute the build command. During that command your URCap will be packaged and the URCapX file will be created. This command needs to be executed every time you want to apply you changes made to the URCap.

npm run build

After successful completion of the build process you should find your ‘light-up-1.0.0.urcapx’ file in the folder ‘ light-up/target’. You could now deploy this file to a PolyScope X Robot.

Install your URCap on URSim

While developing it is easiest to work with the integrated Simulator of PolyScope X. To deploy the URCap to the Simulator use the following command:

#Port is an optional flag.
npm run install-urcap [-- --port <PORT>]

#Your command might look like this
npm run install-urcap -- --port 45000

Tip

Should you run the URSim on a port different than 80 you will need to provide the used port with – –port

To check if the URCap is installed correctly you can Navigate to your Simulator in Chrome via localhost:80 or localhost:YourPort if you are not running on Port 80.

In PolyScope X open the hamburger menu in the upper-left corner and click on System Manager to check the installed URCaps. Your URCap should now be listed here.

Check Installed URCaps

Overview of the Project Structure

The following is a simplified way to help you get started with interpreting the project structure that has just been created. Inside your Dev Container the Project should look something like this:

Project Structure

app.module.ts can be seen as the entry point of your URCap. Inside here all URCap Components are declared. In this case the light-up-program.component.ts is declared. The light-up-program.component.ts is the Angular Component that is used for the Frontend. Inside this file the behavior of the UI can be defined. An Angular Component always consists of such a [...].component.ts, which also contains HTML Code and CSS Code. HTML is used to define the Elements that will be displayed on our UI and with CSS you can define how these HTML Elements should be painted and styled.

Note

At the bottom of this guide you will be able to find the full code for the URCap inside the appropriately named files.

In the case of our autogenerated URCap project, both CSS and HTML are in external files(light-up-program.component.html and light-up-program.component.scss). The HTML and CSS Code could also be “in-line” by including these inside the component.ts directly without referencing to these files. For larger HTML Templates and Style files it is recommended to declare them in their own external files. This should be the standard setup for your URCaps.

Snippet from light-up-program.component.ts
@Component({
    templateUrl: './light-up-program.component.html',
    styleUrls: ['./light-up-program.component.scss'],
    changeDetection: ChangeDetectionStrategy.OnPush,
})

export class LightUpProgramComponent implements OnChanges, ProgramPresenter {

Adding Controls to HTML

The first step will be to add the desired UI elements to our HTML code. In the first step we will not handle any user input. The UI elements needed for this project will be a Slider to choose the time the output should light up for and a dropdown menu to choose the output.

Slider

The Slider in the UR Storybook looks good, however it only allows for selection between 1-100. There is currently no option for selecting a min and max value. Therefore, we will use a standard HTML Component and apply styling so that it looks exactly like the UR Slider. The HTML Code below will render a simple slider with selectable values from 1 to 10 and with steps of 1. Feel free to change these values to your liking.

Snippet from light-up-program.component.html
    <label class="my-slider">
        <input type="range" max="10" min="1" step="1">
    </label>

After inserting the slider in this way you will notice that it does not really fit the theme of PolyScope X. Therefore we will apply correct styling to the slider in the next section.

Styling via SCSS

Styling is applied within the light-up-program.component.scss file. This file is coupled to the HTML Code in thelight-up-program.component.ts. To Style your HTML Elements either CSS or SCSS are used. SCSS is a CSS preprocessor that extends regular CSS with features like variables, nesting, and mixins. It helps developers write cleaner, more organized stylesheets. SCSS files are compiled into standard CSS for use in web development.

We want to add the following styling to the slider.

Snippet from light-up-program.component.scss
.my-slider {    
    height: 40px;
    padding: var(--spacing-04);
    box-sizing: border-box;
    background-color: var(--color-background-interactive-default);
    border-radius: var(--border-radius-medium);
    border: 1px solid var(--color-border-default);
    display: flex;
    align-items: center;
    justify-content: center;
    input {
      appearance: none;
      cursor: pointer;          
    }

    ::-webkit-slider-runnable-track{
      background: var(--color-background-interactive-active);
      height: var(--spacing-01);
      -webkit-appearance: none;
      opacity: .6;
    }

    ::-webkit-slider-thumb{
      height: 22px;
      width: 22px;
      border-radius: var(--border-radius-large);
      background: var(--color-background-level-07);
      border: 1px solid var(--color-border-default);
      -webkit-appearance: none;
      margin: -10px 0 0;
    }
}

Generating a new URCap the default styling should look similar to the following code snippet. Where display: flex will make sure that the elements are placed next to each other “inline” and align-items: center will make sure all elements are vertically aligned. The styling for the slider should be inserted within the curly braces of the .inline-component {}. It can be added anywhere inside but doing so below the gap: var(--spacing-03); similarly to the following code snippet will apply the correct styling.

Snippet from light-up-program.component.scss
.inline-component {
  display: flex;
  align-items: center;
  height: 40px;
  gap: var(--spacing-03);
  
  .my-slider {    
    ...
  }
}

Applying those changes will result in both the slider and the dropdown being rendered next to each other and already looking good. Nonetheless, you will notice a lack of functionality, especially the slider since it does not provide any feedback of its current position. The next section will explore how to add more functionality to the URCap.

Saving the State of the ProgramNode

Saving the State of the DropDown Menu

Right now when the user changes ProgramNodes or loads a saved program, all the selections made in the ProgramNode are lost. To save these changes, the first step is to bind properties of your HTML Elements to your .component.ts. We start by binding an array of options and event listeners to the dropdown menu.

Snippet from light-up-program.component.html
    <ur-dropdown
        [options]="outputs"
        [label]="'Digital Output'"
        [placeholder]="'- Select -'"
        [selectedOption]="output"
        (selectionChange)="selectionChange($event)"
    ></ur-dropdown>

outputs will bind to an array of outputs in our .component.ts. selectedOption provides the tools to be able to set the selected output, for example when initializing the program node. We will utilize the selectionChange event to get notified when the user changes the desired output.

First we will add the properties outputs and output to our .component.ts. To achieve this just add these two lines above the constructor:

Snippet from light-up-program.component.ts
    private outputs = ["DO 0", "DO 1", "DO 2", "DO 3", "DO 4", "DO 5", "DO 6", "DO 7"];
    private output : string;

    constructor(
        ...

The array of options is now declared statically in our component and bound to our HTML Code. This is a simple implementation and more dynamic options would be possible as well.

Now the events need to be bound to a method in our component class (component.ts). This is done by declaring a method with the name selectionChange. Custom methods are usually declared after the ngOnChanges() method.

Snippet from light-up-program.component.ts
    selectionChange($event){
        console.log($event);
    }

In the first step we just want to print out the $event object into the console to observe what kind of value it returns. After building and installing the current version of the URCap, open the developer tools in Chrome by pressing F12 or opening it manually via the hamburger menu on the top right >> more tools >> developer tools. This will bring up the developer tools that are useful when developing and debugging URCap projects. Changing the digital output in the dropdown menu should now print out the selected output as a string, for example DO 0.

Warning

Make sure to refresh F5 your browser window after installing a new URCap to apply the changes.

Now, you have successfully linked the event to a method in your component class. However, the value is not saved because the method currently only prints the selected value to the console. This is where the last two files in the light-up-program folder come into play.

light-up-program.node.ts is an interface representing all the data and parameters that the program node consists of. Considering the layout of the LightUp Project, two parameters need to be added: the time to light up and the digital output that is selected. To add these to your .node.ts should look something like this:

light-up-program.node.ts
import { ProgramNode } from '@universal-robots/contribution-api';

export interface LightUpProgramNode extends ProgramNode {
    type: string;
    parameters: {
        digitalOutput: number;
    };
    lockChildren?: boolean;
    allowsChildren?: boolean;
}

Both parameters are added as numbers, which ensures easy usage in the URScript generation later. When saving the node like this, VS Code will mark the light-up-program.behavior.worker.ts red as there are now errors. By navigating to this file, you will see exactly where the error is. When you move the cursor over parameters:, which is underlined in red, an explanation for the issue will appear. Here in the createProgramNode method a new instance of the LightUpProgramNode is created and the previously defined parameter needs to be initialized as it is required. To initialize the parameters, change the method like this:

Snippet from light-up-program.behavior.worker.ts
const createProgramNode = async (): Promise<LightUpProgramNode> => ({
    type: 'sample-company-light-up-light-up-program',
    version: '1.0.0',
    lockChildren: false,    
    allowsChildren: false,
    parameters: {
        digitalOutput:0
    },
});

The .behavior.worker.ts will be of more relevance later. In the previous steps we added all the necessary parts to be able to store the state. Next the actual save operation needs to be implemented.

Back at the component class in the selectionChange($event) method the selected output can be stored in the parameter of the node like this:

Snippet from light-up-program.component.ts
    selectionChange($event){
        this.contributedNode.parameters.digitalOutput = this.outputs.indexOf($event);
        this.saveNode();
    }

this.contributedNode will resolve to the underlying node, in this case the light-up-program.node. This gives access to the parameter digitalOutput defined previously. As observed earlier $event returns a string like DO 0, but our defined parameter only accepts a number like 0. In this example this number is pulled by getting the index of the array outputs that matches the current selected output. By calling saveNode() the current state of the node is automatically saved. This method should already be present and was generated by newurcap.sh.

This concludes all the steps needed to save the selected output once it was set. The last step is to also load the state when the node is opened and the UI gets initialized. To do that just add the last if-statement shown in below code to the ngOnChanges() method. This will set the output to the corresponding element from the outputs array, depending on the saved value or to the output 0 if no value has been saved previously.

Snippet from light-up-program.component.ts
    ngOnChanges(changes: SimpleChanges): void {
        if (changes?.robotSettings) {
            if (!changes?.robotSettings?.currentValue) {
                return;
            }

            if (changes?.robotSettings?.isFirstChange()) {
                if (changes?.robotSettings?.currentValue) {
                    this.translateService.use(changes?.robotSettings?.currentValue?.language);
                }
                this.translateService.setDefaultLang('en');
            }

            this.translateService
                .use(changes?.robotSettings?.currentValue?.language)
                .pipe(first())
                .subscribe(() => {
                    this.cd.detectChanges();
                });
        }
        
        if (changes?.presenterAPI && this.presenterAPI) {
            this.output = this.outputs[this.contributedNode.parameters.digitalOutput];
        }
    }

Important

Before continuing, make sure that the node indeed preserves its state successfully. If the selected output is saved correctly, it is recommended to try to implment saving
for the Slider without checking the next section.

Saving the State of the Slider

Similar to how the state is saved for the dropdown, the state of the slider is saved as well. One difference is that the slider does not have a predefined way of showing the current selected value. For that a simple span element is added to display the value at all times. Again the first step is to bind the properties from HTML to the component class.

Snippet from light-up-program.component.html
    <span>Time to Light Up:</span>
    <label class="my-slider">
        <input type="range" max="10" min="1" step="1" [(ngModel)]="lightUpTime" (change)="afterLevelChange()">
    </label>
    <span>{{ lightUpTime }}s</span>

The first span element is just to show the user what the slider will do. The second one shows the selected time in seconds.

The [(ngModel)] directive is a two-way binding in angular. When you use [(ngModel)], changes in the UI automatically update the corresponding component property, and vice versa. It combines both one-way binding [] (from component to view) and event binding () (from view to component) into a single syntax. In this case the lightUpTime property on the component class and on the view component will always be in sync.

Important

To use the [(ngModel)] directive it is needed to import the Angular FormsModule. This should be done in the app.module.ts.

To add this import it is crucial to understand the functionality of the app.module.ts. The app module is the root module of your component and bootstraps your components. It contains the following:

  • Declarations: This section lists the components, directives, and pipes that belong to this module.

  • Imports: Here, you import other modules that your app depends on. For example, the BrowserModule is essential for running your app in a web browser.

  • Providers: Is where Services can be injected via dependency injection.

Therefore, we want to add the FormsModule to the Imports section of our AppModule.

Snippet from app.module.ts
// [...]
import { FormsModule } from '@angular/forms';  //import
// [...]
@NgModule({
    declarations: [
        LightUpProgramComponent
    ],
    imports: [
        BrowserModule,
        BrowserAnimationsModule,
        UIAngularComponentsModule,
        HttpClientModule,
        FormsModule, //FormsModule for use of TwoWayBinding
        TranslateModule.forRoot({
            loader: { provide: TranslateLoader, useFactory: httpLoaderFactory, deps: [HttpBackend] },
            useDefaultLang: false,
        })
    ],
    providers: [],
})

Now, due to the Two-Way Binding every change will update our span element.

As we don’t want to save the parameters with multiple saveNode calls every time the user moves the slider, we utilize the change() event as well. This will only call our afterLevelChange() method when the user lets go of the pressed element, thereby selecting the final value.

Next the lightUpTime property needs to be created in the component class:

Snippet from light-up-program.component.ts
    private outputs = ["DO 0", "DO 1", "DO 2", "DO 3", "DO 4", "DO 5", "DO 6", "DO 7"];
    private output : string;
    private lightUpTime : number;

    constructor(
        ...

Again add the parameters to both the .node.ts and the .behavior.worker.ts.

light-up-program.node.ts
import { ProgramNode } from '@universal-robots/contribution-api';

export interface LightUpProgramNode extends ProgramNode {
    type: string;
    parameters: {
        lightUpTime: number;
        digitalOutput: number;
    };
    lockChildren?: boolean;
    allowsChildren?: boolean;
}

And:

Snippet from light-up-program.behavior.worker.ts
const createProgramNode = async (): Promise<LightUpProgramNode> => ({
    type: 'sample-company-light-up-light-up-program',
    version: '1.0.0',
    lockChildren: false,    
    allowsChildren: false,
    parameters: {
        lightUpTime:1,
        digitalOutput:0
    },
});

Finally, the called method afterLevelChange() should be created and the Slider initialized in the ngOnChanges() Method.

Snippet from light-up-program.component.ts
    afterLevelChange(){
        this.contributedNode.parameters.lightUpTime = this.lightUpTime;
        this.saveNode();
    }
Snippet from light-up-program.component.ts
    ngOnChanges(changes: SimpleChanges): void {
        ...
        if (changes?.presenterAPI && this.presenterAPI) {
            this.output = this.outputs[this.contributedNode.parameters.digitalOutput];
            this.lightUpTime = this.contributedNode.parameters.lightUpTime;
        }
    }

This should result in both the slider and the dropdown menu preserving their state. You might notice a less than ideal behavior of the span element. This following styling makes certain the span does not wrap upon white spaces and should be added at the bottom of the inline-component:

Snippet from light-up-program.component.html
.inline-component {
  ...
  span {
    padding-right: 0.5rem;
    white-space: nowrap;
  }
}

This concludes the Section about saving values in an URCap.

Adding URScript Code

Now that the URCap is saving its current state, however on program execution the output does not turn True. This will change by adding URScript Code to the URCap.

Adding ScriptCode to the URCap is done within the light-up-program.behavior.worker.ts. This is the only file needed for this section. Within this class we have access to the ScriptBuilder(). This ScriptBuilder allows contributing lines of ScriptCode to the program that will be generated at the position of the URCapNode’s placement within the program tree.

The code below shows how to add this ScriptBuilder. For this sample we will work with the generateScriptCodeBefore method. Within the scope of this function we have access to the LightUpProgramNode and therefore to both parameters, digitalOutput and lightUpTime.

With builder.addStatements() script lines can be added. In this sample URScript Code similar to this should be generated:

set_standard_digital_out(0, True)
sleep(5)
set_standard_digital_out(0, False)

The values for sleep and the digital_out to light up should be chosen by the saved values in the node.

Snippet from light-up-program.behavior.worker.ts
const generateScriptCodeBefore = async (node: LightUpProgramNode): Promise<ScriptBuilder> => {
    const builder = new ScriptBuilder();
    builder.addStatements(`set_standard_digital_out(${node.parameters.digitalOutput}, True)`);
    builder.sleep(node.parameters.lightUpTime);
    builder.addStatements(`set_standard_digital_out(${node.parameters.digitalOutput}, False)`);
    return builder;
};

Tip

If this structure looks unfamiliar it might help to look up “Arrow functions in TypeScript”.

Now the correct script code will be executed and the URCap should work.

Adding Validation

It is recommended to require the user to make a conscious decision and force the user to select an Output instead of predefining one. This is what will be added with a validation step. First we make the digitalOutput parameter optional by adding a ? to the declaration.

Snippet from light-up-program.node.ts
export interface LightUpProgramNode extends ProgramNode {
    type: string;
    parameters: {
        lightUpTime: number;
        digitalOutput?: number;
    };
    lockChildren?: boolean;
    allowsChildren?: boolean;
}

Further the predefined value set inside the .behavior.worker.ts needs to be removed. Only the slider will receive a predefined value now.

Snippet from light-up-program.behavior.worker.ts
const createProgramNode = async (): Promise<LightUpProgramNode> => ({
    type: 'sample-company-light-up-light-up-program',
    version: '1.0.0',
    lockChildren: false,    
    allowsChildren: false,
    parameters: {
        lightUpTime:1
    },
});

To set the Node to inValid and paint it yellow in PolyScope, the validator needs to be added. This can be done within the validate function inside the .behavior.worker.ts. With the code below, the parameter will be checked. If it is not undefined, it will return a ValidationResponse with the isValid property set to true; otherwise, it will return false.

Snippet from light-up-program.behavior.worker.ts
const validate = async (node: LightUpProgramNode, context: ValidationContext): Promise<ValidationResponse> => ({ 
  isValid: node.parameters.digitalOutput !== undefined 
});

Now the component class will also receive an undefined value for digitalOutput. This will cause an unhandled error without further changes. To catch this case, one option is to check if this value is undefined and react on this case. To do so change the initialization of the UI inside the component class like this.

Snippet from light-up-program.component.ts
        if (changes?.presenterAPI && this.presenterAPI) {
            this.lightUpTime = this.contributedNode.parameters.lightUpTime;
            this.output = this.contributedNode.parameters.digitalOutput !== undefined
                ? this.outputs[this.contributedNode.parameters.digitalOutput] : "";
        }

Now if the value is undefined it will set the output to "". In case the [selectedOption] property on the ur-dropdown element receives an empty string, it will display the string attached to the placeholder property.

Adding a Dynamic Label to the ProgramNode

The final step to complete a full URCap is to add a label representing the URCap Node’s current state. This allows users to quickly see the actions that will be executed by the node at a glance.

The block of code below will first check whether digitalOutput is defined and depending on that either displays DO not defined or a combination of the digital out and the time it will light up for.

Depending on if it is one second or multiple seconds, the text changes as well. This is stored in timeUnit.

Snippet from light-up-program.behavior.worker.ts
const createProgramNodeLabel = async (node: LightUpProgramNode): Promise<string> => {
    if(node.parameters.digitalOutput !== undefined){
        const timeUnit = node.parameters.lightUpTime === 1 ? 'second' : 'seconds';    
        return `DO ${node.parameters.digitalOutput} for ${node.parameters.lightUpTime} ${timeUnit}`;
    }
    return `DO not defined`;
};

Success!

Now the LightUp URCap is finished and should work! Now is the time to explore what else is possible with PolyScope X SDK by looking through the different other guides or by exploring the provided samples bundled within the SDK.

CheatSheet

Used inside the SDK Folder to create a new URCap Project.

./newurcap.sh

Install dependencies in URCap Project. Only needed when changing dependencies or upon the first time.

npm install

Run the build process of an URCap. This will generate the URCap as .urcapx file inside the ./target folder. That file can then be installed on a robot.

npm run build

Install URCap remotely via IP&PORT. Can be used to deploy either to a URSim or to a robot in the network.

npm run install-urcap -- --host <HOST_IP> -- --port <PORT>

Used inside the URSim Folder to run the URSim. By default, will launch the URSim with Port 80. With flag –port a different port can be specified.

./run-simulator --port <PORT> 

Full Code of URCap

Below you will find the full code of the finalized URCap Project. For the best understanding of the SDK and Structure it is highly recommended to follow the Guide above fully before utilizing this source code.

app.module.ts

app.module.ts
import { DoBootstrap, Injector, NgModule } from '@angular/core';
import { LightUpProgramComponent } from './components/light-up-program/light-up-program.component';
import { UIAngularComponentsModule } from '@universal-robots/ui-angular-components';
import { BrowserModule } from '@angular/platform-browser';
import { createCustomElement } from '@angular/elements';
import { HttpBackend, HttpClientModule } from '@angular/common/http';
import { TranslateLoader, TranslateModule } from '@ngx-translate/core';
import { MultiTranslateHttpLoader } from 'ngx-translate-multi-http-loader';
import { PATH } from '../generated/contribution-constants';
import { BrowserAnimationsModule } from "@angular/platform-browser/animations";
import { FormsModule } from '@angular/forms';


export const httpLoaderFactory = (http: HttpBackend) =>
    new MultiTranslateHttpLoader(http, [
        { prefix: PATH + '/assets/i18n/', suffix: '.json' },
        { prefix: './ui/assets/i18n/', suffix: '.json' },
    ]);

@NgModule({
    declarations: [
        LightUpProgramComponent
    ],
    imports: [
        BrowserModule,
        BrowserAnimationsModule,
        UIAngularComponentsModule,
        HttpClientModule,
        FormsModule,
        TranslateModule.forRoot({
            loader: { provide: TranslateLoader, useFactory: httpLoaderFactory, deps: [HttpBackend] },
            useDefaultLang: false,
        })
    ],
    providers: [],
})

export class AppModule implements DoBootstrap {
    constructor(private injector: Injector) {
    }

    ngDoBootstrap() {
        const lightupprogramComponent = createCustomElement(LightUpProgramComponent, {injector: this.injector});
        customElements.define('sample-company-light-up-light-up-program', lightupprogramComponent);
    }

    // This function is never called, because we don't want to actually use the workers, just tell webpack about them
    registerWorkersWithWebPack() {
        new Worker(new URL('./components/light-up-program/light-up-program.behavior.worker.ts'
            /* webpackChunkName: "light-up-program.worker" */, import.meta.url), {
            name: 'light-up-program',
            type: 'module'
        });
    }
}

light-up-program.behavior.worker.ts

light-up-program.behavior.worker.ts
/// <reference lib="webworker" />
import {
    InsertionContext,
    ProgramBehaviors,
    ProgramNode,
    registerProgramBehavior,
    ScriptBuilder,
    ValidationContext,
    ValidationResponse
} from '@universal-robots/contribution-api';
import { LightUpProgramNode } from './light-up-program.node';

// programNodeLabel is required
const createProgramNodeLabel = async (node: LightUpProgramNode): Promise<string> => {
    if(node.parameters.digitalOutput !== undefined){
        const timeUnit = node.parameters.lightUpTime === 1 ? 'second' : 'seconds';    
        return `DO ${node.parameters.digitalOutput} for ${node.parameters.lightUpTime} ${timeUnit}`;
    }  
    return `DO not defined`;
};

// factory is required
const createProgramNode = async (): Promise<LightUpProgramNode> => ({
    type: 'sample-company-light-up-light-up-program',
    version: '1.0.0',
    lockChildren: false,    
    allowsChildren: false,
    parameters: {
        lightUpTime:1
    },
});

// generateCodeBeforeChildren is optional
const generateScriptCodeBefore = async (node: LightUpProgramNode): Promise<ScriptBuilder> => {
    const builder = new ScriptBuilder();
    builder.addStatements(`set_standard_digital_out(${node.parameters.digitalOutput}, True)`);
    builder.sleep(node.parameters.lightUpTime);
    builder.addStatements(`set_standard_digital_out(${node.parameters.digitalOutput}, False)`);
    return builder;
};

// generateCodeAfterChildren is optional
const generateScriptCodeAfter = async (node: LightUpProgramNode): Promise<ScriptBuilder> => new ScriptBuilder();

// generateCodePreamble is optional
const generatePreambleScriptCode = async (node: LightUpProgramNode): Promise<ScriptBuilder> => new ScriptBuilder();

// validator is optional
const validate = async (node: LightUpProgramNode, context: ValidationContext): Promise<ValidationResponse> => ({ 
  isValid: node.parameters.digitalOutput !== undefined 
});

// allowsChild is optional
const allowChildInsert = async (parent: ProgramNode, childType: string): Promise<boolean> => true;

// allowedInContext is optional
const allowedInsert = async (context: InsertionContext): Promise<boolean> => true;

// upgradeNode is optional
const nodeUpgrade = (loadedNode: ProgramNode): ProgramNode => loadedNode;

const behaviors: ProgramBehaviors = {
    programNodeLabel: createProgramNodeLabel,
    factory: createProgramNode,
    generateCodeBeforeChildren: generateScriptCodeBefore,
    generateCodeAfterChildren: generateScriptCodeAfter,
    generateCodePreamble: generatePreambleScriptCode,
    validator: validate,
    allowsChild: allowChildInsert,
    allowedInContext: allowedInsert,
    upgradeNode: nodeUpgrade
};

registerProgramBehavior(behaviors);

light-up-program.component.ts

light-up-program.component.ts
import { ChangeDetectionStrategy, ChangeDetectorRef, Component, Input, OnChanges, SimpleChanges } from '@angular/core';
import { TranslateService } from '@ngx-translate/core';
import { ProgramPresenter, ProgramPresenterAPI, RobotSettings } from '@universal-robots/contribution-api';
import { LightUpProgramNode } from './light-up-program.node';
import { first } from 'rxjs/operators';

@Component({
    templateUrl: './light-up-program.component.html',
    styleUrls: ['./light-up-program.component.scss'],
    changeDetection: ChangeDetectionStrategy.OnPush,
})

export class LightUpProgramComponent implements OnChanges, ProgramPresenter {
    // presenterAPI is optional
    @Input() presenterAPI: ProgramPresenterAPI;

    // robotSettings is optional
    @Input() robotSettings: RobotSettings;
    private _contributedNode: LightUpProgramNode;
//CHANGED
    private lightUpTime : number;
    private outputs = ["DO 0", "DO 1", "DO 2", "DO 3", "DO 4", "DO 5", "DO 6", "DO 7"];
    private output : string;

    constructor(
        protected readonly translateService: TranslateService,
        protected readonly cd: ChangeDetectorRef
    ) {
    }

    // contributedNode is optional
    get contributedNode(): LightUpProgramNode {
        return this._contributedNode;
    }

    @Input()
    set contributedNode(value: LightUpProgramNode) {
        this._contributedNode = value;
        this.cd.detectChanges();
    }

    ngOnChanges(changes: SimpleChanges): void {
        if (changes?.robotSettings) {
            if (!changes?.robotSettings?.currentValue) {
                return;
            }

            if (changes?.robotSettings?.isFirstChange()) {
                if (changes?.robotSettings?.currentValue) {
                    this.translateService.use(changes?.robotSettings?.currentValue?.language);
                }
                this.translateService.setDefaultLang('en');
            }

            this.translateService
                .use(changes?.robotSettings?.currentValue?.language)
                .pipe(first())
                .subscribe(() => {
                    this.cd.detectChanges();
                });
        }

        if (changes?.presenterAPI && this.presenterAPI) {
            this.lightUpTime = this.contributedNode.parameters.lightUpTime;
            this.output = this.contributedNode.parameters.digitalOutput !== undefined
                ? this.outputs[this.contributedNode.parameters.digitalOutput] : "";
        }
    }

//CHANGED
    afterLevelChange(){
        this.contributedNode.parameters.lightUpTime = this.lightUpTime;
        this.saveNode();
    }
    selectionChange($event){
        this.contributedNode.parameters.digitalOutput = this.outputs.indexOf($event);
        this.saveNode();
    }


    // call saveNode to save node parameters
    async saveNode() {
        this.cd.detectChanges();
        await this.presenterAPI.programNodeService.updateNode(this.contributedNode);
    }
}

light-up-program.node.ts

light-up-program.node.ts
import { ProgramNode } from '@universal-robots/contribution-api';

export interface LightUpProgramNode extends ProgramNode {
    type: string;
    parameters: {
        lightUpTime: number;
        digitalOutput?: number;
    };
    lockChildren?: boolean;
    allowsChildren?: boolean;
}

light-up-program.component.html

light-up-program.component.html
<div *ngIf="contributedNode" class="inline-component">
    <span>Time to Light Up:</span>
    <label class="my-slider">
        <input type="range" max="10" min="1" step="1" [(ngModel)]="lightUpTime" (change)="afterLevelChange()">
    </label>
    <span>{{ lightUpTime }}s</span>  
    <ur-dropdown
        [options]="outputs"
        [label]="'Digital Output'"
        [placeholder]="'- Select -'"
        [selectedOption]="output"
        (selectionChange)="selectionChange($event)"
    ></ur-dropdown>
</div>

light-up-program.component.scss

light-up-program.component.scss
@import '../../../styles.scss';

.inline-component {
  display: flex;
  align-items: center;
  height: 40px;
  gap: var(--spacing-03);

  .my-slider {    
    height: 40px;
    padding: var(--spacing-04);
    box-sizing: border-box;
    background-color: var(--color-background-interactive-default);
    border-radius: var(--border-radius-medium);
    border: 1px solid var(--color-border-default);
    display: flex;
    align-items: center;
    justify-content: center;
    input {
      appearance: none;
      cursor: pointer;          
    }

    ::-webkit-slider-runnable-track{
      background: var(--color-background-interactive-active);
      height: var(--spacing-01);
      -webkit-appearance: none;
      opacity: .6;
    }

    ::-webkit-slider-thumb{
      height: 22px;
      width: 22px;
      border-radius: var(--border-radius-large);
      background: var(--color-background-level-07);
      border: 1px solid var(--color-border-default);
      -webkit-appearance: none;
      margin: -10px 0 0;
    }
  }
  span {
    padding-right: 0.5rem;
    white-space: nowrap;
  }
}