Changelog

0.20.49 - 2026-05-29

Fixed

  • Search functionality in the TypeScript API documentation has been fixed. The fix has been backported to earlier versions of the documentation. Check it out here.

  • Issue when using the Remote Debug script in certain scenarios.

0.20.37-preview-0 - 2026-03-18

Compatible with PolyScope X 10.13.

Changed

  • Breaking: Restrict remote deployment of URCaps to External control only

  • TypeScript API: Bump Angular to version 21.0.8

  • ROS 2 Humble is replaced by Jazzy

    • Compatibility overview

      Docker Image
      (urcap_polyscopex_ros2)

      ≤ PolyScope X 10.11

      PolyScope X 10.12

      PolyScope X 10.13

      4.0.5-humble-runtime

      ✔

      ✔

      ❌

      4.1.7-humble-runtime

      ✔

      ✔

      ✔

      5.0.2-jazzy-runtime

      ❌

      ✔

      ✔

      Legend: ✔ = Works, ✔ = Works but no guarantees, ❌ = Memory leak will occur

    • AI Accelerator compatibility

      ≤ PolyScope X 10.12

      PolyScope X 10.13

      AI Accelerator 1.0.4

      ✔

      ❌

      AI Accelerator 2.0.5

      ✔

      ?

      Legend: ✔ = Works, ? = Might work, but NOT RECOMMENDED, ❌ = Memory leak will occur

Added

  • Added Development Mode for the simulator for a more frictionless experience, when developing URCaps. For details, see Working with the PolyScope X Simulator

  • Added ROS 2 Jazzy runtime image

  • TypeScript API: Added isProgramReady added to ProgramExecutionService

  • TypeScript API: Added undo to ProgramTreeService

  • TypeScript API: Added redo to ProgramTreeService

  • TypeScript API: Added canUndo to ProgramTreeService

  • TypeScript API: Added canRedo to ProgramTreeService

  • TypeScript API: Added undo, redo, load and unload to ProgramNodeLifeCycleEventType

  • TypeScript API: Added disabled to all Contribution Behaviors for dynamically hiding contributions

Removed

  • Breaking TypeScript API: Removed deprecated method setSignalValue from SourceService (use setSourceSignalValue instead)

  • Breaking TypeScript API: Removed deprecated method getSignalUpdates in SourceService (use getSourceUpdates instead)

Fixed

  • Prevent unresolved devUrl values (e.g., http://host.gateway.ip:4200/) from breaking robots.

0.19.73 - 2026-01-30

Fixed

  • When installing a URCap with npm run install-urcap --force-replace it could take multiple retries to work.

0.19.62-preview - 2026-01-09

Compatible with PolyScope X 10.12.

Added

Fixed

  • Memory leak when ROS 2 Jazzy nodes are present

    • Fixed an issue where Humble nodes could consume excessive memory and crash when communicating with Jazzy/Rolling nodes using Fast DDS. Reference: PR#130

    • Both URControl and the ROS 2 Docker base image have been updated to prevent memory leaks and improve reliability in mixed‑distribution setups.

Changed

  • API deployment of URCaps now require the target to be in remote mode. Also covered in Remote debug

  • Deprecation of ROS 2 Humble

    PolyScope X 10.12 will be the last version including ROS 2 Humble. PolyScope X 10.13 will include ROS 2 Jazzy

    • Compatibility overview

      Docker Image
      (urcap_polyscopex_ros2)

      ≤ PolyScope X 10.11

      PolyScope X 10.12

      PolyScope X 10.13

      4.0.5-humble-runtime

      ✔

      ✔

      ❌

      4.1.7-humble-runtime

      ✔

      ✔

      ?

      5.0.2-jazzy-runtime

      ❌

      ?

      ✔

      Legend: ✔ = Works, ? = Might work, ❌ = Memory leak will occur

    • Recommendation

      For URCaps including a ROS 2 node. It is recommended to build a version based on 4.1.7-humble-runtime for PolyScope X 10.12 and older releases. And build a version based on 5.0.2-jazzy-runtime for PolyScope X 10.13 and subsequent versions. The 5.0.2-jazzy-runtime will be made available as a preview before the PolyScope X 10.13 release.

0.18.97 - 2025-10-16

0.18.90-preview - 2025-09-25

Compatible with PolyScope X 10.11.

Added

  • The SDK now validates the URCap manifest.yaml against a schema.

  • Simulator support for the UR8 Long.

Changed

  • When building or installing a URCap, the manifest is validated.

    • The validation can be turned off by prefixing skip_validation to the npm command. E.g. skip_validation=true npm run build will skip the validation step

0.17.52 - 2025-08-07

0.17.47-beta - 2025-07-08

Compatible with PolyScope X 10.10.

Changed

  • Bump Angular to version 19.2.4

    • This means all packages starting with @angular should be updated to that version in package.json

  • TypeScript API: SymbolService added methods and parameters to the SymbolService to allow the easier retrieval of functions and variables:

    • Added filter parameter to getFunctionsMap to allow returning only threads or functions. If the filter is not specified, the original behaviour is kept, which is returning both.

    • Added globalVariables to get the current global variables, as return from the controller.

Added

  • Support for new Sidebar contribution including documentation, URCap sample and URCap generator support.

  • Support for new Operator Screen contribution including documentation, URCap sample and URCap generator support.

  • New Redirecting backend REST and WebSocket communication during URCap development document in the How to guides section of the SDK documentation.

  • New Modifying pre-installed files in a container document in the How to guides section of the SDK documentation.

  • TypeScript API: New MotionProfileService added for retrieving the motion profiles used in the new move nodes. The getMotionProfiles method will return the profiles for a given type.

  • TypeScript API: New TeachModeService (Experimental) added. Allows the setting and retrieving of teach mode:

    • The startTeachMode, pauseTeachMode, stopTeachMode, and resumeTeachMode methods set the state appropriately.

    • The getTeachModeState method returns the current state of teach mode.

0.16.31 - 2025-05-26

Compatible with PolyScope X 10.9.

Changed

  • The new URCap generator provided with the SDK has been rewritten as to be more robust and expandable.

Added

  • Simulator support for the UR7e, UR12e and UR15 robot types.

0.15.63 - 2025-04-07

Fixed

  • Fixed issue where the choice of robot type was ignored when starting the simulator.

0.15.59-beta - 2025-03-14

Compatible with PolyScope X 10.8.

Changed

  • Breaking: Major release of @universal-robots/ui-angular-components
    Angular Bumped from 17 to 19 (official migration guide).
    If you choose to update, the following changes are required:

    • ng command can be run with npm run ng in the devcontainer

    • Angular components are now, by default, standalone. This means that components that are part of a module must have the standalone: false property set in the @Component definition. For an example, see the application node in the gripdistance sample.

      • This also means the .eslintrc.json configuration file must be updated to not prefer standalone components (again, see the gripdistance sample for how to do this).

    • Angular-based URCaps will need to be updated with the following changes in their package.json file:

      • The domhandler package must be added with version ^5.0.3 to the peerDependencies section, due to conflicts in transitive dependencies

      • @angular/* (and related) packages must have their version updated. See below for the exact packages or the gripdistance sample for the full context:

      {
        "dependencies": {
          "@angular/animations": "19.0.5",
          "@angular/cdk": "19.0.4",
          "@angular/common": "19.0.5",
          "@angular/compiler": "19.0.5",
          "@angular/core": "19.0.5",
          "@angular/elements": "19.0.5",
          "@angular/platform-browser": "19.0.5",
          "@angular/platform-browser-dynamic": "19.0.5",
          "@angular/router": "19.0.5",
          "@universal-robots/ui-angular-components": "3.1.7",
          "zone.js": "0.15.0"
        },
        "devDependencies": {
          "@angular-devkit/build-angular": "19.0.5",
          "@angular-eslint/builder": "~19.0.2",
          "@angular-eslint/eslint-plugin": "~19.0.2",
          "@angular-eslint/eslint-plugin-template": "~19.0.2",
          "@angular-eslint/schematics": "~19.0.2",
          "@angular-eslint/template-parser": "~19.0.2",
          "@angular/cli": "19.0.5",
          "@angular/compiler-cli": "19.0.5",
          "@angular/language-service": "19.0.5",
          "ngx-build-plus": "^19.0.0",
          "typescript": "5.6.3"
        },
        "peerDependencies": {
          "domhandler": "^5.0.3"
        }
      }
      
      • If you run into issues with npm install, you might try deleting your package-lock.json.

  • TypeScript API: Enhanced updateSubTreeNode function. We have updated the updateSubTreeNode function in PolyScope X to support BranchNode objects containing a children object. This enhancement allows developers to update a program node and its children in one operation, improving efficiency and simplifying program modifications.

  • TypeScript API: SubTreeNode Interface Fix. We have updated the SubTreeNode interface in PolyScope X to correctly include BranchNode as a valid type for ProgramNode. This resolves a previous issue where BranchNode was mistakenly omitted, ensuring that developers can now work with hierarchical structures as intended.

  • TypeScript API: Enhanced SourceBehaviours` for set/get. New methods have been added to SourceBehaviours to allow a contribution to perform extra range checking and validation when using a Source in a Set and Wait node. An example of their use would to range check an analog voltage to between 0-10V.

Added

  • Added a description of communicating with the simulator in the Working with the PolyScope X Simulator document.

  • New Backend Connectivity Guide in the Getting Started section of the SDK documentation.

  • New Serial communication via the Tool Connector in the How to guides section of the SDK documentation.

  • New Design Guidelines section in the SDK documentation, providing components and tools to guide UX designers.

  • TypeScript API: New Program Node Lifecycle Hook, onLifeCycleHook, for program nodes in PolyScope X. This function allows developers to execute custom logic whenever a program node undergoes key lifecycle events, including deletion, pasting, suppression, and unsuppression.

Removed

  • Breaking: Removed deprecated methods in ProgramNodeService, refer to ProgramTreeService instead.

Fixed

0.14.74 - 2024-12-20

Compatible with PolyScope X 10.7.

Changed

  • Breaking: Changed the Analog and Digital types to represent a single IO pin in the ROS 2 urinterfaces.

    • Instead, should use the newly added AnalogIOStateStamped and DigitalIOStateStamped message types.

  • Breaking: Moved isAdvancedProgramLabel from @universal-robots/contribution-api to LabelService.

  • Breaking: Renamed isAdvancedProgramLabel to isAdvancedLabel

  • Breaking: SetAnalogOutput and SetDigitalOutput are using the same message types.

    • This will require any ROS 2 services that uses the Analog or Digital IOs to be updated.

Added

  • The following functionality have been added to the ProgramExecutionService

    • Play the currently loaded program

    • Resume a currently paused program

    • Pause a currently running program

    • Get the status of the current program

    • Step the currently running program

  • ProgramService has been added to the Presenter APIs with the functionality to:

    • Get the list of programs

    • Get the content of a specific program

    • Load a program

    • Get information about the currently loaded

  • The following methods have been added to the ProgramTreeService

    • updateSubTreeNode can update a specific node in the program tree given a node id.

    • getTreeContextFromProgramnodeById gets the tree context given a node id.

    • getContributedNodeInstancesForURCap gets the contributed node instances for the URCap that are currently inserted in the program

  • Added the AnalogStamped and DigitalStamped message types.

    • These types respectively hold the Analog and Digital values and a header.

  • Added the AnalogIO and DigitalIO message types.

    • These types are the aggregates of the vectors of the inputs and outputs.

  • Added the AnalogIOStateStamped and DigitalIOStateStamped message types.

    • These types are the aggregates of the Analog and Digital IOs e.g. control box digital IOs.

Removed

Fixed

0.13.127 - 2024-11-01

Compatible with PolyScope X 10.6.

Changed

  • Updated documentation for: “ROS 2 topics and service” and “UR interface API”.

  • Updated Node version to 20.14.

Added

  • Added default safety password to the documentation.

  • Added “Permanent” mount type, that will prevent data being deleted after a URCap is deleted.

Removed

Fixed

  • When loading a program with a custom safety, after resetting the simulator, will no longer result in an error message.

  • Fixed issue where the simulator sometimes where unable to start in Windows WSL.

  • The URCap project generator “newurcap.sh” now always presents questions in the same order.

0.12.125 - 2024-07-04

Compatible with PolyScope X 10.5.

Changed

  • Breaking: For RobotPositionService in @universal-robots/contribution-api, the getInverseKinematics now needs an input argument for qNear.

  • Breaking: Interface FrameName in @universal-robots/contribution-api has been changed to a type of string.

  • The KinematicPosition interface in @universal-robots/contribution-api has been deprecated.

  • The Position interface in @universal-robots/contribution-api has been deprecated.

  • Revamped introduction to the SDK documentation

Added

  • New Waypoint type in @universal-robots/contribution-api which should be used instead of the now deprecated KinematicPosition and Position

  • The new Getting Started page guiding the user through creating their first URCap

  • A new more thorough guide on Working with the Simulator. There is a known issue when using the --reset option without --clear-application when working with the simulator described in a note in the following linked section.

Removed

Fixed

0.11.95 - 2024-04-23

Compatible with PolyScope X 10.4.

Changed

  • Universal Robots NPM packages for the SDK is available by download and not packaged with the SDK-zip file.

  • Breaking: Bump Angular from 16.1.1 to 17.1.2

Added

  • Add Smart Skill option to the URCap generator in the SDK

  • Option to run the UR30 in the simulator.

Removed

  • Breaking: install.bat from the SDK, directing Windows users towards DevContainers and WSL2.

  • Documentation bundled with the SDK, it is now only available online.

Fixed

  • DevContainer terminal exit on commands with non 0 return code.

  • URProgram Node sample referenced internal component and not sample component.

  • URCap Generator newurcap.sh hanging during execution.

  • Configuring DevContainer takes a long time in VS Code.

0.10.103 - 2024-01-18

Added

Fixed

  • npm run delete-urcap would not delete a URCap including a Device

0.10.94 - 2023-12-20

Compatible with PolyScope X 10.3.

  • URCap development is now done inside a devContainer

  • Slimmed down SDK filesize

  • Cleaned up naming in the SDK, removed UR+ and instead using URCap

Changed

  • Breaking: Renamed following packages:

    • Rename LanguageSettings to RobotSettings

    • Rename ProgramPresenterComponent to ProgramPresenter

  • Breaking: Moved following packages from @universal-robots/contribution-typings to @universal-robots/contribution-api

    • ApplicationPresenter, ProgramPresenter, SmartSkillsPresenter, and SourcePresenter

  • Breaking: Move WebComponentDialogComponent to sub-package @universal-robots/contribution-api known as @universal-robots/contribution-api/angular.

  • Breaking: Move functions convertValue and valueRawConverter, from @universal-robots/utilities-units, to @universal-robots/contribution-api.

  • Breaking: Move interface @universal-robots/contribution-api to @universal-robots/ros2-interfaces

  • Breaking: Rename ApplicationAPI to ApplicationPresenterAPI

  • Breaking: Rename ProgramAPI to ProgramBehaviorApi

  • Breaking: Rename SmartSkillsAPI to SmartSkillsBehaviorAPI

  • Breaking: Rename service TreeService to ProgramNodeService

  • URCap installation guide URCap installation

Added

  • Document: Container cheat sheet

  • Document: Communicate with controller

  • Document: Smart Skills

  • Generate requiments.txt inside URCaps. This file describes what frontend API versions is used by the URCap.

  • Smart Skills URCap API

  • Add RobotPositionService

  • Add built-in PolyScope X program nodes as samples

  • Add --reset flag to URSim

Removed

  • Breaking: remove package @universal-robots/contribution-typings

Fixed

  • hotplug device did not reconnect after reboot

  • hotplug device where assigned to the wrong URCap

  • hotplug device did not reconnect after update

0.9.27 - 2023-09-25

Changed

  • Breaking: Bump Node from 16.14.0 to 18.17.1

  • Breaking: Bump Angular from 14.1.1 to 16.1.1

  • Breaking: In manifest.yaml

    • volumeMounts are now mounts. See datastorage samples and documentation.

    • Devices have changed to include a type instead of a specific device (e.g. device: "ttytool:/dev/ur-ttylink" becomes type: ttyTool)

Added

  • For Application nodes allow descriptive text to card in Applications menu