Communication between backend containers
In some cases it can be useful to split up a URCap into multiple backend containers. This presents the challenge of how to communicate between the two containers when the IP address is dynamic for the containers at container-start up.
In this case it is possible to use the servicegateway alias to allow for an executable to communicate out of its
container to some client that are available on the host network i.e. a sibling container.
servicegateway is the required host for container-to-container (and any backend) calls to ingress on the robot.
Do not use the robot IP or DNS name.
An example where a URCapX has been made with the following manifest file.
vendorId: UniversalRobots
urcapId: InterBeCom
containers:
- id: containerName_1
image: example_image_1:latest
ingress:
- id: rest-api,
containerPort: 2345
protocol: http
proxyUrl: /
- id: containerName_2
image: example_image_2:latest
This URCap contains two backend containers, where containerName_1 includes a webserver that is hosting internally
on localhost:2345/. For more details
see Creating a container backend Contribution.

Inside the implement of the containerName2 it is then possible to make specific requests against
http://servicegateway/UniversalRobots/InterBeCom/containerName_1/rest-api/ to hit the webserver of containerName_1.
In this example the same URCap is providing both backend containers, but that is not a necessity for this to work.
It is possible to make requests against backend containers from separate URCaps as long as the URI follows
http://servicegateway/vendorID/urcapID/containerId/ingressId/.