RTDEClient
The Real Time Data Exchange Client, RTDEClient, class serves as a standalone
RTDE
client. To use the RTDE-Client, you’ll have to initialize and start it separately. When starting
it, it can be chosen whether data should be read in a background thread or if the user has to poll
data in each cycle.
Background read: When background read is enabled (
start(true)) (default), the RTDE client will start a background thread that continuously reads data from the robot. The latest data package can be fetched using thegetDataPackage()method. This method returns immediately with the latest data package received from the robot. If no data has been received since last calling this function, it will block for a specified timeout waiting for new data to arrive.Blocking synchronous read: When background read is not enabled (
start(false)), data can (and has to be) fetched using thegetDataPackageBlocking()method. This call waits for a new data package to arrive and parses that into the passedDataPackageobject. This has to be called with the RTDE control frequency, as the robot will shutdown RTDE communication if data is not read by the client.
The following example uses the background read method to fetch data from the RTDE interface. See the RTDE Client example for an example of the blocking read method.
rtde_interface::RTDEClient my_client(ROBOT_IP, notifier, OUTPUT_RECIPE_FILE, INPUT_RECIPE_FILE);
my_client.init();
my_client.start(true); // Start background read
rtde_interface::DataPackage data_pkg(my_client.getOutputRecipe());
while (true)
{
if (my_client.getDataPackage(data_pkg, READ_TIMEOUT))
{
std::cout << data_pkg.toString() << std::endl;
}
}
Note
Recommended: Construct a DataPackage from getOutputRecipe() after init() and
reuse it in your control loop. With a matching recipe, the normal data receive path of
getDataPackage() and getDataPackageBlocking() does not allocate.
Still supported, but not recommended: The older flow that lets the client allocate a
package remains available for compatibility. The
std::unique_ptr<rtde_interface::DataPackage> getDataPackage(timeout) overload (Deprecated,
use getDataPackage(DataPackage&, timeout) instead) allocates a new package on each call, and
passing a null unique pointer to either read method also allocates a package. Passing a package
with a foreign recipe is supported through automatic repair, which may allocate. The null-pointer and foreign-recipe paths log
warnings; these warn about allocation, not unsupported usage. Prefer a reusable, matching-recipe
package for new code, especially in real-time loops.
The allocation-free guarantee applies only to the normal data receive path with that reused package. It does not cover error handling, non-data messages or reconnection.
A recipe only lists field names. The data types belonging to them are reported by the robot when
it acknowledges the recipe, and the first read applies them to your DataPackage without
allocation. Until that has happened getData() throws std::bad_variant_access. See
Field data types for how to ask a package what type it gave a field.
Upon construction, two recipe files have to be given, one for the RTDE inputs, one for the RTDE outputs. Please refer to the RTDE guide on which elements are available.
The recipes can be either passed as a filename or as a list of strings directly. E.g. the following will work
rtde_interface::RTDEClient my_client(
ROBOT_IP,
notifier,
{"timestamp", "actual_q"},
{"speed_slider_mask", "speed_slider_fraction"}
);
Note
timestamp will always be a part of the output recipe and will be added afterwards, if not defined. As the timestamp used for verifying the connectivity.
Connection timeout
When the robot is switched off, it neither accepts nor refuses connection requests, and each
connection attempt of init() waits until the operating system gives up. On Linux this takes
up to about two minutes. To give up earlier, set a connect timeout before calling init(). It applies
to each single connection attempt, including automatic reconnects:
rtde_interface::RTDEClient my_client(ROBOT_IP, notifier, OUTPUT_RECIPE, INPUT_RECIPE);
my_client.setConnectTimeout(std::chrono::seconds(2));
my_client.init(1); // Throws after about 2 seconds, if the robot does not answer
By default, the connect timeout is disabled and the operating system’s timeout applies.
Reading data
After calling my_client.start(), data can be read from the RTDEClient. Which read method
to use depends on how the client was started:
With background reading, start(true) (the default):
bool getDataPackage(DataPackage& data_package, std::chrono::milliseconds timeout): copies the latest package received by the background reader thread into the caller’s package.bool getDataPackage(std::unique_ptr<DataPackage>& data_package, std::chrono::milliseconds timeout): same, for a caller-owned pointer; a null pointer is allocated (with a warning) only on success.std::unique_ptr<DataPackage> getDataPackage(std::chrono::milliseconds timeout)(Deprecated, usegetDataPackage(DataPackage& data_package, std::chrono::milliseconds timeout)instead): allocates a new package on every call. It will be removed in May 2027.
Without background reading, start(false):
bool getDataPackageBlocking(std::unique_ptr<DataPackage>& data_package): waits for the next package from the robot and parses it straight into the caller’s package.
Calling a method from the other group logs an error and returns false.
Remember that, when not using a background thread, data has to be polled regularly, as the robot will shutdown RTDE communication if the receiving side doesn’t empty its buffer.
Reusing a package with the negotiated recipe keeps the normal data receive path free of memory allocations; prefer an overload that fills an existing, reusable package, especially for real-time use.
Always check the return value before using received data. A background read returns false on
timeout or when stopping or reconnecting cancels the pending read; restarting the reader does not
make a cancelled read succeed with stale data. Both unique-pointer overloads retain caller
ownership on failure and assign a previously null pointer only on success. A failed blocking read
can still partially update an existing package’s values if the incoming data is malformed.
Pacing a loop with the robot
Both read modes can pace an application loop at the robot’s negotiated RTDE output frequency, without a separate fixed-period sleep. Choose the mode according to how directly the loop should follow incoming packages:
With
start(false),getDataPackageBlocking()waits for the next package when no data is already buffered. Calling it at the start of each iteration lets packet arrival pace the loop, coupling it directly to the RTDE stream without a background-reader handoff. This is useful when each iteration should read data and then compute and submit a response. See the RTDE register round-trip example.With
start(true),getDataPackage(package, timeout)can also pace the loop: after the latest sample has been consumed, it waits for the background reader to publish another one, up to the timeout. If a newer sample is already available, it returns immediately. This mode decouples socket reading from application work and favors the latest sample; intermediate samples can be overwritten when the application is slower than the stream. It suits loops that need less direct synchronization and do not need to process every received sample.
For background reads used as a loop clock, allow enough timeout for the expected RTDE period
and scheduling jitter, and handle a false return instead of processing old data. In either
mode, the loop must keep up with the negotiated frequency for steady pacing. Buffered data can
make synchronous reads return immediately, and network or scheduling delays can make arrivals
irregular. Neither mode guarantees phase synchronization with the robot’s internal control cycle
or receipt of a command in the next cycle. Use the output timestamp to track robot time and
detect gaps between samples.
Field data types
getData() has to be given a variable of the field’s own type. A missing name returns
false; a type mismatch throws std::bad_variant_access.
Rather than hardcoding which type a field has, ask the package: getDataType() reports the
DataType a field currently holds. A successful client read applies the robot’s negotiated
types to an output package; init() alone does not type application-owned packages.
createInputDataPackage() returns an input package with the negotiated types already applied.
On a recipe-only package, setData() establishes an untyped field’s type from the value written;
subsequent writes must match that type. An untouched field has no type. This is useful for code
that has to handle whatever recipe it is configured with, such as a bridge to another middleware:
const std::optional<rtde_interface::DataType> type = data_pkg.getDataType(field_name);
if (!type)
{
// Not part of the recipe, or the field has no type yet
return;
}
// For "actual_q" this prints "VECTOR6D", the same spelling the RTDE guide uses
std::cout << field_name << " is a " << rtde_interface::toString(*type) << std::endl;
switch (*type)
{
case rtde_interface::DataType::DOUBLE:
{
double value;
data_pkg.getData(field_name, value);
break;
}
case rtde_interface::DataType::VECTOR6D:
{
vector6d_t value;
data_pkg.getData(field_name, value);
break;
}
// ... remaining types
}
DataType covers the complete set the protocol defines: BOOL, UINT8, UINT32,
UINT64, INT32, DOUBLE, VECTOR3D, VECTOR6D, VECTOR6INT32 and
VECTOR6UINT32. Switching over it exhaustively means the compiler will point out any case a
future protocol addition leaves unhandled.
Writing data
For writing data to the RTDE interface, use the RTDEWriter member of the RTDEClient. It can be
retrieved by calling getWriter() method. The RTDEWriter provides convenience methods to write
all data available at the RTDE interface. Make sure that the required keys are configured inside the
input recipe, as otherwise the send-methods will return false if the data field is not setup in
the recipe.
An example of a standalone RTDE-client can be found in the examples subfolder. To run it make
sure to
have an instance of a robot controller / URSim running at the configured IP address (or adapt the address to your needs)
run it from the package’s main folder, as for simplicity reasons it doesn’t use any sophisticated method to locate the required files.
Note
The URDriver class creates a RTDEClient during initialization using the provided
recipes and utilizing the robot model’s maximum frequency. If you would like to use a different
frequency, please use the resetRTDEClient() method after the UrDriver object has been
created.
Read-Only RTDEClient
While RTDE allows multiple clients to connect to the same robot, only one client is allowed to
write data to the robot. To create a read-only RTDE client, the RTDEClient can be created with
an empty input recipe, like this:
rtde_interface::RTDEClient my_client(ROBOT_IP, notifier, OUTPUT_RECIPE, {});
// Alternatively, pass an empty filename when using recipe files
// rtde_interface::RTDEClient my_client(ROBOT_IP, notifier, OUTPUT_RECIPE_FILE, "");
my_client.init();
auto data_pkg = std::make_unique<rtde_interface::DataPackage>(my_client.getOutputRecipe());
my_client.start();
while (true)
{
if (my_client.getDataPackage(data_pkg, READ_TIMEOUT))
{
std::cout << data_pkg->toString() << std::endl;
}
}
RTDEWriter
The RTDEWriter class provides an interface to write data to the RTDE interface. Data fields that
should be written have to be defined inside the INPUT_RECIPE as noted above.
Important
Use RTDEClient to initialize and access RTDEWriter (recommended). Create an RTDEClient
with a non-empty input recipe, call init(), then use its writer through getWriter().
The client handles the connection, protocol negotiation, input recipe setup and writer
initialization, including the field types and recipe ID reported by the robot.
Constructing and using RTDEWriter directly is still supported, but is a lower-level option
for applications that manage the RTDE connection and handshake themselves. It is not the
recommended approach for normal application code.
The class offers convenience methods for common inputs and sendPackage() for a complete input
recipe.
Data is sent asynchronously to the RTDE interface. A successful sendPackage() or send...()
call updates the pending send buffer and notifies the writer thread; it does not confirm delivery
or processing by the robot. This is not a FIFO queue of calls: multiple updates before the writer
consumes the pending buffer can be coalesced, and a later sendPackage() can replace an earlier
pending package. Separate helper calls may be transmitted separately or coalesced, depending on
when the writer runs. Use sendPackage() to submit related fields together in one buffer update,
not to guarantee a distinct transmission for every call.
To write several fields at once, ask the client for a package that already carries the data types
the robot reported for the input recipe. Call createInputDataPackage() after a successful
init() with a non-empty input recipe, fill the fields you care about and pass it to
sendPackage(). The new package starts with zero values; when reusing it, fields retain their
previous values unless explicitly changed or reset. Because the package is already typed,
setData() reports a value written with the wrong type immediately:
rtde_interface::DataPackage input_pkg = my_client.createInputDataPackage();
input_pkg.setData("speed_slider_mask", uint32_t{ 1 });
input_pkg.setData("speed_slider_fraction", 0.5);
my_client.getWriter().sendPackage(input_pkg);
A package constructed from getInputRecipe() still works. Its types are taken from the values
written to it and are checked when the package is submitted to sendPackage(). The field names
and order must match the negotiated input recipe. Fields that remain untyped are sent as typed
zeros, while incompatible types cause sendPackage() to return false. See the
RTDE register round-trip example for a complete example.
If direct RTDEWriter use is required instead of the recommended RTDEClient flow, perform the RTDE handshake
and configure the stopped writer with setProtocolVersion(negotiated_version) and
setRecipeTypes(acknowledged_types) before calling init(recipe_id) with the acknowledged
input recipe ID. acknowledged_types is a std::vector<rtde_interface::DataType>; the
type names of the robot’s setup answer are converted with rtde_interface::parseDataTypes(),
which also keeps the NOT_FOUND and IN_USE entries visible. Constructing the writer or calling init(recipe_id) alone does not establish
the field types. RTDEClient::init() handles these steps automatically.
Note
The RTDEWriter will return false on any writing attempts for fields that have not been
setup in the INPUT_RECIPE. When no input recipe was provided, all write operations will
return false. No writer thread is started in that case, and createInputDataPackage()
throws UrException even after successful client initialization. The factory also throws
before input recipe negotiation or while the writer is stopped.