ur_simulation_gz
This package contains configurations and example files for Gazebo simulation of Universal Robots manipulators.
Structure of the repository
To set up the simulation the used files are:
urdf/ur_gz.ros2_control.xacro
- macro for ros2_control configuration, defining the initial joint positions and the hardware interface plugin for the simulationurdf/ur_gz.urdf.xacro
- main file that contains the robot description, defines reference for the Gazebo world and initializes ros2_control Gazebo plugin.