Changelog
0.12.x - (In development)
Compatible with upcoming PolyScope X 10.5.
Changed
Added
Removed
Fixed
0.11.95 - 2024-04-23
Compatible with PolyScope X 10.4.
Changed
Universal Robots NPM packages for the SDK is available by download and not packaged with the SDK-zip file.
Breaking: Bump
Angular
from16.1.1
to17.1.2
Added
Add Smart Skill option to the urcap generator in the SDK
Option to run the UR30 in the simulator.
Add URCap upgrade guide from v0.10 to v0.11
Removed
Breaking:
install.bat
from the SDK, directing Windows users towards DevContainers andWSL2
.Documentation bundled with the SDK, it is now only available online.
Fixed
DevContainer terminal exit on commands with non 0 return code.
URProgram Node sample referenced internal component and not sample component.
URCap Generator
newurcap.sh
hanging during execution.Configuring DevContainer takes a long time in VS Code.
0.10.103 - 2024-01-18
Added
Document: Networking - Macvlan
Add
macvlan
SDK sample
Fixed
npm run delete-urcap
would not delete a URCap including a Device
0.10.94 - 2023-12-20
Compatible with PolyScope X 10.3.
URCap development is now done inside a devContainer
Slimmed down SDK filesize
Cleaned up naming in the SDK, removed
UR+
and instead usingURCap
Changed
Breaking: Renamed following packages:
Rename
LanguageSettings
toRobotSettings
Rename
ProgramPresenterComponent
toProgramPresenter
Breaking: Moved following packages from
@universal-robots/contribution-typings
to@universal-robots/contribution-api
ApplicationPresenter
,ProgramPresenter
,SmartSkillsPresenter
, andSourcePresenter
Breaking: Move
WebComponentDialogComponent
to sub-package@universal-robots/contribution-api
known as@universal-robots/contribution-api/angular
.Breaking: Move functions
convertValue
andvalueRawConverter
, from@universal-robots/utilities-units
, to@universal-robots/contribution-api
.Breaking: Move interface
@universal-robots/contribution-api
to@universal-robots/ros2-interfaces
Breaking: Rename
ApplicationAPI
toApplicationPresenterAPI
Breaking: Rename
ProgramAPI
toProgramBehaviorApi
Breaking: Rename
SmartSkillsAPI
toSmartSkillsBehaviorAPI
Breaking: Rename service
TreeService
toProgramNodeService
URCap installation guide URCap installation
Added
Document: Container cheat sheet
Document: Communicate with controller
Document: Smart Skills
Generate
requiments.txt
inside URCaps. This file describes what frontend API versions is used by the URCap.Smart Skills URCap API
Add
RobotPositionService
Add built-in PolyScope X program nodes as samples
Add
--reset
flag toURSim
Removed
Breaking: remove package
@universal-robots/contribution-typings
Fixed
hotplug device
did not reconnect after reboothotplug device
where assigned to the wrong URCaphotplug device
did not reconnect after update
0.9.27 - 2023-09-25
Changed
Breaking: Bump
Node
from16.14.0
to18.17.1
Breaking: Bump
Angular
from14.1.1
to16.1.1
Breaking: In
manifest.yaml
volumeMounts
are nowmounts
. Seedatastorage
samples and documentation.Devices have changed to include a type instead of a specific device (e.g.
device: "ttytool:/dev/ur-ttylink"
becomestype: ttyTool
)
Added
For
Application nodes
allow descriptive text to card inApplications menu