Private
Readonly
eventReturns the generated script code for getting the value of a given signal
use getGetSignalScript instead
The ID of the source containing the signal to get
The ID of the signal to get
Returns the generated script code for setting the signal to the given value
use getSetSignalScript instead
The ID of the source containing the signal to set
The ID of the signal to set
The value to set the signal to - for digital values use 0 or 1, for registers use only integers, for analog values use any float
Returns an object literal containing a mapping of SignalIDs -> AnalogDomains
should be handled by the individual contribution
The ID of the Source for which to get Domain data
Returns the generated script code for getting the value of a given signal
The Source group, containing the source to provide events for
The ID of the source containing the signal to get
The ID of the signal to get
Returns the generated script code for setting the signal to the given value
The Source group, containing the source and signal to provide script for
The ID of the source containing the signal to set
The ID of the signal to set
The value to set the signal to - for digital values use 0 or 1, for registers use only integers, for analog values use any float
Returns an object literal containing a mapping of SignalIDs -> Labels
Source contributions will be responsible for providing labels for signals directly
The ID of the Source for which to get the Label mappings
Returns an object literal containing a mapping of SignalIDs -> Presets
Source contributions will be responsible for handling presets themselves
The ID of the Source for which to get the Preset mappings
Returns an Observable providing Signal events
use getSourceUpdates instead
The Source containing the Signals to provide events for
Optional
filter: Partial<Pick<Signal, "direction" | "valueType">>SignalFilter used to filter only events for Signals which match the filter
Returns the list of Signals in a Source
use getSourceSignals instead
The Source to list Signals for
Optional
filter: Partial<Pick<Signal, "direction" | "valueType">>SignalFilter used to filter only Signals which match the filter
Returns the list of Signals in a Source
The Source group, containing the source to provide signals for
The Source to list Signals for
Optional
filter: Partial<Pick<Signal, "direction" | "valueType">>SignalFilter used to filter only Signals which match the filter
Returns an Observable providing Signal events
The Source group, containing the source to provide events for
The Source containing the Signals to provide events for
Optional
filter: Partial<Pick<Signal, "direction" | "valueType">>SignalFilter used to filter only events for Signals which match the filter
Returns the ID's of Sources that are available to the application
Optional
filter: Partial<Pick<Signal, "direction" | "valueType">>SignalFilter used to filter only Sources which contain Signals matching the filter
Sets a value on a signal
use setSourceSignalValue instead
The ID of the Source, containing the Signal to set
The ID of the Signal to set
The value to set
Sets a value on a signal
The Source group, containing the source to provide events for
The ID of the Source, containing the Signal to set
The ID of the Signal to set
The value to set
Generated using TypeDoc
Service for getting information about Sources and Signals