Initialize the object.
Entity is the possibly complex object that TabInput is representing
SelectedType is the type of value that the user has selected: 'Value' | 'Variable' | 'Expression'
Value is either the "value" of the "variable" or the "expression" entered by the user
Static
getReturns TabInputValue from TabInputModel which is the input for the TabInput component
Static
isChecks if tabInputModel has an entity and a selectedType
to be interrogated
Static
isValidates the model
to validate
Static
setSets TabInputValue on TabInputModel which is the input for the TabInput component
to update the TabInputValue
the inserted value for the model.
Generated using TypeDoc
Model to be used in collaboration with tabInputComponent.