Creates a new instance of the ValidationService
the target to send message events on
the id of the currently selected node
Readonly
eventPrivate
Readonly
selectedReturns the last validation response generated from the behavior worker. If the node is valid the returned response will be exactly { isValid: true } without any extra data.
Generated using TypeDoc
Allows program nodes to obtain the validation response generated from their respective behavior worker.