A KinematicPosition defines a position of the robot, including the kinematics data from the robot where it was taught, so it can be accurately reproduced on another robot.
Optional
Generated using TypeDoc
A KinematicPosition defines a position of the robot, including the kinematics data from the robot where it was taught, so it can be accurately reproduced on another robot.
Deprecated