1. Introduction

1.1 ROS 2 versions

Controller is using ROS 2 Jazzy version. Default DDS implementation (Fast DDS) is used for underlying communication.

ROS 2 and underlying DDS are interoperable to some extent between versions. Note that ROS 2 Humble was affected by a bug where node would leak memory if exposed to messages from newer versions of ROS 2. While the version linked to the controller has been patched, other nodes such as your own, or the ones used in URCapX may still be vulnerable. Proceed with caution especially when mixing ROS 2 versions older and newer than the one used in the controller.

1.2 Quality of Service settings

Quality of Service(QoS) is feature in ROS 2 that allows users to fine tune the communication between nodes. The policies range from being as *reliable *as TCP to as *best-effort *as UDP and many more options in between. A set of policies make a profile, the right set of profiles need to be set based on the application (https://docs.ros.org/en/jazzy/Concepts/About-Quality-of-Service-Settings.html#qos-policies). The default profile for a publisher on the robot is as follows

  • default History - Keep last[n]

  • default Depth  - Queue size[n]=1

  • default Reliability - Reliable

  • default Durability - Volatile

  • default Deadline - Forever

  • default Lifespan - Forever

  • default Liveliness - Liveliness_Automatic

  • default Lease Duration - Forever

The important point to remember is that the QoS settings have to be compatible (or ideally the same) on the publisher and subscriber side. Incompatible QoS settings will prevent communication entirely. More information about QoS compatibility can be found in https://docs.ros.org/en/jazzy/Concepts/About-Quality-of-Service-Settings.html#qos-compatibilities.