URCap manifest
manifest.yaml
All URCapX files must provide a manifest.yaml file to identify itself as a URCap. The metadata in the manifest file provides id and name for the URCap and one or more artifacts.
All manifest.yaml files must contain the following Vendor and URCap fields in the metadata section:
vendorID : The id to identify the vendor or company.
vendorName : The name of the vendor or company.
urcapID : Is used to identify a URCap.
urcapName : Defines the name of a URCap.
version : The version of the URCap.
The fields vendorID and urcapID in combination uniquely defines an ID
for the URCap. They must only contain letters, digits and hyphens. The fields vendorName,
urcapName and versionare used for presentation.
Web Contributions
The following example is the manifest file for the “Grip Distance” URCap
metadata:
vendorID: universal-robots
vendorName: "Universal Robots"
urcapID: gripdistance
urcapName: "Grip Distance"
version: 1.0.0
artifacts:
webArchives:
- id: gripdistance
folder: gripdistance
Fields required for a web frontend artifact are:
webArchives : Specifies the type of artifacts. The artifacts are a list if web-archives.
id : The name to identify the artifact. All artifacts must have a name.
folder : Defines a folder to this specific artifact and is part of a unique path to the artifact.
In this example the URCap name is `Grip Distance’ and it contains an artifact with the name ‘gripdistance’. A manifest file could also contain more artifacts, each with its own artifact name.
Docker Container
If a Docker Container is included then an artifact entry for that needs to be added, like in this sample manifest.yaml file:
metadata:
vendorID: universal-robots
urcapID: sample-docker
version: 0.0.1
vendorName: Universal Robots
urcapName: Sample Docker Contribution
contactInfo: Energivej 25, 5260 Odense S, Denmark
description: Daemon Sample URCap
copyright: Copyright (c) 2009-2021 Universal Robots. All rights reserved.
licenseType: Sample license
artifacts:
containers:
- id: sample-docker-backend
image: sample-docker-backend
ingress:
- id: rest-api
containerPort: 5000
protocol: http
proxyUrl: /
mounts:
- mount: mount-type:/mount
devices:
- device: ttytool:/dev/ur-ttylink
containers Specifies a list of container contributions. Container contributions have the following fields:
id : The name to identify the artifact. All artifacts must have a name.
image : The name of the docker image.
ingress
: A list of container network configurations, each configuration consists of: name, port, protocol and proxyUrl.
The service configured in the ingress will be reachable at a URL defined using this template:
<vendorID>/<urcapID>/<container-name>/<ingress-name>.
In the above example the REST endpoint can be accessed at:
universal-robots/sample-docker/sample-docker-backend/rest-api.
The docker container will receive the requests on port 5000 at location “/”.
* id: Used to reach the service or WebSocket.
* containerPort: Container port of the HTTP server in the container.
* protocol: Specifies the communication protocol. Supported values are “HTTP” (default), “HTTPS” or “WebSocket”.
* proxyUrl: Specifies the URL being forwarded to.
mounts
: List of volumes (mounts) that will be available in the docker container and is set by choosing
the type of mount, and a path.
devices
: Mapping a list of host devices (device) to docker container device. This example will make the tool serial port
“/dev/ur-ttylink” available inside the contributed docker container.
ROS 2
If ROS 2 is included it will have to reside in a container. Therefore, the artifact type must be
containers and all the container YAML parameters can be used as described above.
Installing/Uninstalling URCaps
The SDK comes with a sdk-utils npm package, containing various helper functionalities for
URCaps. This enables you to install and uninstall URCaps using the NPM command line tools.
To use the NPM package, add @universal-robots/urcap-utils to the devDependencies element in package.json
(it is included by default in URCaps created with the URCap Generator)
Building
When building your URCap for the first time or if any package dependencies have changed you need to run
npm install
Then afterward you can build the URCap with
npm run build
And now you are ready to test the URCap either in the simulator or on a robot.
Installing
To install a URCap, use the following command
npm run install-urcap -- [--host <HOST_IP>] [--port <PORT>] [--force-replace]
This will install the URCap in PolyScope X. If you are running the simulator on a different port,
you can specify it by using the -- --port <PORT> parameter (NB: notice the -- in front of the
--host/--port/--force-replace parameters; this is NPM’s way of adding parameters to an npm run command).
If a URCap with the same VendorId and URCapId exists this will be updated, thus preserving any persisted data. If you
wish to completely remove the existing URCap before installing the new version, use the --force-replace flag.
To see the changes in PolyScope X, it is necessary to refresh the browser, once the URCap is installed.
If no --host parameter is given to install-urcap or delete-urcap, it will default to the Docker gateway IP which means it will be
installed/deleted in the currently running simulator.
Example DevContainer
You have started the simulator and created a URCap named my-urcap and built it so a
target/my-urcap.urcapx file exists. Then the command would be
npm run install-urcap
Example Robot
You have a robot with the IP address 192.168.2.80, and have created a URCap named my-urcap and built it so a
target/my-urcap.urcapx file exists. Then the command would be
npm run install-urcap -- --host 192.168.2.80
Uninstalling
Uninstalling a URCap is similar to installing; simply use the following command
npm run delete-urcap <VENDOR_ID> <URCAP_ID> [-- --host <HOST_IP>] [-- --port <PORT>]
As when installing, it is necessary to refresh the browser to see the changes in PolyScope X.
Example
The simulator has a URCap installed, with vendorID: my-vendor and urcapID: my-urcap.
Then the command would be
npm run delete-urcap my-vendor my-urcap