ReverseInterface

The ReverseInterface opens a TCP port on which a custom protocol is implemented between the robot and the control PC. The port can be specified in the class constructor.

It’s basic functionality is to send a vector of floating point data together with a mode. It is meant to send joint positions or velocities together with a mode that tells the robot how to interpret those values (e.g. SERVOJ, SPEEDJ). Therefore, this interface can be used to do motion command streaming to the robot.

In order to use this class in an application together with a robot, make sure that a corresponding URScript is running on the robot that can interpret the commands sent. See this example script for reference.

The ReverseInterface together with the Script Command Interface, the Trajectory Point Interface and the external_control.urscript creates a communication protocol in order to control many of the robot’s functionalities.

Also see the ScriptSender for a way to define the corresponding URScript on the control PC and sending it to the robot upon request.

Communication protocol

The ReverseInterface’s “reverse_socket” on the robot is expecting 32 bit integer representations 8 datafields frequently. The timeout with which new data is expected can vary depending on the current control mode and is set as part of the message. The data fields have the following meaning:

Table 1 reverse_socket message format

index

meaning

0

read timeout in milliseconds. The next read from the socket will use this timeout.

1-6

Current motion target. depending on the control mode, this can be interpreted as

  • joint positions (SERVOJ)

  • joint velocities (SPEEDJ)

  • trajectory instructions (FORWARD)

    • field 1: Trajectory control mode (1: TRAJECTORY_MODE_RECEIVE, 2: TRAJECTORY_MODE_STREAM_START, 3: TRAJECTORY_MODE_STREAM_END, -1: TRAJECTORY_MODE_CANCEL). See Streaming trajectories for the streaming modes.

    • field 2: Trajectory point count. Its interpretation depends on the control mode in field 1.

    • field 3: The identifier of the move that is being started, for the two control modes which start one. The robot adopts this identifier and then executes only those trajectory points which carry it, and that is what prevents points left over from a move that has already ended from running as part of the next one. The remaining control modes do not start a move, and the robot ignores the field for them. The field is 0 unless set with setMoveId(), which UrDriver does for every move. See Trajectory Point Interface for the point record which carries the identifier back.

  • Cartesian velocities (SPEEDL)

  • Cartesian pose (POSE)

  • freedrive instruction (FREEDRIVE)

    • field 1: Freedrive mode (1: FREEDRIVE_MODE_START, -1: FREEDRIVE_MODE_STOP)

  • target joint torques (TORQUE, see Direct torque control mode).

7

Control mode. Can be either of

  • -2: STOPPED – status - not meant to be sent

  • -1: UNINITIALIZED – status - not meant to be sent

  • 0: IDLE – no motion

  • 1: SERVOJ – High-frequent joint position control

  • 2: SPEEDJ – High-frequent joint velocity control

  • 3: FORWARD – Trajectory interpolation on the robot, see Trajectory Point Interface

  • 4: SPEEDL – High-frequenct Cartesian velocity control

  • 5: POSE – High-frequent Cartesian pose control (servoj using inverse kinematics)

  • 6: FREEDRIVE – Use the robot’s freedrive mode

  • 7: TOOL_IN_CONTACT – status - not meant to be sent. In tool contact mode this will encode whether tool contact has been established or not.

  • 8: TORQUE – Direct torque control mode (since PolyScope 5.23.0 / 10.10.0)

Note

In URScript the socket_read_binary_integer() function is used to read the data from the reverse socket. The first index in that function’s return value is the number of integers read, so the actual data starts at index 1. The indices in the table above are shifted by one when accessing the result array of the URScript function.

The motion target is encoded into an integer representation and has to be divided by the MULT_JOINTSTATE constant to get the actual floating point value. This constant is defined in ReverseInterface class.

Depending on the control mode one can use the write() (SERVOJ, SPEEDJ, SPEEDL, POSE, TORQUE), writeTrajectoryControlMessage() (FORWARD) or writeFreedriveControlMessage() (FREEDRIVE) function to write a message to the “reverse_socket”.

Streaming trajectories

A FORWARD-mode trajectory can be executed in one of two ways.

A finite trajectory declares its total length up front: writeTrajectoryControlMessage(TRAJECTORY_START, n) promises exactly n points, and execution completes once they have been consumed. This is the mode used by Trajectory Joint Interface example.

A streaming trajectory is open-ended. The producer does not commit to a point count in advance; it opens the stream, writes points for as long as it likes, and signals end-of-stream explicitly. This suits points produced on the fly – from a planner or a teleoperation source – where the total length is unknown when motion begins. The message sequence is:

writeTrajectoryControlMessage(TRAJECTORY_STREAM_START)   // open the stream
// write a motion primitive, any number of times:
// writeTrajectoryPoint(...) / writeTrajectorySplinePoint(...) / writeMotionPrimitive(...)
writeTrajectoryControlMessage(TRAJECTORY_STREAM_END, n)  // close the stream

TRAJECTORY_STREAM_START opens the trajectory; its point-count argument is unused. The producer then writes motion primitives – via writeTrajectoryPoint(), writeTrajectorySplinePoint() or writeMotionPrimitive() – for as long as it likes. TRAJECTORY_STREAM_END closes it.

Important

The n passed to TRAJECTORY_STREAM_END must equal the total number of motion primitives the producer wrote since TRAJECTORY_STREAM_START. The controller consumes primitives asynchronously as it executes them and cannot otherwise tell how many are still outstanding; it uses n to account for those still in flight before completing. Aborting a stream with TRAJECTORY_CANCEL requires the same count, for the same reason. (For a finite TRAJECTORY_START trajectory the cancel argument is unused.)

Three obligations fall on the producer:

  • Do not starve the controller. The robot consumes the stream as it executes it, so the producer must keep work available: the next primitive must arrive before the robot finishes the ones it already holds. The budget for delivering it is simply the duration of the work in hand – a primitive that runs for five minutes gives five minutes to produce its successor, while a stream of eight-millisecond primitives demands one every eight milliseconds. If the robot runs out of submitted work before the next primitive arrives and before TRAJECTORY_STREAM_END is sent, the trajectory ends with TRAJECTORY_RESULT_FAILURE. Delivering primitives as they are produced, without holding them back, is the natural way to satisfy this.

  • End at rest. Streaming adds no wind-down deceleration of its own. Make the final point a controlled stop, with zero velocity and acceleration, so the spline interpolates smoothly to rest at the goal. The trajectory thread issues stopj on exit regardless, so a non-zero terminal point still stops the robot, but the transition will be less smooth.

  • Keep each move’s points within its own bounds. All of a move’s points must be written after the control message that begins it, and before the control message that ends it or begins the next. A producer running on its own thread must be quiesced, not merely signalled to stop, before another thread sends either.

On completion the callback registered with setTrajectoryEndCallback() reports TRAJECTORY_RESULT_SUCCESS for a clean end (TRAJECTORY_STREAM_END processed, all points consumed), TRAJECTORY_RESULT_FAILURE for a producer underrun, or TRAJECTORY_RESULT_CANCELED if the stream was aborted with TRAJECTORY_CANCEL.

See Trajectory streaming example for a complete, working example.

Direct torque control mode

Direct torque control mode is available since PolyScope version 5.23.0 / 10.10.0. It allows to command joint torques directly to the robot.

Note

Target torques are given after gravity compensation. A vector of zeros will hold the current position given that the payload is known to the controller.

Warning

Direct torque control is a very low-level command interface. Commanding high torques in free space can make the robot move very fast and hereby trigger a fault due to joint velocities or the TCP speed violating the safety settings. Keep that in mind when using this mode.