ur_rtde_publisher
A ROS 2 package that provides a RTDE (Real Time Data Exchange) publisher for Universal Robots manipulators. The node connects to a robot’s IP via UR’s RTDE protocol, retrieves selected robot state variables (such as robot mode, safety status and timestamps), and exposes them as ROS 2 topics.
Note
This package is currently in an early development stage. At this point, we don’t make any guarantees about ROS API stability, so the interface types for published data might change in the future. Hence, this package is currently not available as a pre-built binary in any ROS distribution, and users need to build it from source.
Usage
The node is started using the provided launch file:
ros2 launch ur_rtde_publisher rtde_publisher.launch.xml \
robot_ip:=192.168.56.101 \
output_recipe:='["payload", "robot_mode"]' \
rtde_frequency:=125 \
use_robot_timestamp:=true \
t_delay:=0.004
See the documentation’s usage section for more details on how to run the node and verify its operation.
Parameters
robot_ip(string): IP address of the robot.output_recipe(string[]): List of RTDE output variables to request and publish.rtde_frequency(int, optional, default:500): RTDE communication frequency in Hz.tf_prefix(string, optional, default:""): Optional prefix applied to theframe_idof stamped ROS 2 messages.use_robot_timestamp(bool, optional, default:false): If true, uses the robot’s hardware clock.t_delay(double, optional, default:0.0): Network latency compensation in seconds[s]to align the data timeline with the actual physical measurement time.
Architecture
The package follows the following structure:
rtde_publisher_node: Implements the ROS2 node. It handles parameters loading, RTDE connections setup, and the main publish loop.
rtde_publisher: Responsible for creating ROS publishers based on the RTDE recipe and the YAML mapping file.
rtde_converter: Contains utility functions to convert RTDE raw data types into ROS messages types.
Build status
Humble |
Jazzy |
Kilted |
Lyrical |
Rolling |
|
|---|---|---|---|---|---|
Branch |
|||||
Build status main |
|||||
Build status testing |