You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.4.
MotionPlus URCap
URCap Architecture
The following diagram shows the architecture design of the MotionPlus URCap:

The MotionPlus URCap consists of:
MotionPlus Service Process - Hosts an EtherCAT Master Device Implementation and an XML-RPC server to help interface with the EtherCAT Master Device Implementation from the URScript program. Functionality provided through the XML-RPC interface is described here. The URCap provides an URScript API that interacts with the XML-RPC interface.
Installation Node - Provides a GUI for configuring, starting, and stopping the MotionPlus Service Process. See here.
EtherCAT URScript API - Provides a URScript interface for lower-level EtherCAT functionality that is loaded into the Polyscope program preamble by the Installation Tab. The API abstracts much of the XML-RPC communication with the MotionPlus Service Process.
MotionPlus URCap Errors
This section describes the public error codes generated by the EtherCAT URCap and reported directly to the user via URScript popups.
It does not describe the various internal error codes which may be reported in the EtherCAT Daemon log file. These error codes are not fixed as they are generated by various software components, many of which are maintained separately from the URCap.
Error Categories
Each public error code for the EtherCAT URCap falls under one of the following categories, according to the value of the error code:
Error Range |
Category |
Description |
|---|---|---|
0 |
Success |
indication that no error has occurred |
100-199 |
XML-RPC client |
any error generated when client passes an invalid argument to XML-RPC method or fails to meet one of the method’s preconditions |
200-299 |
XML-RPC service |
any error generated during the execution of an XML-RPC method (with valid arguments and its preconditions met) |
300-399 |
EtherCAT master |
any error generated by the EtherCAT master (after it has been configured and started)NOTE: Each of these errors will cause the EtherCAT master to halt and will prevent it from being restarted until the error is cleared. (See “Error Display” section of URCap Installation Page Documentation for more information.) |
100-199 XML-RPC client errors
Code |
Name |
Description |
Corrective Action |
|---|---|---|---|
101 |
Invalid Network Interface |
Given device name references a network device that does not exist or is unsuitable for EtherCAT communication. |
Try again with a supported device name. |
102 |
Invalid Axis Index |
Given axis index is negative or larger than the maximum supported axis index. |
Try again with a valid axis index. |
103 |
Duplicate Axis Config |
Given axis configuration has an axis index, axis name, or station address that is already in use by another existing axis configuration. |
Try again with axis index, axis name, and station address values that are not already in use. |
104 |
No Network Interface Selected |
No network device has been selected for EtherCAT communication. |
Select an EtherCAT network device and try again. |
105 |
No Axes Configured |
No axes have been configured for the EtherCAT master. |
Define one or more axes configurations and try again. |
106 |
Master Halted from Error |
EtherCAT master has halted due to a runtime error and cannot be restarted until error has been cleared. |
Inspect Error Display on URCap Installation Page to determine which runtime error has occurred. Then look up the runtime error in the EtherCAT Master Errors section of this document and perform the recommended corrective action. |
107 |
Master Already Running |
An attempt was made to start the EtherCAT master while it was already running. |
Stop the EtherCAT master and try again. |
200-299 XML-RPC service errors
Code |
Name |
Description |
Corrective Action |
|---|---|---|---|
201 |
Internal Service Error |
An internal error (e.g. software bug) occurred during execution of the XML-RPC method. |
Reattempt operation. If problem persists, contact UR with error details from EtherCAT daemon log file. |
202 |
Network Interface Enable Failed |
Network device selected for EtherCAT communication could not be enabled. |
Select a different network device and reattempt operation. If problem persists, contact UR with error details from EtherCAT daemon log file. |
203 |
Master Start Failed |
An error occurred while starting the EtherCAT master. |
Verify |
300-399 EtherCAT master errors
Code |
Name |
Description |
Corrective Action |
|---|---|---|---|
301 |
Internal Master Error |
EtherCAT master has encountered an internal error (e.g. software bug). |
Clear the error and restart the master. If problem persists, contact UR with error details from EtherCAT daemon log file. |
302 |
Missing URControl Feedback |
EtherCAT master has no realtime communication with UR Controller. |
Verify UR Controller is running and is not in a fault state. Then clear error and restart EtherCAT master. |
303 |
Master State Update Failed |
EtherCAT master failed to reach target state (e.g. OP) within expected deadline. |
Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. |
304 |
EtherCAT Send Failed |
EtherCAT master failed to send data over EtherCAT network. |
Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. |
305 |
EtherCAT Receive Failed |
EtherCAT master failed to receive data over EtherCAT network. |
Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. |
306 |
Slave Command Failed |
EtherCAT slave failed to process command word within expected deadline. |
Verify slave is not in fault sate. Then clear error and restart EtherCAT master. |
305 Sub Error Codes - EtherCAT
Code |
Name |
Description |
Corrective Action |
|---|---|---|---|
305.0 |
Slave Number Mismatch |
Number of slaves configured and connected do not match. |
Check the EtherCAT cable/network, check the program, make sure the number of connected and configured slaves matches. |
305.1 |
Unknown Master State |
The EtherCAT network is in an unknown state. |
Clear the error and restart the master. |
305.2 |
Set INIT State Failure |
Failed to transit the EtherCAT network to INIT state. |
Clear the error and restart the master. |
305.3 |
Set PRE_OP State Failure |
Failed to transit the EtherCAT network to PRE_OP state. |
Clear the error and restart the master. |
305.4 |
Set SAFE_OP State Failure |
Failed to transit the EtherCAT network to SAFE_OP state. |
Clear the error and restart the master. |
305.5 |
Set OP State Failure |
Failed to transit the EtherCAT network to OP state. |
Clear the error and restart the master. |
305.6 |
Mode Update Failure |
Failed to set slave to an OPERATION MODE. |
Clear the error and restart the master. |
305.7 |
Unsupported Mode |
This OPERATION MODE is not supported. |
Contact UR with error details from MotionPlus Service log file. |
305.8 |
Consecutive PDO Timeout |
Failed to receive PDO for more than 5 consecutive cycles. |
Check the Ethernet cable. Consider using the native Ethernet port (instead of USB Ethernet adapter). Clear the error and restart the master. |
305.9 |
SDO Write Failure |
Failed to write SDO to the slave. |
Check the MotionPlus Service log for more details. |
305.10 |
SDO Read Failure |
Failed to read SDO from the slave. |
Check the MotionPlus Service log for more details. |
305.11 |
Master State Read Failure |
Failed to read MASTER STATE of the EtherCAT network. |
Clear the error and restart the master. |
305.12 |
Target Position Overflow |
The target position is out of the range for a 32bit integer. |
The motion has run out of range. Check axis configuration, and try to limit the range of motion in the program. |