You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.5.

EtherCAT Drive Config Script

This script should be placed first within a program.

# EtherCAT Single Axis Config Script
# This script provides the MotionPlus configuration for the EtherCAT drive, servo motor, gearing and encoder.

# NOTE: You must first create the following global variable in the installation tab under "General"
#       CAL_AX1_ROTARY  p[0,0,0,0,0,0]
# This will be used to store the calibrated poses calculated here

PI = acos(-1)

AXIS_TYPE1 = 0                # 0:rotary, 1:linear
VELOCITY_LIMIT1 = 0.7*2       # rad/s
ACCELERATION_LIMIT1 = 0.1*100 # rad/s^2
ENCODER_RESOLUTION1 = <ENCODER>
FEED_CONSTANT1 = 2 * PI       # make sure +Z points out of motor
GEAR_RATIO1 =  <GEAR>
ZERO_OFFSET1 = 0

def run_axis_config():
    # stop EtherCAT master first, otherwise, reset_world_model may throw an error
    ethercat_clear_error()
    ethercat_stop(True)
    reset_world_model()

    # after calibration, change this to use CAL_AX1_ROTARY
    axis1_position = p[0,0,0,0,0,0]
    #axis1_position = CAL_AX1_ROTARY    
    
    axis_group_add("positioner", p[0,0,0,0,0,0], "base")
    axis_group_add_axis("positioner", "axis1", "", axis1_position, AXIS_TYPE1, VELOCITY_LIMIT1, ACCELERATION_LIMIT1)

    ethercat_config_axis("axis1", 1, ENCODER_RESOLUTION1, GEAR_RATIO1, FEED_CONSTANT1, ZERO_OFFSET1)

    ethercat_start(10)

    if (ethercat_is_axis_in_fault_state("axis1")):
        textmsg("FAULT in: ", "axis1")
        if(ethercat_reset_axis_fault("axis1")):
            textmsg("Axis 1 FAULT cleared")
        else:
            return False
        end
    end
    ethercat_enable_axis("axis1")
    return True
end

run_axis_config()  #run the axis configuration