You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.5.
Ethernet Port Swap (eth0, eth1)
April 2025
Default Setup
The native Ethernet port is interface: eth0
Inserting a USB-Ethercat adapter creates interface: eth1
The goal is to swap the interface names so that the USB adapter is assigned eth0 and the native ethernet port is assigned eth1. The native Ethernet port provides a better physical device for EtherCAT communications, reducing latency and jitter.
Step 1 – Connect to the Robot
Connect an Ethernet cable (cat5e or better) to communicate with the robot.
Make sure you have an IP address configured in Polyscope (Settings->System->Network)
Use ping to check connection to the robot.
$ ping <robotIPAddress>
Step 2 - Create a Script for Port Swap
On your local machine, copy the script below to a text file, and name it portswap.sh.
#!/bin/sh
echo 'ACTION=="add", SUBSYSTEM=="net", DRIVERS=="igb", NAME="eth1"' \
> /etc/udev/rules.d/70-persistent-net.rules
echo 'ACTION=="add", SUBSYSTEM=="net", DRIVERS=="intel-eth-pci", NAME="eth1"' \
>> /etc/udev/rules.d/70-persistent-net.rules
echo 'ACTION=="add", SUBSYSTEM=="net", SUBSYSTEMS=="usb", NAME="eth%n"'\
>> /etc/udev/rules.d/70-persistent-net.rules
Step 3 - Transfer Script to the Robot
Use scp to transfer the script to the /programs folder of the Robot.
$ scp <pathToYourScript>/portswap.sh root@<robotIPAddress>:/programs
Step 4 - Log in to the Robot
Use ssh to log in to the robot.
$ ssh root@<robotIPAddress>
Step 5 - Run Script
After login, go to /programs folder to run the script.
$ cd /programs
$ bash ./portswap.sh
The script will create a file at /etc/udev/rules.d/70-persistent-net.rules.
Step 6 - Restart the Robot
$ shutdown -r now
Your native ethernet port is now interface eth1 and should be used for EtherCAT. Your USB ethernet port is now interface eth0 and should be used for ssh and other TCP/IP communications.
Do not route the EtherCAT cable through a switch - it should be connected directly to the first EtherCAT drive on the fieldbus.
Try connecting again over ssh using same IP address.