You're reading an old version of this documentation. If you want up-to-date information, please have a look at v10.15 or the latest docs.

Welcome to ROS 2 Documentation for Polyscope X

This documentation contains information about the ROS 2 components built into Polyscope X. It is intended to use ROS 2 messages and services directly from URScript and access robot realtime data over ROS 2.

Note

There is a separate ROS 2 driver documentation, see Universal Robots ROS2 driver page for more details.

The ROS2 integration paths page explains the difference between the built-in ROS 2 support and the ROS 2 driver.

If you need help with ROS2, please email support@universal-robots.com