You're reading an old version of this documentation. If you want up-to-date information, please have a look at v10.14 or the latest docs.
Welcome to ROS 2 Documentation for Polyscope X
This documentation contains information about the ROS 2 components built into Polyscope X 10.13 and later. It is intended to use ROS 2 messages and services directly from URScript and access robot realtime data over ROS 2.
Note
There is a separate ROS 2 driver documentation, see Universal Robots ROS 2 driver page for more details.
The ROS2 integration paths page explains the difference between the built-in ROS 2 support and the ROS 2 driver.
Contents
If you need help with ROS2, please email support@universal-robots.com