Ethernet Port Swap (eth0, eth1)

October 2024

Default Setup

The native Ethernet port is device: eth0

Inserting a USB-Ethercat adapter creates device: eth1

The goal is to swap the device names so that the USB adapter is assigned eth0 and the native ethernet port is assigned eth1. The native ethernet port provides a better physical device for ethercat communications, reducing latency and jitter.

Step 1 – Connect to the Robot

Connect an Ethernet cable (cat5e or better) to communicate with the robot over ssh.

Make sure you have an IP address configured in Polyscope (Settings->System->Network)

Use ssh to connect to the robot.

$ ssh root@<robotIPAddress>

Step 2 - List the network devices

Insert the USB adapter into the USB 3.0 port of the control box, and run the following command.

$ ls -l /sys/class/net
lrwxrwxrwx  1 root root 0 May 14 17:56 eth0 -> ../../devices/pci0000:00/0000:00:14.0/0000:05:00.0/net/eth0/
lrwxrwxrwx  1 root root 0 May 14 18:01 eth1 -> ../../devices/pci0000:00/0000:00:15.0/usb2/2-3/2-3:2.0/net/eth1/

You can see that eth0 is assigned to the native Ethernet port eth1 is assigned to the USB Ethernet adapter.

Step 3 - Find the native Ethernet driver

Run the following command to identify the kernel driver used by the eth0 native Ethernet interface.

$ basename $(realpath /sys/class/net/eth0/device/driver)

The output should usually be igb (for older control boxes) or intel-eth-pci (for newer control boxes).

Step 4 - Assign the interfaces device names

Change the net generator rules to set device assignment to specific interfaces

Create or edit the file /etc/udev/rules.d/75-persistent-net-generator.rules to have the following lines, substituting <eth0-driver-name> for the name of the eth0 driver you found on the previous step:

SUBSYSTEM=="net", ACTION=="add", DRIVERS=="<eth0-driver-name>", NAME="eth1"
SUBSYSTEM=="net", ACTION=="add", SUBSYSTEMS=="usb", NAME="eth0"

Step 5 - Restart the UR control box

$ shutdown -r now

Your native ethernet port is now eth1 and should be used for ethercat. Your USB ethernet port is now eth0 and should be used for ssh and other TCP/IP communications.

Do not route the ethercat cable through a switch - it should be connected directly to the first EtherCAT drive on the fieldbus.

Try connecting again over ssh using same IP address.