MotionPlus Documentation Logo

Contents

  • Introduction
  • Installation
  • MotionPlus URCap
  • World Model
  • APIs
  • Servos
  • Examples
    • EtherCAT & Axis Configuration
      • EtherCAT Drive Config Script
      • Homing Script
      • Single Rotary Axis Calibration
      • Single Linear Axis Calibration
      • Dual Rotary Axis Calibration Script
    • Motion
      • Constructing and Jogging a Single Axis Positioner
      • Constructing the Kinematics of a Two Axis Positioner
      • Jogging Two Axis Groups Using Threads
      • Attaching Frames to An Axis
      • Basic Frame Tracking with an Axis
      • Programming Waypoints in a Moving Frame
      • Coordinated Motion with an Axis
      • Coordinated Motion Script
      • Manually Setting the Axis Indices and Streaming over RTDE
      • Configuring, Enabling, and Driving EtherCAT Axes
      • URCaps for MotionPlus
    • World Model
      • Adding, Moving, and Attaching Frames
      • Moving the Robot Using Frames
      • Moving the Robot Relative to the TCP
      • Computing Payloads With Kinematic Tree
      • Moving the Robot’s Base While Following A Trajectory
  • FAQ - Frequently Asked Questions
  • Release Notes
MotionPlus Documentation
  • Examples

You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.5.

Examples

EtherCAT & Axis Configuration

  • EtherCAT Drive Config Script
  • Homing Script
  • Single Rotary Axis Calibration
  • Single Linear Axis Calibration
  • Dual Rotary Axis Calibration Script

Motion

  • Constructing and Jogging a Single Axis Positioner
  • Constructing the Kinematics of a Two Axis Positioner
  • Jogging Two Axis Groups Using Threads
  • Attaching Frames to An Axis
  • Basic Frame Tracking with an Axis
  • Programming Waypoints in a Moving Frame
  • Coordinated Motion with an Axis
  • Coordinated Motion Script
  • Manually Setting the Axis Indices and Streaming over RTDE
  • Configuring, Enabling, and Driving EtherCAT Axes
  • URCaps for MotionPlus

World Model

  • Adding, Moving, and Attaching Frames
  • Moving the Robot Using Frames
  • Moving the Robot Relative to the TCP
  • Computing Payloads With Kinematic Tree
  • Moving the Robot’s Base While Following A Trajectory
Previous Next

© Copyright 2025, Universal Robots A/S.

Other Versions v: mp1.2
Branches
mp1.5
mp1.0
mp1.1
mp1.2
mp1.3
mp1.4