C++ API Reference
There is a generated API documentation as a part of the ROS package documentation:
https://docs.ros.org/en/rolling/p/ur_client_library/generated/index.html
It is generated directly from the source code using Doxygen. Though the documentation is hosted inside the ROS documentation structure, it is not a ROS-specific API. The API is the same for all platforms.