Build / installation

Plain cmake

To build this library standalone so that you can build you own applications using this library, follow the usual cmake procedure:

$ git clone https://github.com/UniversalRobots/Universal_Robots_Client_Library ur_client_library
$ cd ur_client_library
$ mkdir build && cd build
$ cmake ..
$ make
$ sudo make install

This will install the library into your system so that it can be used by other cmake projects directly.

Inside a ROS / ROS 2 workspace

The ur_client_library is available in all maintained ROS distribution and can be installed using

$ sudo apt install ros-$ROS_DISTRO-ur-client-library

Unless you explicitly want to contribute to this library we recommend using the binary installation instead of building from source as explained below.

ROS noetic

If you want to build this library inside a ROS workspace, e.g. because you want to build the Universal Robots ROS driver from source, you cannot use catkin_make directly, as this library is not a catkin package. Instead, you will have to use catkin_make_isolated or catkin build to build your workspace.

ROS 2

If you want to build this library inside a ROS 2 workspace, e.g. because you want to build the Universal Robots ROS2 driver from source, simply clone this project into your workspace and build your workspace as usual.

Use this library in other projects

When you want to use this library in other cmake projects, make sure to

  • Add find_package(ur_client_library REQUIRED) to your CMakeLists.txt (Requires to have the client library installed and your PATH setup done correctly. As an alternative, fetch and build it as part of your project as shown below.)

  • add ur_client_library::urcl to the list of target_link_libraries(...) commands inside your CMakeLists.txt file.

As a minimal example, take the following “project”:

As a minimal executable, we’ll create a client for the dashboard server and ask for the PolyScope version.

Note

This will not work on PolyScope X versions, as the dashboard server is not available there.

Listing 1 main.cpp
 1#include <iostream>
 2#include <ur_client_library/ur/dashboard_client.h>
 3
 4int main(int argc, char* argv[])
 5{
 6  urcl::DashboardClient my_client("192.168.56.101");
 7  bool connected = my_client.connect();
 8  if (connected)
 9  {
10    std::string answer = my_client.sendAndReceive("PolyscopeVersion\n");
11    std::cout << answer << std::endl;
12    my_client.disconnect();
13  }
14  return 0;
15}

In this example, we’ll fetch the client library as part of the project and build it together with our application:

Listing 2 CMakeLists.txt
 1cmake_minimum_required(VERSION 3.11.0) # That's the minimum required version for FetchContent
 2project(minimal_example)
 3
 4include(FetchContent)
 5FetchContent_Declare(
 6  ur_client_library
 7  GIT_REPOSITORY https://github.com/UniversalRobots/Universal_Robots_Client_Library.git
 8  GIT_TAG        master
 9)
10
11# This will download the ur_client_library and replace the `find_package(ur_client_library)` call.
12FetchContent_MakeAvailable(ur_client_library)
13
14add_executable(db_client main.cpp)
15target_link_libraries(db_client ur_client_library::urcl)

To build the project, create a build directory and run cmake:

$ mkdir build && cd build
$ cmake ..
$ cmake --build .

Then (with a robot switched on and available on 192.168.56.101), you can test the minimal example application:

$ ./db_client
INFO /<...>/ur/dashboard_client.cpp 72: Connected: Universal Robots Dashboard Server

URSoftware 5.19.0.1210631 (Oct 23 2024)
INFO /<...>/ur/dashboard_client.cpp 98: Disconnecting from Dashboard server on 192.168.56.101:29999