ur_robot_driver
keep_alive_count -> robot_receive_timeout
Doing real-time control with a robot requires the control pc to conform to certain timing
constraints. For this keep_alive_count
was used to estimate the tolerance that was given to the
ROS controller in terms of multiples of 20 ms. Now the timeout is directly configured using the
robot_receive_timeout
parameter of the hardware interface.
ros2_control xacro tag moved to driver package
The description package no longer adds the ros2_control
tag to the robot’s URDF. This is done
in the driver now. Therefore, there is a urdf
folder containing the macro for generating a
ros2_control
tag and a ready-to-use xacro file for a UR robot with a ros2_control
tag.
If you want to create your own controlled robot, you should mimic that structure, as done e.g. in the custom_workcell_tutorial.
robot_description is now distributed by the robot_state_publisher
The robot_description
isn’t propagated to all interested parties as a parameter. Instead, only
the robot_state_publisher
is provided with the parameter, republishing it on the
robot_description
topic.
Therefore, there is a new launchfile ur_rsp.launch.py
which takes care about loading the
description and starting the robot_state_publisher
. If you create a description that needs
other parameters than the packaged one, you can write your own rsp
launch file and pass that as
description_launchfile
argument to ur_control.launch.py
.
Enforce absolute paths in launchfiles
All launchfiles now expect an absolute path for files that should be used to alter the launch
process (e.g. description file, controllers file). Before it was expecting e.g. a
description_package
and a description_file
argument with a relative path to the package.
The default files have not been changed, so unless you specified your custom package / file combinations, you will need to update that to an absolute path.
Absolute paths can still be generated dynamically using a package + relative path structure inside
other launchfiles or by using ros2 pkg prefix
on the command line. For example, you can do
$ ros2 launch ur_robot_driver ur_control.launch.py ur_type:=ur20 robot_ip:=192.168.56.101 \
kinematics_params_file:=$(ros2 pkg prefix my_robot_cell_control)/share/my_robot_cell_control/config/my_robot_calibration.yaml
Removal of ros2_control_node
The ros2_control_node
has been removed from the driver in #939. Instead, the
ur_control.launch.py
launchfile now uses the controller_manager
’s ros2_control_node
directly. This change is only relevant if you wrote your own launchfile starting the
ur_robot_driver
’s ros2_control_node
. In that case, you should adapt your launchfile to use
the controller_manager
’s ros2_control_node
instead. Remember to also remove the
robot_description
parameter as explained above.
ur_control_node = Node(
- package="ur_robot_driver",
- executable="ur_ros2_control_node",
+ package="controller_manager",
+ executable="ros2_control_node",
parameters=[
- robot_description,
update_rate_config_file,
ParameterFile(initial_joint_controllers, allow_substs=True),
],